L-com

Troubleshooting Servo and VFD Cable Issues

By Eileen Harvey 

Servo and variable frequency drive (VFD) cables are the lifelines of modern industrial automation systems. From CNC machines and robotic arms to conveyors and motion control systems, these cables transmit both power and signals with precision. Any malfunction in a servo or VFD cable can cause downtime, loss of productivity and even equipment damage. Proper installation, maintenance and troubleshooting are therefore essential to ensure reliable performance.  

Common Issues in Servo and VFD Cables 

Servo and VFD cables can experience several electrical problems that affect system performance. 

  • Electrical problems such as voltage drops occur when cables are undersized or made from poor quality materials, reducing the power delivered to the motor. Insulation breakdown is another issue, developing over time as heat, oil or chemicals weaken the insulating layers. EMI and RFI interference can disrupt drive systems when shielding is inadequate, leading to unstable operation or communication errors. 
  • Mechanical failures are also common, especially in environments with continuous motion. Constant bending in robotic applications can cause cable fatigue, while cuts and abrasions may result from sharp edges or improper routing.  
  • Environmental conditions contribute further challenges because exposure to oil, UV radiation, water or harsh chemicals accelerates cable degradation. Outdoor installations face additional stress from extreme temperatures that can make jackets brittle or deform under heat. 
  • Connector and termination problems often lead to intermittent faults. Loose or corroded connections reduce power or signal integrity, and poor shielding continuity creates pathways for electrical noise to escape. Proper installation and regular inspection are essential to prevent these issues and maintain reliable system performance. 

Symptoms of Cable Problems 

From internet service providers to enterprise networks, the integrity of cable systems directly impacts performance and reliability. However, like any critical infrastructure, cables can experience a variety of issues that may compromise their functionality. Recognizing the symptoms of cable problems is essential for timely intervention and resolution, thereby minimizing downtime and maintaining operational efficiency.  

Early detection saves downtime. Watch out for: servo motor vibration or instability, unexpected drive shutdowns or error codes, signal noise or intermittent communication loss, overheating of cables or connectors and reduced machine accuracy or efficiency. 

Troubleshooting Methods 

Effective troubleshooting of servo and VFD cable issues begins with a thorough visual inspection. This involves checking for cuts, abrasions, cracks, discoloration or burn marks along the cable jacket and examining connectors for corrosion or loose fittings. Continuity and insulation resistance testing provide deeper insight into cable health. A multimeter can verify conductor continuity, while a megohmmeter tests the integrity of the insulation to reveal breakdowns that may not be visible externally. Signal integrity tests are also important, using appropriate equipment to measure the performance of EMI shielding and ensuring that all shield connections are continuous and properly grounded. Thermal monitoring with infrared thermography helps detect hotspots that may indicate overload conditions or poor connections. A final step is assessing connectors and shielding by confirming that the shields are properly grounded at both ends and re-crimping or replacing any faulty connectors. 

Installation Best Practices 

Proper installation plays a major role in preventing cable failures. Servo and VFD cables should be routed separately from high voltage power lines to reduce electromagnetic interference, and installers must maintain the recommended bending radius, usually between 7.5 and 10 times the cable diameter, to prevent mechanical stress. Grounding and shielding practices are equally important. Braid shields should always be grounded at both the drive and motor ends, and 360-degree shield terminations are preferred over pigtail connections to maintain full shielding effectiveness. Strain relief and support measures, such as using strain relief clamps and installing cable trays or conduits in harsh environments, help reduce mechanical fatigue and extend cable life. 

Maintenance Tips for Longevity 

Regular maintenance is essential to ensure long term reliability of servo and VFD cables. Inspections should be scheduled every 6 to 12 months to catch early signs of wear. Connectors and terminals should be cleaned periodically to prevent oxidation and dirt buildup that can affect signal or power flow. Worn cables should be replaced before complete failure occurs to avoid unexpected downtime. Keeping a performance log of cable faults, inspections and replacements helps track trends and predict future issues. When systems operate in harsh environments, using cables that are oil resistant and UV stable adds another layer of protection and supports long service life. 

When to Replace vs. Repair 

Repair is feasible for minor connector issues or damaged shielding. Replacement is necessary if insulation is cracked or brittle, EMI issues persist even after re-shielding and multiple conductors show wear. Investing in high-quality replacements like Kaweflex servo and VFD cables ensures long-term reliability. 

Real-World Case Example 

A CNC machine shop reported random drive shutdowns and motor vibration. An inspection determined that the VFD cables were routed parallel to high-voltage lines and EMI was disrupting servo control signals. The solution was to reroute cables separately and to upgrade to shielded Kaweflex EMC-optimized VFD cables. 

FAQs About Servo and VFD Cable Issues 

Q1: Can I use regular power cables instead of VFD cables? 
A: No. VFD cables are specifically designed with EMC shielding and low capacitance to handle high-frequency switching. 

Q2: How often should I inspect my servo cables? 
A: At least every six months, but more frequently in high-motion or harsh environments. 

Q3: What happens if I ignore minor cable damage? 
A: Even small cuts can lead to moisture ingress, EMI leakage or insulation breakdown, causing costly downtime. 

Q4: Are TKD Kabel products suitable for outdoor use? 
A: Yes, many TKD Kabel products are UV-, oil- and chemical-resistant, making them ideal for both indoor and outdoor applications. 

Q5: Can EMI issues be solved just with ferrite cores? 
A: Ferrite cores help, but shielded VFD cables are the best long-term solution. 

Servo and VFD cables play a vital role in keeping industrial automation running smoothly. By following installation best practices, performing regular maintenance and knowing how to troubleshoot issues, you can prevent costly downtime. 

When replacement is needed, choosing reliable, EMC-optimized and industrial-grade cables such as TKD Kabel ensures maximum performance and durability. 

Explore the full range of TKD Kabel through L-com. We’ll fill your orders fast, with same-day shipping on all qualified, in stock, online orders received Monday through Friday before 5 p.m. EST. For TKD-related inquiries, connect with our U.S-based TKD expert Eileen Harvey at eharvey@infiniteelectronics.com. 

Resources

Search Entries