By Dustin Guttadauro, Product Line Manager - Telecom & Fiber, Infinite Electronics
Key Takeaway
- M12 connectors use a letter-coded keying system (A, B, D, X, K, L, S, T) — the code determines pin layout, application, and whether the connector will physically mate with the device.
- D-code handles 100 Mbps Ethernet (4 pins, 2 pairs); X-code handles Gigabit and 10G Ethernet (8 pins, 4 pairs) — these are not interchangeable.
- All standard M12 codings achieve IP67 sealing, making them the default choice over RJ45 in any environment with coolant, wash-down, or dust.
- Field-terminated connectors give you custom cable lengths; molded cordsets are faster to install and more reliable in vibration-heavy applications — the trade-off is worth understanding before you order.
- The most common installation mistake is ordering the wrong coding — usually D-code when X-code is needed for Gigabit, or A-code in a B-code PROFIBUS socket.
The M12 connector standard has been around since the 1980s, but the catalog has gotten more complex as industrial Ethernet moved into the form factor. If you're specifying connectors for a new control system — or migrating from DB9 or RJ45 — the coding table below is the first thing to get right.
What Do the M12 Codes Actually Mean? (Cheat Sheet)
The letter code stamped on an M12 connector tells you its electrical application and keying position. Different codes use different key shapes to prevent mismating — an A-code plug won't seat in a B-code socket, and vice versa. Here's the full reference:
|
Code |
Pin Count |
Application |
IP Rating |
Common Use |
|
A-code |
3, 4, 5, 8 |
Sensors / I/O |
IP67/IP68 |
Proximity sensors, photoelectric sensors, solenoid valves |
|
B-code |
5 |
PROFIBUS |
IP67 |
PROFIBUS DP field device connections |
|
D-code |
4 |
100 Mbps Ethernet |
IP67 |
Industrial cameras, PROFINET, EtherNet/IP at 100 Mbps |
|
X-code |
8 |
Gigabit / 10G Ethernet |
IP67/IP68 |
High-speed machine vision, edge computing nodes, 10GBASE-T links |
|
K-code |
6 |
AC/DC power (up to 63 A) |
IP67 |
Servo drives, motor power distribution |
|
L-code |
4 |
DC power (PELV) |
IP67 |
24 VDC bus power for sensors/actuators |
|
S-code |
4 |
AC power (up to 630 V) |
IP67 |
High-voltage AC distribution in cabinet-free panels |
|
T-code |
4 |
DC power (high-current PELV) |
IP67 |
DC bus distribution at up to 630 V DC |
📌 Quick rule: If you're wiring sensors and I/O, you're almost certainly using A-code. If you're running Ethernet at 100 Mbps, use D-code. Gigabit or 10G? X-code only. Power distribution in a cabinet-free panel usually means K, L, S, or T depending on voltage and current.
How Many Pins Do You Need?
Pin count follows application.
- 3-pin A-code: Basic sensors with one output (PNP/NPN proximity sensors, simple photoelectrics).
- 4-pin A-code: The most common format — covers the majority of discrete sensors and actuators with a ground, supply, and two signal wires.
- 5-pin A-code: Used when you need two independent outputs or an analog output alongside a digital one.
- 8-pin A-code: Multi-function sensors, IO-Link masters with multiple channels, and some encoders.
- 4-pin D-code: Industrial 100 Mbps Ethernet — two TX pairs, two RX pairs. Standard for PROFINET, EtherNet/IP, and Modbus TCP at this speed.
- 8-pin X-code: Gigabit and 10GBASE-T Ethernet — all four pairs active. Required by IEEE 802.3 for anything above 100 Mbps.
- 5-pin B-code: PROFIBUS DP only. Not interchangeable with A-code 5-pin despite the same pin count — the key slot is in a different position.
What IP Protection Do M12 Connectors Provide?
Standard mated M12 connectors are IP67 — dust-tight and protected against temporary submersion up to 1 meter for 30 minutes. That covers wash-down environments, coolant splash, and most outdoor installations.
IP68-rated variants exist for permanent submersion applications (underwater conveyors, pump monitoring, subsea sensors). These typically require a specific mating torque and a compatible IP68 socket. X-code connectors are increasingly specified at IP67/IP68 as 10G infrastructure moves into harsher environments.
One thing worth noting: IP ratings apply to the mated pair. An unmated M12 socket sitting open on a machine is not IP67. Always cap unused ports with protective plugs.
What Is the Difference Between M12 D-Code and X-Code?
D-code and X-code are both designed for industrial Ethernet, but they're built for different speed tiers and are physically incompatible.
D-code (4-pin): Carries 100BASE-TX using two differential pairs. It's the standard for PROFINET Class A and EtherNet/IP at 100 Mbps, and it's what most existing Ethernet-capable sensors and cameras with M12 ports use. The 4-pin layout maps cleanly to the T568B wiring convention on the Ethernet side.
X-code (8-pin): Carries all four pairs needed for Gigabit and 10GBASE-T. If your switch or controller negotiates at 1000BASE-T or 10GBASE-T, you need X-code. Using a D-code cordset with an X-code device will either auto-negotiate down to 100 Mbps (if the switch permits it) or produce no link at all.
M12 connector pinout reference for D-code and X-code:
|
Pin |
Wire Color |
D-code (100 Mbps) |
X-code (Gigabit/10G) |
|
1 |
Yellow |
TD+ (Transmit Data +) |
DA+ (pair 1 +) |
|
2 |
White |
RD+ (Receive Data +) |
DA- (pair 1 -) |
|
3 |
Orange |
TD- (Transmit Data -) |
DB+ (pair 2 +) |
|
4 |
Blue |
RD- (Receive Data -) |
DB- (pair 2 -) |
|
5 |
— |
Shield/GND (in 5-pin variants) |
DC+ (pair 3 +) |
|
6 |
— |
— |
DC- (pair 3 -) |
|
7 |
— |
— |
DD+ (pair 4 +) |
|
8 |
— |
— |
DD- (pair 4 -) |
📌 Rule of thumb: Check your switch's negotiation capability before ordering cordsets. If the switch is 10/100 only, D-code is fine and saves you money. If it's 10/100/1000, spec X-code from the start to avoid re-cabling when you upgrade.
M12 vs RJ45: When Does M12 Actually Win?
RJ45 connectors are cheap and universal. M12 connectors cost more and come in more flavors. So when does M12 make sense?
Sealing: RJ45 has no IP rating. In any environment with coolant mist, dust, wash-down, or outdoor exposure, an unprotected RJ45 port will eventually fail. M12 at IP67 is the answer.
Vibration: RJ45's clip-lock retention is notoriously poor in vibrating machinery. M12's threaded coupling nut stays put.
Connector abuse: Industrial environments are hard on cables. M12's metal or reinforced-plastic bodies hold up better than RJ45's fragile tab.
Panel space: M12's 12 mm diameter is compact. Crowded control panels and junction boxes with six to twelve Ethernet ports benefit from M12's smaller footprint.
RJ45 still makes sense in clean, controlled environments — office-style electrical rooms, server racks, and HMI cabinets. On the machine itself, M12 is the better call almost every time.
Field-Terminated Connectors vs. Molded Cordsets: Which Should You Use?
Molded cordsets are factory-assembled with the connector bonded to the cable under controlled conditions. Field-terminated connectors are assembled by hand on-site using a separate housing and the cable you pull.
When molded cordsets make sense:
- Standard lengths work for your machine layout (0.5 m, 1 m, 2 m, 3 m, 5 m are widely stocked)
- High-vibration applications where a hand-assembled connection might loosen
- You want guaranteed IP67 without depending on field assembly quality
- Production volume justifies keeping pre-tested assemblies in stock
When field termination makes sense:
- You need a non-standard cable length or are pulling cable in conduit
- You're doing repair work and need to terminate on-site without ordering a specific assembly
- You're assembling a custom harness for a complex machine
The main risk with field termination is getting the pin order wrong. Print the pinout and tape it to your workbench. Double-check continuity before the cable goes into service.
For standard runs on new builds, molded cordsets from a stocked supplier like L-com remove the assembly variable entirely. Browse
the full selection of M12 connectors and cordsets to find stocked options by code, length, and pin count.
Mistakes We See in the Field
These are the errors that show up most often when engineers and installers are specifying or deploying M12 connectors. Most are easy to avoid once you know to look for them.
|
Mistake |
What Goes Wrong |
How to Avoid It |
|
Wrong coding (D vs X) |
D-code connectors physically fit X-code panel cutouts in some cases, but the pin layout differs — you'll get no link or damaged pairs |
Label the code clearly on your BOM; double-check before ordering cordsets |
|
Over-torquing the coupling nut |
Plastic coupling threads strip at anything above 0.6 N·m; metal bodies fare better but seals can deform |
Use a torque screwdriver. 0.4–0.6 N·m is the sweet spot for IP67 |
|
Mixing connector brands mid-run |
Thread pitch or sealing face geometry may differ between manufacturers, causing incomplete mating and loss of IP rating |
Standardize on one brand per interface type per project |
|
Using D-code for Gigabit |
D-code is 2-pair; Gigabit needs 4 pairs. You'll train at 100 Mbps or get no link at all |
Gigabit = X-code, always. Check switch negotiation if unsure |
|
Ignoring bend radius on field-terminated cables |
Kinking cable at the connector back-end cracks foil shields and causes intermittent faults that are nearly impossible to trace |
Follow manufacturer's minimum bend radius; use a strain relief boot for field installs |
|
Confusing B-code and A-code on 5-pin |
Both have 5 pins, different key positions. An A-code plug will not mate with a B-code socket and vice versa — but cheap connectors occasionally let you force it |
Inspect the keyway before mating. B-code has a different key slot than A-code |
📌 If you've over-torqued connectors before: You'll know because the coupling nut spins freely before it should, or you can feel the threads skip. Stop, replace the connector, and use a torque driver going forward. A stripped M12 coupling nut in a wet environment is a ticking clock for intermittent faults.
Sourcing Checklist Before You Order
Use this before finalizing your bill of materials:
|
✓ |
Pre-Purchase Checklist |
|
☐ |
Confirmed coding type (A / B / D / X / K / L / S / T) — checked against fieldbus and speed requirements |
|
☐ |
Pin count verified against device datasheet (3, 4, 5, or 8 pin) |
|
☐ |
IP rating confirmed for wash-down, immersion, or standard industrial environment |
|
☐ |
Decided between molded cordset and field-terminated: molded for long stable runs, field-term for custom lengths and repairs |
|
☐ |
Coupling nut type selected: push-pull for rapid disconnect, threaded M12 for high-vibration |
|
☐ |
Cable jacket material selected: PUR for oil/flex, PVC for general use, TPE for food-grade |
|
☐ |
Manufacturer standardized across the installation: no mixing of brands mid-run |
|
☐ |
Verified cable AWG vs current draw for power codes (K/L/S/T) |
|
☐ |
Ordered 10–15% spare connectors and cordsets for installation losses and future service |
|
☐ |
Cross-referenced L-com M12 catalog for stocked cordset lengths and assemblies |
L-com stocks a broad range of M12 connectors and cordsets across all coding types, pin counts, and cable lengths. You can also search the industrial Ethernet cable assemblies catalog for pre-built M12-to-M12 and M12-to-RJ45 assemblies. For the connector hardware side, see our Ethernet connectors section.
Frequently Asked Questions (FAQs)
What is an M12 connector?
An M12 connector is a circular, threaded connector with a 12 mm diameter locking nut, standardized under IEC 61076-2-101. It's designed for industrial environments that need reliable IP67 sealing, vibration resistance, and compact form factor. The connector comes in multiple codings (A, B, D, X, and others) that define the pin layout and the application — sensors, PROFIBUS, Ethernet, or power.
Can I use a D-code M12 connector for Gigabit Ethernet?
No. D-code is a 4-pin, 2-pair connector rated for 100 Mbps. Gigabit Ethernet (1000BASE-T) and 10GBASE-T both require all four pairs to be active, which means you need an 8-pin X-code connector. Plugging a D-code cordset into an X-code device will result in either a 100 Mbps fallback negotiation or no link at all.
What is the IP rating of M12 connectors?
Mated M12 connectors are rated IP67 as standard — dust-tight and protected against temporary immersion up to 1 meter for 30 minutes. IP68-rated variants are available for continuous submersion applications. The rating applies only when the connector is fully mated and tightened to the specified torque. Unmated sockets require a protective cap to maintain their IP rating.
What is the difference between M12 A-code and B-code?
Both A-code and B-code come in 5-pin versions, which is the main source of confusion. A-code is for sensors, actuators, and general I/O. B-code is exclusively for PROFIBUS DP. The key slot on A-code and B-code is in a different position, so they won't mate — but some lower-quality connectors have enough slop to allow forced mating, which will damage pins. Always verify the code before connecting.
Should I use field-terminated M12 connectors or molded cordsets?
Molded cordsets are the better choice for most new installations: they come pre-tested, maintain IP67 without depending on field assembly quality, and are available in standard lengths from most industrial suppliers. Field-terminated connectors make sense for non-standard cable lengths, repair situations, and custom harnesses. If you go field-terminated, print the pinout, verify your work with a continuity tester, and don't skip the torque spec on the coupling nut.