L-com

Impedance, Bandwidth and Data Transmission in PROFINET Systems

PROFINET has emerged as the backbone of industrial Ethernet communication, offering a robust framework that facilitates seamless data exchange across factories, process plants and automation systems. This advanced communication protocol allows for real-time interaction between various devices, ensuring that operations run smoothly and efficiently. However, the reliability of PROFINET is not coincidental; it rests on three critical technical pillars: impedance, bandwidth and data transmission.  

These factors are essential for maintaining the integrity and speed of communication within complex industrial environments. For instance, impedance refers to the resistance that electrical signals encounter as they travel through cables and connectors. If there are mismatches in impedance—often due to poor cable selection or substandard connections—it can lead to signal reflections and loss, severely impacting communication quality. 

What is Impedance? 

Impedance is the opposition that a cable presents to the flow of alternating current (AC) signals. In PROFINET cables, the standard characteristic impedance is 100 ohms ±15%, ensuring compatibility with Ethernet-based communication. 

Why is Consistent Impedance Important? 

When impedance varies along a cable, it creates signal reflections and echoes, leading to errors, noise and reduced network reliability. Correct impedance (100 ohms) is needed for smooth data transfer. Impedance mismatch causes attenuation, jitter and packet loss. 

 

Problems that can result from impedance mismatch include unstable communication between devices, reduced cable length capacity, and increased error rates and retransmissions. 

Specialized cable testers help measure impedance. Consistent impedance is critical for achieving PROFINET certification and ensuring long-term system reliability. 

Bandwidth in PROFINET Systems 

Bandwidth represents the amount of data that can be transmitted per second. In PROFINET, it determines how many devices and processes can communicate without delays. Bandwidth for standard PROFINET is 100 Mbps; for advanced applications it is up to 1 Gbps (Gigabit PROFINET). 

Bandwidth matters because high bandwidth ensures smooth data exchange in real-time control systems, robotics and motion control, and Industry 4.0 applications where large amounts of sensor data must be transmitted instantly. 

Cable Categories and Bandwidth 

Cat5e cables bring bandwidth of up to 100 MHz and they support 100 Mbps PROFINET. Cat6 cables offer up to 250 MHz and support Gigabit PROFINET. Cat7 delivers up to 600 MHz bandwidth and is best suited for future-proofing high-bandwidth systems. 

Data Transmission Principles 

PROFINET uses Ethernet frames for transmitting data between devices. These frames must move reliably even in electrically noisy industrial environments. 

Factors Affecting Data Transmission 

Let’s look at four factors. First is shielding quality, since shielding prevents EMI. A second factor is cable length—PROFINET limits cable length to 100 meters between devices. Crosstalk is a third factor, and it must be minimized with twisted-pair designs. A fourth factor affecting data transmission is latency and jitter, since low latency and minimal jitter are crucial for motion control applications. 

Deterministic Communication 

Unlike office Ethernet, PROFINET ensures deterministic communication, meaning data reaches its destination at predictable intervals critical for automation. 

Relationship Between Impedance, Bandwidth and Data Transmission 

Impedance, bandwidth and data transmission are deeply connected. Consistent impedance ensures signals don’t reflect, enabling stable data transmission. Adequate bandwidth allows high-volume communication with low latency. And quality data transmission ensures real-time communication in harsh industrial conditions. 

An example is a plant experiencing communication delays because it is running Cat5e cables with impedance mismatches. Upgrading to Cat6 shielded PROFINET cables reduces errors, supports higher bandwidth and improves reliability. 

Standards and Compliance 

PROFINET systems must adhere to international cabling standards for performance and safety. IEC 61158 and IEC 61784 standards are for industrial communication. ISO/IEC 11801 standards are for structured cabling systems. And PI guidelines (PROFIBUS and PROFINET International) ensure interoperability and certification. 

Practical Tips for Engineers and Installers 

  • Check impedance consistency before deployment using certified testers. 
  • Choose Cat6 or Cat7 cables if your plant requires Gigabit PROFINET or future scalability. 
  • Use shielded cables (S/FTP or SF/UTP) in high-noise environments. 
  • Follow bend radius limits during installation to avoid micro-cracks in shielding. 
  • Keep cable runs under 100 meters between devices. 
  • Perform regular certification testing to ensure compliance. 

 

Real-World Applications 

Consider four popular applications for PROFINET systems. First is factory automation, with robots, conveyors and PLCs requiring low-latency communication. Second is process control, with oil and gas and chemical plants depending on uninterrupted data exchange. A third application is the automotive industry; Gigabit PROFINET is used in high-speed assembly lines. And fourth, smart factories use PROFINET—Industry 4.0 relies on high bandwidth and minimal jitter. 

Future Trends 

  • Gigabit and 10-Gigabit PROFINET: Emerging for advanced applications 
  • Time-Sensitive Networking (TSN): Ensures ultra-low latency and synchronization 
  • Hybrid Cables: Combining data + power (Single Pair Ethernet) 
  • Enhanced Shielding Designs: To support IoT-driven smart factories 

Impedance, bandwidth and data transmission form the foundation of PROFINET system performance. By selecting the right cables, maintaining proper installation practices and adhering to standards, engineers can build reliable, high-speed and future-ready industrial Ethernet networks. 

Whether you’re upgrading from Cat5e to Cat6, troubleshooting impedance mismatches or designing a gigabit-ready plant, keeping these fundamentals in mind ensures smooth industrial communication. 

Explore the full range of TKD Kabel through L-com. We’ll fill your orders fast, with same-day shipping on all qualified, in stock, online orders received Monday through Friday before 5 p.m. EST. For TKD-related inquiries, connect with our U.S-based TKD expert Eileen Harvey at eharvey@infiniteelectronics.com. 

Resources

Search Entries