L-com

What Is the Maximum Length of a PROFINET Cable?

By Eileen Harvey 

In modern industrial automation, PROFINET has become the backbone of communication between programmable logic controllers (PLCs), sensors, actuators, robots and entire factory networks. Being an Industrial Ethernet standard, it inherits many of the technical characteristics of Ethernet, including performance limits related to cable length. 

One of the most important factors in designing and maintaining a PROFINET network is understanding the maximum cable length. If you exceed this limit, you risk data errors, communication breakdowns and costly downtime. 

Standard Maximum Length of PROFINET Cables 

The golden rule is that the maximum length of a PROFINET copper cable = 100 meters (328 feet). This limitation applies to: Category 5e or higher cables, both shielded and unshielded twisted pair (UTP/STP), and horizontal runs in industrial networks. This aligns with the Ethernet IEEE 802.3 standard, meaning PROFINET shares the same physical layer limitations as Ethernet. 

Typical Applications Within 100 Meters 

Common applications are: connecting PLCs to sensors/actuators within a machine, linking operator panels and drives to control cabinets and wiring devices inside automation cells. If your installation is within a single production line or factory floor, 100 meters is usually more than enough. 

Factors Affecting Cable Length 

While the 100-meter rule is standard, real-world conditions may reduce the effective maximum length. Let’s look at the key factors: 

  • Cable Type: Cat5e PROFINET cables are most common, supporting data rates up to 100 Mbps. Cat6 or Cat6a cables offer higher bandwidth and better shielding. Double-shielded cables (foil + braid) provide stronger EMI protection in harsh environments. 
  • Environmental Conditions: Industrial environments expose cables to: electromagnetic interference (EMI) from motors, drives and high-voltage lines; UV radiation, which degrades PVC jackets outdoors; and chemicals, oils and moisture, which can corrode or weaken insulation. Choosing the right jacket material—PVC, PUR or TPE—helps extend cable life. For example: PVC = cost-effective, general use; PUR = oil/UV resistant, flexible; and TPE = excellent in extreme temperatures. 
  • Installation Practices: Improper installation can reduce cable performance. A tight bending radius damages the conductor and shielding. Running PROFINET alongside power lines increases EMI risk. 

Extending Beyond the 100-Meter Limit 

What if your factory layout requires more than 100 meters of PROFINET cable? Don’t worry—there are several effective solutions. 

One option is to use switches or repeaters. A PROFINET switch can act as a repeater, allowing each network segment to be extended by another 100 meters. It’s important to note, however, that adding more switches can introduce latency, although it’s typically minimal and not problematic for most applications. 

Another solution is to use fiber optic cables, which are ideal for long-distance connections that can extend up to several kilometers. Fiber is immune to electromagnetic interference (EMI), making it an excellent choice for heavy industrial environments. While fiber optic systems have a higher upfront cost, they deliver exceptional long-term reliability and performance. 

A third option is wireless PROFINET, which is commonly used in applications such as Automated Guided Vehicles (AGVs) and cranes. This approach eliminates concerns about cable wear and physical limitations but requires careful network design and strong signal planning to ensure dependable communication. 

Quick Facts About PROFINET Cable Lengths 

  • Standard maximum copper length: 100 meters 
  • Fiber optic PROFINET cables: several kilometers 
  • Bending radius: typically, 10x cable diameter for fixed installation 
  • Incorrect shielding may reduce effective distance by 20% to 30% 

 

FAQs (Frequently Asked Questions) 

Q1: Can I use standard Ethernet cables for PROFINET? 
A: Technically yes, but it is not recommended. PROFINET-certified cables are designed for harsh industrial environments and provide better shielding, durability and compliance. 

Q2: What happens if I exceed 100 meters with copper PROFINET cables? 
A: You may face packet loss, jitter or complete communication failure. The system may run unreliably and could cause downtime. 

Q3: Is fiber better than copper for PROFINET? 
A: Yes, if you need long distances or EMI immunity. Copper is fine for short to medium distances (up to 100 meters). 

Q4: Do switches or repeaters affect PROFINET performance? 
A: Switches add minimal latency, usually microseconds, which is negligible for most industrial applications. 

The maximum length of a PROFINET cable depends on the medium: 100 meters for copper (Cat5e or higher), several kilometers for fiber optics. 

Going beyond 100 meters with copper requires switches, repeaters or fiber optic solutions. To ensure long-term reliability, use certified PROFINET cables, follow the best installation practices (bending radius, shielding and separation), and choose the correct jacket material (PVC, PUR, TPE) depending on the environment. 

By following these guidelines and using trusted suppliers like L-com and TKD Kabel, you can design a PROFINET network that delivers reliability, speed and future-ready performance for Industry 4.0 applications. 

Explore the full range of TKD Kabel through L-com. We’ll fill your orders fast, with same-day shipping on all qualified, in stock, online orders received Monday through Friday before 5 p.m. EST. For TKD-related inquiries, connect with our U.S-based TKD expert Eileen Harvey at eharvey@infiniteelectronics.com. 

Resources

Search Entries