L-com

PROFINET for Harsh Environments: Oil, UV and Chemical Resistant Cable Options

By Eileen Harvey 

As factories and manufacturing plants become increasingly sophisticated, the demand for seamless communication among high-speed robotics, machinery and outdoor logistics systems has never been greater. PROFINET cabling has emerged as a critical component for ensuring that these complex operations run smoothly. However, not every environment is conducive to the longevity and performance of standard cables.  

Factors such as exposure to oil, harsh chemicals, ultraviolet (UV) radiation and mechanical stress can quickly compromise the integrity of conventional Ethernet cables, leading to potential failures, interruptions in production and ultimately, costly downtime that can impact a business's bottom line. 

This is where industrial-grade PROFINET cables come into play. Engineering advancements have resulted in cables specifically designed to withstand the rigors of challenging industrial settings. Equipped with specialized jackets that resist abrasion, chemicals and UV exposure, as well as robust shielding to minimize electromagnetic interference, these cables are built to thrive where ordinary cables would falter.  

Understanding Harsh Industrial Conditions 

Industrial environments expose cables to a wide range of hazards that can compromise performance and longevity. In automotive plants and machining centers, oils and lubricants often seep into cable jackets, leading to swelling, cracking or insulation failure. Outdoor installations such as solar farms, ports and construction systems face continuous UV radiation, which gradually breaks down plastic materials and shortens cable lifespan. In pharmaceutical, food and chemical facilities, aggressive cleaning agents and solvents attack cable jackets and shielding, creating risks of corrosion and failure. Mechanical stress is another major challenge, as constant bending, flexing and abrasion in robotic systems and conveyor lines can significantly reduce cable durability and reliability over time. 

The Role of Specialized PROFINET Cables 

Unlike commercial Ethernet cables, PROFINET cables are engineered for industrial automation. They follow IEC 61158 and IEC 61784 standards, ensuring stable real-time communication even under stress. Let’s look at four key differentiators. First, they have rugged jackets (PVC, PUR, TPE) designed for specific environments. Second, specialized PROFINET cables have shielding (foil, braid or combination) for protection against EMI. Third, they have voltage ratings (typically 300V for industrial grade). And fourth, PROFINET cables have high flexibility for continuous-motion applications. 

Oil-Resistant PROFINET Cables 

Why They Matter: Oil-resistant PROFINET cables are essential in environments such as automotive manufacturing, robotics, CNC machining and packaging lines. Oils and lubricants can penetrate standard cable jackets, leading to material degradation, signal loss and eventual cable failure. Using oil-resistant designs ensures continuous performance and longevity in machinery exposed to these substances. 

Features of Oil-Resistant Cables: These cables typically use PUR (polyurethane) jackets that resist swelling, cracking and deterioration caused by oil exposure. They offer high mechanical strength to endure the motion of moving machine parts, making them ideal for dynamic applications. Many oil-resistant PROFINET cables are also available in flame-retardant and halogen-free variants to enhance safety in industrial environments. 

UV-Resistant PROFINET Cables 

Why They Matter: Outdoor installations such as renewable energy farms, construction sites, ports and automated warehouses expose cables to prolonged sunlight. UV rays can break down conventional plastic materials, causing brittleness and cracking over time. UV-resistant PROFINET cables are designed to withstand continuous sun exposure, maintaining performance and structural integrity for years. 

Features of UV-Resistant Cables: These cables feature jackets made with UV-stabilized polymers that prevent degradation from sunlight. They deliver extended service life in outdoor environments and maintain flexibility and reliability despite temperature fluctuations and moisture. This durability ensures consistent operation in exposed industrial or field-deployed systems. 

Chemical-Resistant PROFINET Cables 

Why They Matter: In industries such as pharmaceuticals, food and beverage and chemical processing, equipment is often cleaned or sanitized with powerful detergents, acids and solvents. Standard cable jackets cannot withstand these chemicals and may corrode, leading to safety issues and communication failures. Chemical-resistant PROFINET cables are specifically designed to overcome these challenges and maintain performance in harsh cleaning or production environments. 

Features of Chemical-Resistant Cables: These cables use jackets made of PUR or TPE that resist detergents, acids and other corrosive substances. They comply with strict hygiene and washdown standards, including FDA and EHEDG requirements in food industry settings. Their robust design ensures a long service life even in highly corrosive or chemically intensive applications. 

Choosing the Right Cable for Harsh Environments 

When selecting PROFINET cables for harsh environments, there are five chief considerations to make. First is environment—is it oily, outdoor (UV) or chemically aggressive? Second is cable type; Type A is for fixed installation, Type B has limited flexibility and Type C is continuous flexing for robotics and conveyors. 

The third consideration is jacket material. PVC is the standard jacket, at lower cost. PUR has superior oil and chemical resistance. TPE has extreme chemical durability. Fourth is shielding—use double-shielded cables in high-EMI environments. And fifth is brand reliability. Choose trusted brands like TKD Kabel for proven performance. 

Case Studies and Applications 

Automotive assembly lines use oil-resistant Type C PROFINET cables that enable continuous robotic welding and painting without jacket degradation. Solar farms deploy UV-resistant Type A cables to ensure reliable long-term connectivity in outdoor weather. In pharmaceutical production, chemical-resistant PROFINET cables withstand daily wash downs, ensuring compliance and uptime. 

Tips and Recommendations 

  • Always match cable type to movement requirements—use Type C for robotics, not Type A. 
  • Prioritize PUR jackets for environments with oils and chemicals. 
  • Double shielding pays off in areas with heavy EMI from motors and drivers. 
  • Factor in future maintenance—installing the right cable upfront reduces downtime costs. 

Quick Facts 

  • Standard Ethernet cables last 6 to 12 months in harsh conditions, while industrial-grade PROFINET cables can last 5 to 10 years. 
  • UV can cause PVC cable jackets to lose up to 50% tensile strength in just two years without protection. 
  • PUR jackets are up to five times more resistant to oil and abrasion compared to PVC. 

 

In industrial automation, the right cabling makes the difference between smooth operations and costly downtime. Oil-resistant, UV-resistant and chemical-resistant PROFINET cables are purpose-built to survive where ordinary cables fail. By choosing the correct jacket material, shielding and type (A, B or C), businesses can ensure reliable performance even in the harshest conditions. 

Explore the full range of TKD Kabel through L-com. We’ll fill your orders fast, with same-day shipping on all qualified, in stock, online orders received Monday through Friday before 5 p.m. EST. For TKD-related inquiries, connect with our U.S-based TKD expert Eileen Harvey at eharvey@infiniteelectronics.com. 

Resources

Search Entries