L-com

Difference Between Flexible vs. Rigid Control Cables

By Eileen Harvey 

Control cables are essential components in numerous applications, ranging from automotive and aerospace to industrial machinery and consumer electronics. Understanding the fundamental differences between flexible and rigid control cables is crucial for engineers and project managers tasked with selecting the right materials for their specific needs.

TKD Flexible control cables are designed to withstand repeated bending and movement, making them ideal for dynamic environments where flexibility and adaptability are paramount. Conversely, rigid control cables offer enhanced strength and stability, suited for applications requiring less motion and greater structural integrity.

Whether you're involved in product design or system integration, grasping the nuances between flexible and rigid control cables is essential for optimizing performance in your projects.

What Are Control Cables?

Control cables are multi-conductor cables designed to transmit signals or low-voltage power in automation, machinery and industrial systems. They are used to connect sensors, relays, motors and controllers, ensuring smooth communication and control.

Depending on how they are built, control cables fall into two main categories. Flexible control cables are designed for continuous motion and bending. Rigid control cables are designed for fixed installations with minimal or no movement.

What Are Flexible Control Cables?

Flexible control cables, commonly referred to as continuous flex cables, are engineered specifically to endure the rigors of constant bending, twisting and movement. Unlike traditional cables that may suffer from wear and tear under dynamic conditions, these cables are constructed with advanced materials and innovative design features that enhance their durability and performance. The ability to withstand repetitive motion makes them ideal for applications in various industries, including robotics, where precise and reliable control is essential.

Key Features of Flexible Control Cables

These cables are made of stranded copper conductors for maximum flexibility. Jacket materials like PUR or TPE provide durability in motion-heavy environments. They can withstand millions of bending cycles without damage. They are often shielded to reduce electromagnetic interference in industrial automation. And they are resistant to oils, chemicals, abrasion and temperature fluctuations.

Advantages of Flexible Control Cables

Let’s consider four key advantages. First, they are designed for dynamic movement. Second, they are long-lasting in robotic and automated applications. Third, flexible control cables resist harsh environments (oil, chemicals, UV). And fourth, they reduce cable fatigue and breakage.

Applications of Flexible Control Cables

Four popular applications for flex control cables are robotics and automated machinery, conveyor systems, CNC machines, moving components in assembly lines and renewable energy equipment, such as wind turbines.

What Are Rigid Control Cables?

Rigid control cables are specifically engineered for applications that require a permanent installation, where the cable is not intended to move after it has been set in place. These cables are constructed with a robust, inflexible design that ensures they can withstand environmental factors and physical stress without compromising their functionality. Commonly utilized in control panels and distribution boards, rigid control cables provide a reliable means of transmitting electrical signals and power.

Key Features of Rigid Control Cables

These cables are typically made of solid copper conductors or larger-gauge wires. They are less flexible than stranded designs. They are optimized for long-term stability and durability in fixed setups. Rigid control cables are generally more cost-effective than flexible cables. Their common insulation materials are PVC, XLPE or PE.

Applications of Rigid Control Cables

They are commonly used for fixed wiring in control panels, power distribution in industrial facilities, building wiring systems and static electrical connections with no movement.

Advantages of Rigid Control Cables

Their advantages include that they are ideal for permanent installations with no movement, they are more cost-effective for large-scale wiring projects, they are easier to terminate in panels and fixed equipment, and they exhibit stable performance in controlled environments.

Limitations of Each Cable

Neither type of cable is perfect for everything. Flexible control cables have a higher initial cost and may require specialized installation practices. Rigid control cables cannot handle movement; bending or twisting over time may lead to breakage.

Which One Should You Choose?

The choice between flexible and rigid control cables depends on application needs. Choose flexible control cables if the cable will be installed in moving machinery, it must handle continuous bending or twisting, and/or the environment involves oil, abrasion or temperature fluctuations. Choose rigid control cables if the cable will remain fixed after installation, cost efficiency is a top priority, and it’s used in panels, distribution boards or building wiring.

Why Multi-Conductor Flexible Control Cables Are Preferred in Automation

In highly automated industries, multi-conductor flexible control cables are the preferred choice. This is because they consolidate multiple signals into one compact cable, they can withstand millions of bending cycles without conductor failure, shielded options prevent interference in environments with variable frequency drives (VFDs) and motors, and their durability reduces downtime and maintenance costs.

Both flexible and rigid control cables play vital roles in industrial and electrical systems. Flexible control cables shine in dynamic, motion-heavy applications, while rigid control cables are best for stationary, cost-effective installations.

For industries relying on automation and robotics, multi-conductor TKD flexible control cables provide the reliability, flexibility and safety required for uninterrupted operations.

By understanding the differences between flexible vs. rigid control cables, you can select the best option to improve performance, reduce downtime and maximize efficiency in your system.

Resources

Search Entries