L-com

Can You Use Tray Cables in Residential Wiring?

By Eileen Harvey 

Tray cables have established a strong reputation in industrial and commercial settings due to their durability and robust construction. Designed to withstand demanding electrical environments, they are typically used where exposure to harsh conditions is expected, such as in cable trays, raceways and other protective conduits. However, as electrical codes evolve and new certifications emerge, homeowners, electricians and builders are showing greater interest in using tray cables for residential wiring. 

But can tray cables be used effectively in residential wiring? This inquiry is not without merit, as the electrical landscape continually adapts to meet modern demands for safety and efficiency. Understanding the updated standards is essential for anyone considering the use of tray cables in a residential context. 

This article explores the latest code guidelines, including the National Electrical Code (NEC) provisions that govern the use of these cables. It also highlights some practical applications that may be suitable for residential environments. 

What Are Tray Cables? 

Tray cables (type TC) are multi-conductor cables that serve various functions, including power distribution, lighting, control systems and signal transmission. They are notable for their robust construction, featuring thick insulation that ensures electrical safety and performance in demanding environments. Their outer jackets are typically crafted from durable materials such as polyvinyl chloride (PVC), cross-linked polyethylene (XLPE) or other advanced polymers.  

These materials provide exceptional resistance to oil, chemicals, temperature fluctuations and ultraviolet (UV) radiation, thereby extending the lifespan of the cables and ensuring reliable operation in diverse conditions. Tray cables are available in both shielded and unshielded variants, catering to different application needs, and are rated for either 600 volts for standard types or 300 volts for power-limited tray cables (PLTC). 

Updates to Residential Wiring Codes 

Historically, tray cables have been subject to stringent restrictions when it comes to general residential wiring, primarily due to preferences outlined in residential codes such as the National Electrical Code® (NEC) in the U.S. Traditionally, nonmetallic-sheathed cable (commonly referred to as NM-B or Romex) and underground feeder (UF) cable were favored for residential applications due to their safety and ease of installation. 

These codes were established to promote wiring methods that provide robust protection against environmental factors and mechanical damage, thereby minimizing the risk of electrical hazards in residential settings. As a result, tray cables were largely overlooked in the context of home wiring, which led to limited options for contractors and builders seeking flexibility in their wiring solutions. 

Where Can You Use Tray Cables in a Home? 

Type TC-ER-JP tray cable has several main uses in a home: 

For interior wiring, the cable may be installed following the same requirements as NM-B (Romex), such as between framing members, through studs or above ceilings. NEC Article 334 governs proper support, securing and protection. 

For exterior wiring, the cable can be used where UF-B (underground feeder) cable is allowed, such as outdoor branch circuits, outbuildings and exterior lighting. NEC Article 340 covers these applications. 

For high-quality, NEC-compliant tray cables, you can explore the TKD Tray Cable collection which includes TC-ER-JP-rated options suitable for residential applications. 

Application Examples 

These include running power to detached garages or sheds; outdoor lighting systems; electrical feeds to HVAC units; and certain home automation or alarm circuits. 

Always check local code amendments, as some jurisdictions may not yet have adopted the latest NEC edition or may have additional rules. 

Benefits of Tray Cables in Residential Settings 

Tray cables bring together ruggedness, versatility, performance and ease of installation in one solution. Their thicker jackets and tough insulation provide enhanced resistance to nicks, rodents and mechanical stress, ensuring reliable protection in demanding environments. They are equally at home indoors or outdoors and are flexible enough to allow easier routing around obstacles. 

Beyond durability and flexibility, tray cables often support higher current loads and longer runs than traditional NM-B cables, giving them higher ampacity. Installation is also simplified in many cases: for exposed runs in garages, basements or attics, TC-ER-JP cables can often be installed without conduit, provided they meet code requirements. 

Limitations and Safety Considerations 

  • Only TC-ER-JP cables are approved for these residential uses—other tray cable types are not. 

  • Cost: Tray cables tend to be more expensive and bulkier than NM-B or UF cable. 

  • Installation rules: Must be installed in compliance with the requirements for NM-B (indoor) or UF-B (outdoor). For example, in attics, basements, and crawl spaces, cables must be stapled and protected as specified by the NEC. 

  • Compatibility: Tray cable may not fit standard residential boxes/connectors without adapters. 

  • Inspection: Home inspectors may flag unconventional cable if not familiar with the latest code; always provide documentation. 

 

Installation Tips 

  • Always read and follow manufacturer instructions. 

  • Ensure cable type (TC-ER-JP) is listed on the jacket. 

  • Follow NEC Article 334 for indoor installations and Article 340 for outdoor. 

  • Secure cables using appropriate staples/supports per code. 

  • When used outdoors, check for UV resistance or a black outer jacket. 

Frequently Asked Questions (FAQs) 

Q1: Can I use standard tray cable (TC) in my home? 
A: No. Only tray cable marked TC-ER-JP is allowed in residential settings by NEC Article 336.10(9). Regular TC or TC-ER without the JP designation is not permitted for dwelling unit wiring. 

Q2: Do I need a conduit to use tray cable in my house? 
A: Not necessarily. TC-ER-JP tray cables may be installed without conduit in certain exposed runs, as long as all other code requirements (support, protection, routing) are met. However, local code or specific applications may still require conduit. 

Q3: What’s the difference between TC-ER and TC-ER-JP? 
A: TC-ER cables are rated for exposed runs (ER), but only TC-ER-JP cables are approved for joist pulls and residential use without a tray system, per the NEC. 

Q4: Are tray cables more durable than NM-B or UF cable? 
A: Yes. They are generally more rugged, with thicker insulation and outer jackets, making them ideal for demanding conditions, including garages, sheds and outdoors. 

Tray cables, specifically those designated as type TC-ER-JP, have been permitted for use in residential wiring since 2017, according to the National Electrical Code (NEC). This advancement reflects an increasing recognition of the advantages these cables offer in terms of durability and adaptability for a variety of home electrical projects, both inside and outside the residence. 

However, it is crucial for homeowners and contractors alike to adhere strictly to the guidelines set forth in the NEC when selecting and installing tray cables. Ensuring the correct type of TC cable is employed is paramount, as is familiarizing oneself with all applicable installation codes, which can vary by locality. 

Related Products: 

Resources

Search Entries