L-com

Applications in Robotics, Motion Control and Packaging Machines

By Eileen Harvey 

Modern manufacturing is going through one of the most transformative eras in history. From robots assembling cars with flawless precision, to packaging machines that process thousands of products per hour, automation has become the heartbeat of industrial efficiency. At the core of these innovations are high-performance cabling and connectivity solutions that power, control and transmit critical data across systems. 

Industries like automotive, pharmaceuticals, food and beverage, and logistics rely heavily on reliable cables that can handle high speeds, mechanical stress and environmental challenges. Whether it’s robotics, motion control or packaging machinery, the backbone of success lies in robust cabling solutions designed specifically for industrial applications. 

Applications in Robotics 

Robotics in Modern Industries: Robotics has become an integral part of modern manufacturing and automation, enabling faster, more precise and more consistent performance than manual labor. Industrial robots are commonly deployed in a wide range of sectors, including automotive assembly lines where they handle welding, painting and component positioning with high accuracy. In electronics manufacturing, robots manage delicate processes such as printed circuit board (PCB) assembly and micro-soldering. In healthcare and pharmaceutical industries, robotic systems assist in surgery, drug packaging and sterile material handling, ensuring accuracy and hygiene in sensitive environments. 

Cable Requirements for Robotics: The demanding motion and precision of robotic systems place extreme requirements on cable performance. Cables must endure continuous torsional stress as robotic arms twist and pivot during operation, while also resisting abrasion, oils and chemical exposure in industrial settings. They must preserve signal integrity even under constant movement, preventing data loss or interference that could disrupt automated processes. TKD Kabel solutions excel in these conditions, as they are purpose-built for dynamic motion with high flexibility, strong EMI shielding and long-lasting materials that maintain reliability through millions of motion cycles. 

Applications in Motion Control 

What is Motion Control? Motion control technology enables machines to move with precision and coordination using servo motors, drives and feedback systems. It is essential to applications that require synchronized or repeatable motion, such as CNC machines used for metal cutting, conveyor systems in logistics and manufacturing, and automated storage and retrieval systems that enhance efficiency in warehouses and production facilities. 

Cable Needs for Motion Control Systems: Cables in motion control applications must transmit high-frequency signals without distortion to ensure accurate, real-time feedback. They also require effective electromagnetic shielding to prevent signal interference from surrounding equipment. Additionally, the cables must possess strong mechanical durability to withstand continuous bending and flexing in dynamic installations. Industrial-grade PROFINET Ethernet cables meet these needs by providing the stability, shielding and performance necessary for reliable motion control in demanding automated environments. 

Applications in Packaging Machines 

Why Packaging Machines Matter: In industries such as food and beverage or pharmaceuticals, automated packaging machines play a vital role in maintaining safety, hygiene and efficiency. These systems can seal thousands of units per hour while performing carton forming, labeling and filling tasks with exceptional precision and minimal human intervention. Automation in packaging not only increases production speed but also reduces contamination risk, ensuring compliance with stringent safety and quality standards. 

Cable Demands in Packaging Environments: Cables used in packaging machines must be flexible enough to endure continuous motion cycles while maintaining mechanical integrity. They must also resist cleaning agents and moisture and meet food-safe compliance requirements. In addition, UV and flame retardancy are essential for operation in harsh industrial conditions. Products such as the PROFINET Category 5e Type A Solid Double Shielded Cable are specifically engineered for packaging environments, offering superior shielding and high data integrity to ensure uninterrupted performance and long-term reliability. 

Benefits of Reliable Cabling in Robotics, Motion Control and Packaging 

  • Reduced Downtime – Preventing cable failures minimizes costly production halts. 
  • Enhanced Safety – Flame-retardant and chemical-resistant cables protect operators and equipment. 
  • High-Speed Data – Shielded cables ensure uninterrupted signal transmission. 
  • Cost Efficiency – Long-lasting cables reduce replacement and maintenance expenses. 

Industry Standards and Certifications 

When choosing cables, compliance matters. Look for UL and CE certification for safety, IEC standards for industrial environments, food and pharma compliance for packaging lines, and UV and flame resistance ratings for outdoor and high-heat environments. 

Future Trends 

Let’s glance at four future trends. First is collaborative robots (cobots), which are designed to work alongside humans. Second is IoT-enabled packaging machines, which monitor uptime and predictive maintenance. A third future trend is AI-driven motion control for near-zero error margins. And fourth is next-gen cabling, which is designed for Industry 4.0 and IIoT environments with higher bandwidth. 

Tips and Recommendations 

  • Always choose cables with proper shielding for data-critical applications. 
  • For robotics, select torsion-rated cables to avoid early wear. 
  • For packaging lines, consider PUR jacketed cables for chemical resistance. 
  • Plan for scalability—future-proof your cabling with Cat5e/6 PROFINET solutions. 
  • Inspect cables regularly to catch small wear issues before they cause downtime. 

FAQs About Robotics, Motion Control and Packaging Machines 

 

Q1: What type of cables are best for robotics applications? 
A: Cables with high flexibility, torsion resistance and EMI shielding are best. TKD Kabel is a strong choice. 

Q2: Why is shielding important in motion control cables? 
A: Shielding prevents EMI to ensure precision and reliability in high-frequency motion systems. 

Q3: Are specialized cables necessary for packaging machines? 
A: Yes. Packaging machines require cables resistant to chemicals, cleaning agents and constant bending. 

Q4: Which industries benefit most from these applications? 
A: Automotive, food and beverage, pharmaceuticals, logistics and electronics manufacturing. 

Robotics, motion control and packaging machines form the foundation of modern industrial automation. But their performance and reliability are only as good as the cabling that connects them. By investing in certified, industrial-grade solutions like TKD Kabel and PROFINET cables from L-com, businesses can safeguard uptime, improve efficiency and prepare for the future of Industry 4.0. 

Explore the full range of TKD Kabel through L-com. We’ll fill your orders fast, with same-day shipping on all qualified, in stock, online orders received Monday through Friday before 5 p.m. EST. For TKD-related inquiries, connect with our U.S-based TKD expert Eileen Harvey at eharvey@infiniteelectronics.com. 

 

Resources

Search Entries