L-com

Mitigating Receiver Desensitization (Desense) in UAV Comms

By Santos Lopez 

UAV communication systems often operate in tightly integrated environments where multiple RF systems share limited space. While this compact design supports efficiency, it also introduces a critical challenge: receiver desensitization (desense). 

Receiver desensitization occurs when high-power onboard transmitters interfere with nearby receivers, reducing their ability to detect weaker signals. This issue can compromise command and control (C2) links, even when signal strength appears sufficient. 

To maintain reliable communication, engineers must manage signal levels, minimize interference and protect sensitive receiver components. Techniques such as controlled attenuation and proper cable shielding play a key role in mitigating desense and improving overall RF performance. 

Key Takeaways 

  • Receiver desense occurs when strong onboard signals overwhelm nearby receivers 
  • Desense can reduce range, increase packet loss and degrade link reliability 
  • Fixed attenuators help maintain signals within a receiver’s linear operating range 
  • Shielded cable assemblies prevent internal RF leakage between components 
  • Proper RF design improves signal-to-noise ratio and communication stability 

Understanding Receiver Desensitization (Desense) 

Receiver desensitization is caused by excessive RF energy entering the front end of a receiver. When a nearby transmitter emits a strong signal, it can overload the receiver’s low noise amplifier (LNA), reducing its sensitivity to incoming signals. 

In this state, the receiver is not damaged but becomes less effective at detecting weaker signals. This results in reduced communication range, intermittent signal loss and degraded data performance. 

Desense can be particularly difficult to diagnose because systems may appear to have strong signal levels while still experiencing communication issues. 

Why Desense Is a Major Risk in UAV Systems 

UAV platforms often have limited physical space, which forces RF components to operate in close proximity. Transmitters for video, telemetry and data links may be located near command and control receivers, increasing the risk of interference. 

In addition to direct signal coupling, broadband interference and harmonic emissions from transmitters can further degrade receiver performance. These unwanted signals can overlap with or distort the desired communication frequencies. 

Because UAV systems rely on stable RF links for safe operation, managing these interference sources is essential. 

Implementing Fixed Attenuators for Signal Control 

One effective method for reducing desense is the use of fixed attenuators. These components reduce signal power to ensure that receivers operate within their optimal dynamic range. 

A fixed attenuator provides a controlled reduction in signal strength, preventing the receiver from becoming overloaded. This helps maintain linear operation and improves the receiver’s ability to detect weaker signals. 

The key is finding the correct level of attenuation. Too little attenuation may not prevent desense, while too much can reduce overall signal strength. Engineers must balance these factors to maintain reliable communication. 

How High-Performance Cables Prevent Signal Leakage 

In addition to controlling signal levels, preventing RF leakage within the system is critical. 

Standard cable assemblies can act as unintended antennas, allowing RF energy to escape and couple into nearby components. This internal leakage can bypass intended signal paths and contribute to desense. 

High-performance, double-shielded cable assemblies help contain RF signals within the intended transmission path. By minimizing leakage, these cables reduce interference between transmit and receive systems. 

Maintaining proper shielding ensures that signals travel only through the designed RF chain, preserving system integrity. 

Practical Steps for RF Hardening 

Mitigating desense requires a system-level approach. Engineers must consider component placement, signal levels and shielding when designing UAV communication systems. 

Increasing physical separation between transmitters and receivers can reduce interference, but space constraints often limit this option. In these cases, attenuation and shielding become even more important. 

Testing is also critical. Measuring signal strength, noise floor and receiver sensitivity under full-power operation helps identify potential desense issues before deployment. 

By combining careful design with thorough validation, engineers can significantly improve communication reliability. 

Improving UAV Communication Reliability by Controlling RF Interference 

Receiver desensitization is a common but manageable challenge in UAV communication systems. By controlling signal levels and preventing internal interference, engineers can maintain receiver sensitivity and ensure stable command and control links. 

Using fixed attenuation and properly shielded cabling helps protect critical RF components and improve overall system performance, even in compact and high-power environments. 

L-com’s broad selection of wireless connectivity and networking solutions supports reliable UAV communications in demanding environments. For minimal downtime and rapid deployment, we ship quickly, with same-day shipping on qualified in-stock online orders placed Monday through Friday before 5 p.m. EST. 

View L-com UAV solutions 

Frequently Asked Questions 

What is receiver desense in a UAV system? 
Receiver desense occurs when a strong signal from a nearby transmitter overwhelms a receiver, reducing its ability to detect weaker signals. 

Why would reducing signal strength improve performance? 
If a signal is too strong, it can overload the receiver and cause distortion. Controlled attenuation keeps the signal within a usable range, improving reliability. 

Can increasing antenna separation solve desense? 
Physical separation helps, but space constraints in UAV systems often limit its effectiveness. Additional measures such as attenuation and shielding are typically required. 

Will using an attenuator reduce communication range? 
In some cases, attenuation can improve effective range by preventing receiver overload and lowering the noise floor, allowing weaker signals to be detected more reliably.

Resources

Search Entries