L-com

Fiber Optics vs. Copper in High-EW Environments

By Santos Lopez

Unmanned aerial vehicles operating in contested environments must maintain reliable data transmission despite intense electromagnetic interference. Electronic warfare (EW) systems are specifically designed to disrupt communications, making internal networking a critical vulnerability. 

Traditional copper-based cabling has long been the standard for RF and data transmission. However, in high-EW environments, these systems can be susceptible to interference, signal degradation and data loss. 

Fiber optics offer an alternative approach. By transmitting data using light instead of electrical signals, fiber eliminates many of the vulnerabilities associated with copper, providing a more resilient solution for high-interference environments. 

Key Takeaways 

  • Fiber optics are immune to electromagnetic interference and RF jamming 
  • Copper cables can act as unintended antennas in high-noise environments 
  • Shielded copper remains essential for RF signal delivery to antennas 
  • Hybrid architectures combine the strengths of fiber and copper 
  • Fiber optics can reduce weight and improve system efficiency 

Why Copper Networks Struggle in High-EW Environments 

Copper cabling relies on electrical signals, which makes it inherently vulnerable to electromagnetic interference. In high-EW environments, powerful transmitters can induce unwanted currents in cables, disrupting signal integrity. 

Even well-shielded cables can experience interference under extreme conditions. High-frequency energy can penetrate shielding or couple into the system through connectors and grounding paths. 

Additionally, long copper runs can act as antennas, capturing ambient RF energy and introducing noise into the system. This can lead to data corruption, increased error rates and reduced communication reliability. 

Understanding these limitations is essential when designing systems for contested environments. 

Fiber Optics as an EMI-Resistant Solution 

Fiber optic systems transmit data using light pulses, which are unaffected by electromagnetic fields. This makes them inherently immune to RF interference and jamming. 

Because fiber does not conduct electricity, it eliminates the risk of induced currents and ground loops. This provides a stable communication pathway even in the presence of high-power electronic warfare systems. 

Fiber optics also offer high bandwidth capabilities, supporting large volumes of data without degradation. This is particularly important for applications such as high-resolution imaging and real-time data processing. 

These characteristics make fiber an effective solution for maintaining reliable communication in challenging environments. 

The Role of Shielded Copper in RF Systems 

While fiber optics provide advantages for internal data transmission, copper remains essential for RF signal delivery. 

Connections between radios and antennas require coaxial cables designed to carry RF signals efficiently. High-performance, shielded coaxial assemblies help minimize signal loss and protect against interference. 

These cables are optimized for maintaining signal integrity over short distances, making them a critical component of the overall RF system. 

In many cases, copper and fiber are used together to achieve optimal performance. 

Designing a Hybrid Network Architecture 

Combining fiber optics and copper creates a hybrid architecture that leverages the strengths of both technologies. 

Fiber can be used for long internal data runs, where immunity to interference is most important. Copper can be reserved for short connections where RF transmission is required. 

Media converters allow data to transition between optical and electrical formats as needed. Strategic placement of these components helps maintain efficiency and minimize complexity. 

This approach provides a balanced solution that supports both performance and resilience. 

Durability and Deployment Considerations 

Modern fiber optic systems are designed for durability in demanding environments. Reinforced cables and rugged connectors improve resistance to vibration, shock and environmental exposure. 

While fiber requires different handling and repair techniques compared to copper, advances in field-ready solutions have made it more practical for tactical use. 

Copper systems remain easier to repair in some scenarios, but fiber offers advantages in long-term reliability and resistance to interference. 

Selecting the appropriate technology depends on mission requirements and operational conditions. 

Building Resilient UAV Networks in Contested Environments 

Maintaining reliable communication in high-EW environments requires a strategic approach to system design. 

By understanding the strengths and limitations of both fiber optics and copper, engineers can develop network architectures that withstand interference and maintain data integrity. 

Using fiber for internal data transmission and shielded copper for RF connections provides a robust solution for modern UAV systems. 

L-com’s broad selection of wireless connectivity and networking solutions supports reliable UAV communications in demanding environments. For minimal downtime and rapid deployment, we ship quickly, with same-day shipping on qualified in-stock online orders placed Monday through Friday before 5 p.m. EST. 

View L-com UAV solutions 

Frequently Asked Questions 

Why are fiber optics better in high-EW environments? 
Fiber optics transmit data using light, making them immune to electromagnetic interference and RF jamming. 

Can shielded copper cables still be used in contested environments? 
Yes. High-quality shielded cables can reduce interference, but they are not completely immune in extreme conditions. 

Why use both fiber and copper in UAV systems? 
Fiber is ideal for internal data transmission, while copper is necessary for RF connections between radios and antennas. 

Are fiber optic systems durable enough for UAV applications? 
Yes. Modern fiber systems are designed to withstand vibration, shock and environmental stress when properly installed.

Resources

Search Entries