L-com

Cable Jacket Materials: PVC vs. PUR vs. TPE – Which is Best?

When you're selecting a cable for industrial, automation or everyday use, its jacket material plays a crucial role. A cable's jacket doesn't just protect the internal conductors; it determines the cable's durability, flexibility, chemical resistance and overall performance in the environment it's built for.

PVC remains the industry default: affordable, easy to install and reliable for static, indoor use. PUR is known for its flexibility, abrasion resistance and resilience in harsh, high-motion environments, making it a go-to for robotics and automation. TPE blends the properties of rubber and plastic, offering elasticity, a wide temperature range and eco-friendly performance for outdoor and safety-sensitive applications.

So how do you know which one is right for your application? Let's look at the trade-offs that matter.

 

Key Takeaways

  • PVC is the most cost-effective and widely used jacket material but has limited flexibility in cold or continuous-motion applications.
  • PUR offers superior abrasion, oil and chemical resistance, making it a common choice for robotics and drag-chain applications.
  • TPE combines flexibility with good chemical resistance, sitting between PVC and PUR on cost and performance.
  • Material choice should be driven by the operating environment — temperature range, chemical exposure and flex requirements — not cost alone.

 

Overview of Cable Jacket Materials

Cable jackets serve as the first line of defense against external stress factors such as moisture, oil, abrasion, UV exposure and mechanical wear. The choice of jacket material can make the difference between a cable lasting a few months or several years in a demanding environment.

The three most popular materials in industrial and control cable jacket design are PVC, PUR and TPE:

  • PVC (polyvinyl chloride) is affordable and versatile, widely used for general applications.
  • PUR (polyurethane) is highly flexible and resistant to abrasion, ideal for robotic and motion control cables.
  • TPE (thermoplastic elastomer) is eco-friendly, chemical-resistant and suitable for harsh environments.

Here's a quick side-by-side before we break down each material in detail.

 

At a Glance: PVC vs. PUR vs. TPE

PropertyPVCPURTPE
Flexibility Moderate — best for static/light-flexing use High — built for continuous motion and tight bend radii High — performs well in static and dynamic use
Chemical resistance Moderate resistance to oils, acids and alkalis Strong resistance to oils, greases and solvents Strong resistance to chemicals and UV
Temperature range Approx. −10°C to +70°C Good flexibility across a wide range; can stiffen at very low temps Approx. −50°C to +125°C (blend-dependent)
Typical cost Lowest Higher Higher
Best for General-purpose, indoor, static wiring Robotics, drag chains, high-motion industrial use Outdoor, eco-conscious, fire-safety-sensitive applications

 

Properties of PVC Cable Jackets

For general-purpose wiring, PVC is often the starting point. Its low cost, ease of processing and wide availability make it one of the most commonly used cable jacket materials. Here's what it offers:

  1. Cost-effective — affordable compared to PUR and TPE, making it ideal for general-purpose cables.
  2. Good insulation properties — provides reliable electrical insulation.
  3. Moderate flexibility — suitable for static and light-flexing applications.
  4. Chemical resistance — resists oils, acids and alkalis to some extent.

PVC Cable Jacket Applications

PVC jackets are commonly used in data cables, control cables and household wiring, where flexibility is not a primary concern. For example, industrial Ethernet cables often use PVC for indoor installations — see our guide to choosing the right industrial Ethernet cable for more on matching cable type to environment.

PVC Cable Jacket Limitations

PVC has three notable limitations:

  1. It is not highly resistant to abrasion.
  2. It has limited performance in extreme temperatures (typically −10°C to +70°C).
  3. It can release toxic fumes when burned, making it less suitable for certain safety-sensitive environments.

But when cables face constant motion or abrasion, PVC's limits are exactly where PUR was designed to take over.

 

Advantages of PUR Cable Jackets

PUR (polyurethane) brings mechanical toughness and flexibility to applications where cables keep moving, such as robotics, conveyor systems and drag chain installations. Its four main advantages are:

  1. Superior abrasion resistance — ideal for environments where cables are dragged or moved frequently.
  2. High flexibility — perfect for continuous motion and tight bending radii.
  3. Oil and chemical resistance — performs well in industrial settings with oils, greases and solvents.
  4. Tear-resistant — offers enhanced durability in demanding conditions.

PUR Cable Jacket Applications

PUR jackets are widely used in robotics, automation and machine tools. For example, robotic cables and control cables in manufacturing plants often feature PUR jackets for an extended lifespan. L-com's industrial-grade cables are designed for demanding motion control environments.

PUR Cable Jacket Limitations

PUR's three main limitations are:

  1. It is more expensive than PVC.
  2. It is sensitive to hydrolysis in very humid conditions unless specially treated.
  3. It can be stiffer compared to TPE in very low temperatures.

If PUR's higher cost or humidity sensitivity rules it out, TPE is another option to consider, especially outdoors.

 

Benefits of TPE Cable Jackets

TPE (thermoplastic elastomer) combines the properties of plastics and rubber, giving you a versatile and environmentally friendly option. It's becoming more popular in cable design for five key reasons:

  1. Wide temperature range — performs in both hot and cold environments (−50°C to +125°C depending on the blend).
  2. Eco-friendly — halogen-free and recyclable, making it a greener choice than PVC.
  3. Excellent flexibility — maintains performance in both static and dynamic applications.
  4. Chemical and UV resistance — suitable for outdoor and industrial use.
  5. Low smoke emission — safer in fire situations compared to PVC.

TPE Cable Jacket Applications

TPE jackets are used in medical devices, renewable energy, outdoor equipment and automation systems where environmental safety and flexibility are important.

TPE Cable Jacket Limitations

TPE's two main limitations are:

  1. Higher cost compared to PVC.
  2. Less abrasion-resistant than PUR.

With all three materials on the table, here's how to turn these trade-offs into an actual decision.

 

Choosing the Right Material

To choose between PVC, PUR and TPE cable jacket materials, start with these four factors:

  1. Application environment — PVC is best indoors and under low stress. PUR is good for high-motion, robotic and abrasive environments. TPE excels outdoors and is eco-friendly and chemical resistant. If you're weighing cable types for a facility upgrade, our guide on choosing the right industrial Ethernet cable covers related environmental considerations.
  2. Flexibility needs — PVC is best for static wiring, while PUR and TPE suit continuous movement.
  3. Budget considerations — PVC suits cost-sensitive projects. PUR and TPE are best for long-term reliability and performance.
  4. Safety and compliance — TPE is best when there are fire safety and halogen-free requirements.

Once you've narrowed down a material, these practical checks help you avoid costly mistakes during selection and installation.

 

Tips for Selecting the Right Cable Jacket

  • Check the datasheet. Always check the manufacturer's datasheet for temperature, chemical resistance and flexibility ratings.
  • Match material to motion type. If your system involves constant bending or drag chains, avoid PVC.
  • Plan for the environment. Outdoor applications need UV- and weather-resistant materials like PUR or TPE.
  • Think long-term. While PUR and TPE cost more, they often reduce replacement and downtime costs.
  • Consider bus and industrial applications. Many industrial control systems rely on bus cable applications where jacket material directly affects reliability and lifespan.
  • Consult experts. Distributors like L-com provide detailed specifications for different cable types.

Choosing the right jacket deserves the same care as choosing the conductor or insulation. Start with where your cable will run, how much it needs to flex and which safety requirements it must meet. Those checks will help you find the right fit among PVC, PUR and TPE.

Still have questions? Here are answers to help you make your choice.

 

FAQ

What is the difference between PVC, PUR and TPE cable jackets?

PVC is a low-cost, moderately flexible material best suited to static, indoor use. PUR is a tougher, highly flexible material built for continuous motion and abrasion resistance. TPE combines flexibility, a wide temperature range and eco-friendly properties, making it well suited to outdoor and safety-sensitive applications.

Which cable jacket material is most flexible?

PUR and TPE both offer high flexibility and are suited to continuous-motion applications, with PUR generally preferred for tight bending radii and repetitive movement, and TPE offering strong flexibility across a wider temperature range.

Is PUR or PVC better for outdoor use?

PUR generally performs better outdoors than PVC thanks to its abrasion, oil and chemical resistance, though TPE is often the stronger overall choice outdoors due to its UV resistance and wide operating temperature range.

What cable jacket material is best for robotics applications?

PUR is the most common choice for robotics and drag-chain applications because of its superior abrasion resistance, tear resistance and ability to withstand continuous flexing.

 

Read Next

Resources

Search Entries