L-com

Wireless Antenna and Access Point Mounting Options Overview

Download the Full Whitepaper (PDF)

Executive Summary

Key Takeaways:

  • Antenna and access point mounting play a critical role in wireless network performance and coverage.
  • Common mounting options include ceiling, wall, pole, and mast installations, each suited to different environments.
  • Ceiling-mounted access points provide more uniform and centralized coverage, especially in indoor environments.
  • Wall mounting is useful in specific layouts or when ceiling installation is impractical.
  • Outdoor deployments typically rely on pole or wall mounts to maximize signal propagation.
  • Proper height, orientation, and placement reduce interference, dead zones, and signal loss.
  • Environmental factors like metal structures, walls, and electronic interference significantly impact performance.

Introduction

This paper details different antenna mounting options which are available for Directional and Omni directional antennas. The paper describes common installation options for antennas and wireless access points.

NEMA Enclosure Mounting

For mounting an antenna to a NEMA enclosure, a typical configuration includes running a pigtail cable from the access point or radio to a bulkhead N-female adapter or coax lightning protector. Outside of the enclosure directly attach the antenna to the adapter or lightning protector. (This mounting scenario utilizes HGV series or outdoor rated rubber duck style antennas.)

Antenna directly attached to a bulkhead adapter on a NEMA enclosure

For remote mounting of antennas, cables can be connected to the bulkhead adapters on the NEMA enclosure then directly to the antenna or to a surge protector attached to the antenna.

Antenna remotely mounted and cabled to a NEMA enclosure bulkhead adapter

Recommendations

To optimize wireless antenna and access point performance:

  • Conduct a site survey before installation
  • Choose the right mounting type based on the environment (indoor vs outdoor)
  • Use ceiling mounts for general indoor coverage
  • Use pole or mast mounts for outdoor and long-range applications
  • Position equipment centrally and at an appropriate height
  • Avoid interference sources like metal structures and electrical equipment
  • Align antennas according to their radiation patterns

Pole Mounting

Most of L-com’s Omni directional antennas include a rugged clamp style mounting bracket which is ideal for pole mounting.

Omni directional antenna with clamp style pole mounting bracket

L-com’s sector style antennas include upper and lower articulated clamp mounts for pole mounting.

Sector antenna with upper and lower articulated clamp brackets on a pole

Yagi and Patch Style antennas utilize a tilt and swivel clamp mounting system. These mounting clamps are standard on all of L-com’s Yagi antennas and are included with most of our patch style antennas.

Yagi and patch antennas with tilt and swivel clamp mounting system

Side of Building Mounting

The HGX-UMOUNT can be used to mount antennas to the side of a building, roof parapet or even under the roof eaves of a building. The HGX-UMOUNT will work with our Omni, Panel/Patch and Yagi style antennas.

Omni and Panel antennas mounted to the side of a building with the HGX-UMOUNT

L-com’s Sector antennas can either be mounted to a pole, as mentioned previously, or to the side of a building or structure using two of the HGX-UMOUNT mounting brackets.

Sector antenna mounted to the side of a building with two HGX-UMOUNT brackets

Mobile Mounting

L-com offers several options for mobile mounting an antenna. The first option involves using an HMA3 Series magnetic mount with either an HGV series or outdoor rated Rubber duck antenna such as the HG2408UR-NM or HG2458-7RDR-NM.

HMA3 Series magnetic mount with a rubber duck style antenna

Another mobile mounting option uses the NMO style HMA1 series magnetic mount along with an antenna such as a HG2403UR-NMOW.

NMO style HMA1 series magnetic mount with antenna

One other option is to use a NMO bulkhead style mount such as the AXA-AMNFB. This mounting option would require a hole drilled through the vehicle body, an N Male connecting cable to the appropriate radio connector and an NMO antenna.

Exploded diagram of a NMO bulkhead style mount installed through a vehicle body
AXA-AMNFB NMO bulkhead style mount hardware

Additionally a CA-AM1RSPA010 mounting cable could be used in a mobile mounting application. These NMO cable mounts are available with multiple connector types on the other end of the assembly to accommodate any antenna interface.

CA-AM1RSPA010 NMO cable mount assembly

Window Mounting

For window mounting of Patch antennas we recommend the HGX-PMT08 suction cup mounting kit.

HGX-PMT08 suction cup mounting kit
Patch antenna mounted to a window with suction cups

Outdoor Access Point Mounting

Access points can either be pole mounted or wall mounted. The HGX-UMOUNT mounting bracket can be used for wall mounting and is compatible with many manufacturers’ access points.

Outdoor access point shown pole mounted and wall mounted

PoE injectors used with any outdoor access point need to be mounted in a dry location such as inside a shelter or building, or outside in a weatherproof NEMA enclosure.

PoE injector mounted inside a weatherproof NEMA enclosure

Read About Antenna and Access Point Mounting

Wireless antenna and access point mounting is not just a physical installation step—it is a core component of wireless network design. The right mounting strategy ensures better signal distribution, reduces interference, and enhances overall network performance.

By selecting appropriate mounting options and considering environmental factors, organizations can build reliable and high-performing wireless systems.

Frequently Asked Questions

A: Mounting directly affects how radio signals propagate. Poor placement can lead to weak signals, dead zones, and unreliable connectivity, even with high-quality equipment.

A: Ceiling-mounted access points distribute signals in a dome-shaped pattern, ensuring even coverage across the area below and minimizing dead zones.