L-com Global Connectivity
  
Cart is Empty
  
USA & Canada (800) 341-5266     International +1 (978) 682-6936

Print
What is the difference between VGA, SVGA and UXGA, and does L-com sell cables for each?

The terms VGA, SVGA, XGA, SXGA, UXGA etc., all relate to the resolution a monitor supports.

The video format is the same despite the different designations and as an example a UXGA monitor can Display resolutions from VGA all the way up to UXGA. In all cases they use the same HD15 connector (below images) and VGA and SVGA cabling.

Male HD15 Connector
HD15 Male Interface image
Female HD15 Connector
HD15 Female Interface image

Regardless of what resolution a Monitor or Video Card is able to support, they are commonly referred to as just being VGA, the naming conventions listed above never really caught on with the general public and thus even the most High End 3-D Graphics card from Companies like NVIDIA or ATI will have what they term a VGA port (in addition to a DVI port in many cases) even though the card may output resolutions greater than 1920 x 1440.

Some High End Monitors support resolutions up to 2048x1536 @ 79Hz, which is still part of the same Multisync format and is backwards compatible to lower resolutions. Most High End Monitor Manufacturers don't mention VGA, SVGA etc at all, they typically refer to Monitors as CRT's, LCD's or Plasma Displays and list the maximum resolution that they support and at what refresh rate.

The relationship is as follows:

*Legacy Resolutions no longer supported (included only for reference)
     
Description
Code Resolution
*(Color Graphics Adapter) CGA 320 x 200
*(Enhanced Graphics Adapter) EGA 640 x 350
     
(Video Graphics Array) VGA 640 x 480
(Super Video Graphics Array) SVGA 800 x 600
(High Definition Television 720i/p) HDTV 1280 x 720
(Extended Graphics Array) XGA 1024 x 768
(Wide Extended Graphics Array) WXGA 1366 x 768
(Super Extended Graphics Array) SXGA 1280 x 1024
(Super Extended Graphics Array+) SXGA+ 1400 x 1050
(Wide Super Extended Graphics Array) WSXGA 1600 x 1024
(Wide Super Extended Graphics Array+) WSXGA+ 1680 x 1050
(High Definition Television 1080i/p) HDTV 1920 x 1080
(Ultra Extended Graphics Array) UXGA 1600 x 1200
(Wide Ultra Extended Graphics Array) WUXGA 1920 x 1200
(Quad Extended Graphics Array) QXGA 2048 x 1536
(Quad Super Extended Graphics Array) QSXGA 2560 x 2048
(Wide Quad Super Extended Graphics Array) WQSXGA 3200 x 2048
(Quad Ultra Extended Graphics Array) QUXGA 3200 x 2400
(Wide Quad Ultra Extended Graphics Array) WQUXGA 3840 x 2400
(Hex Super Extended Graphics Array) HSXGA 5120 x 4096
(Wide Hex Super Extended Graphics Array) WHSXGA 6400 x 4096
(Hex Ultra Extended Graphics Array) HUXGA 6400 x 4800
(Wide Hex Ultra Extended Graphics Array) WHUXGA 7680 x 4800


Other Frequently Asked Questions:
 
Account Management Can I change my billing address?
How can I apply for a credit account?
How can I view my account and payment types and pricing information?
How do I change my communication preferences?
How do I change my password or password hint information?
How do I change my product interests?
How do I change my product use?
How do I request a packing slip?
How do I review my order history?
How do I track my order?
How do I view and manage my saved carts?
How do I view my item history?
What if I forgot my password?
What is your remittance address?
Who is my L-com contact?
Enclosures What does NEMA mean?
How do I ... How can I assemble the 4 wires onto CNUSB-A or CNUSB-B USB sockets? Do I need to solder these 4 wires or use crimp tool?
How do I find and download the free 2D Engineering Drawings on your products?
How do I split out two of the unused lines on my existing cat5 cable to add phone capability without pulling new lines in my building?
How do I use a flat panel monitor with a standard VGA connected computer?
L-com Policies How do I return a purchase?
Is L-com ISO certified?
What are your shipping and processing fees?
What are your terms and conditions?
What is L-com's Customer Service Pledge?
What is L-com's Minimum Order Quantity (MOQ) or Minimum Dollar Amount?
What is your privacy policy?
Ordering How do I track my order?
Is your website secure?
What if I have a question about my order?
What payment methods do you offer?
Product Applications Does part # MWP4BNK work for light switches or is this just for some type of computer/video equipment?
I want to connect two computers to one printer. Is there a connector or switch I can purchase to accomplish this task?
Is the SATA cable usable for a 2.5 inch standard Seagate Momentus 5400.2 hard drive?
Will either cables TFC6101 or TFCLS6001, stranded, shielded, 26 AWG, work with TDS8PC6 plug?
Will the TDC053 series and ECF504-8SK coupler work in a 100-Base-T RJ45 product application?
Product Information How do I look up an item by NIN or NSN?
I am seeking 4x4 handset couplers, or extension cords. Are they even available anywhere?
I need the connector's measurements for cable model DK238MM series because I have to put it into a 1/2" hole.
I need to get waterproof cable, connectors, or adapters. What does IP67 mean?
I want cable assemblies at a special length. How do I request custom length cables?
What are products that start with SP?
What is your part # for the RJ45 Keystone Jack (used with the MWP10 series)?
Coaxial Products Can you tell me the frequency range for the SMA/BNC (e.g. BA29, BA38) and SMA/SMA (e.g. BA23) adapters?
What does RG316/U mean?
What is an MCX Connector and what applications are MCX Connectors used in?
What is the difference between 75 Ohm and 50 Ohm coaxial cable and when should each one be used?
What is the difference between an SMB plug and SMB jack?
What is the difference between low loss coax cable and RG style coax cable?
Where can I get Low Loss coaxial cable for high-frequency applications and wireless systems?
Why is proper termination of coaxial connectors imperative?
D-Sub Products Are your Economy 25 Pin D-Sub Molded Cables (CSM series) pass-through cables?
Is the material that the SD121 Plastic D-Sub Hoods are made of (PBT) Polybutylene Terephthalate Glass filled Thermoplastic?
What is a DB9 Connector?
What is cable dia of CSMN25MF D-sub cables?
What is the CS2N Series Operating Temperature Range?
What is the current carrying capacity of your CS2N37MM-10 and CS2N37MM-15 cables?
What is the wire color code for L-com's D-Subminiature cables?
When the CSNULL9FF cables ship, do they come with dust caps on both ends?
Fiber Optic Products I downloaded your 3D model of your LC/LC Duplex Fiber Coupler. The As don’t line up with each other. The A on one end lines up with the B on the other end. Is this correct?
I have an existing copper infrastructure, what's the most cost-effective way to upgrade to fiber?
I'm trying to connect two male MTRJ connectors using the MTRJ fiber coupler part number FOA-600 and they won't work. What gender is the FOA-600 on each side?
Is fiber more difficult to install than copper?
Multimode, singlemode, laser optimized - What does it all mean?
What is the difference between simplex and duplex fiber optic cable?
What is the minimum bend radius for L-com model SFOSC fiber patch cords?
What is the MT-RJ connector? How does it work?
When I use the fiber configurator, I get items with a strange description like CA ST ST 50DX OFR OR 040 F. What does it mean?
Modular Products Can Cat 5E cabling be used in Gigabit Ethernet Applications?
How are your TRD855SIG-15 cables wired? Are they crossover?
I am trying to find something that looks like the TRD855SIG (double shield, zero halogen, CAT5e with RJ45 plugs) but with stranded conductors instead of solid (and preferably also AWG 26 if possible).
I need to know what the max material thickness your TDG1026KC6 couplers can fit in to.
I would like to know the crimp height and tolerance of a L-com Crimper P.N. HTS2500 using a TDS8PC5 Modular plug.
What is the conductor resistance per meter of TDB4 flat silver satin modular cable?
What is the difference between a shielded and unshielded modular coupler?
What is the minimum temperature rating for bulk cable TDB series?
What is the panel thickness of TDG1026KC5 modular couplers?
What is the recommended maximum panel thickness for our ECF style couplers with the metal flange?
What kind of shield does the RS series modular to d-sub adapter use?
What kinds of cables work in HDBaseT applications?
What type of keystone wall mounting styles are there?
Why is choosing the right type of cabling important for a network?
USB Products How can I find the USB cable for my camera on your website?
How do I connect a IEEE-1394 (Firewire) device to the USB port on my computer or laptop?
How fast is USB?
Is there a difference for 1.0 or 2.0 on ECF504B-UAB?
What is a USB cable?
What kinds of USB peripherals can I connect to my PC?
Video Products How do I convert VGA to S-Video?
I have a computer with a single video card and would like to connect 2 monitors, creating a dual-display to increase the area available for computer programs running on the computer. Is this something that is available?
What is a VGA cable?
What is Digital Signage and where is it used?
What is HDMI?
What is the max length of DVI cable assemblies?
What is the max length of HDMI cable assemblies?
Technology and Terminology Are there any maximum recommended lengths for CAT5/5E UTP, CAT5/5E STP, USB, 50 micron fiber or 62.5 micron fiber?
Can you please provide a table of minimum bend radius values that includes values for CAT5 UTP, CAT5E STP, USB, 50micron fiber optic and 62.5micron fiber optic cables?
Keystone connector dimensions
Minimum Lengths for Ethernet Cabling
Using PMOD4U-1 on a Cat5 Network?
We have a 100 megabit Ethernet network that is cabled with category-5 in our office...
What are the basic things a network consists of?
What is a PL-259 Plug and does L-Com carry any PL-259 products?
What is Cat5e plenum cable, and why is the plenum cable so much more expensive than PVC?
What is EIA232C?
What is the color code for SVGA Cable?
What is the difference between VGA, SVGA and UXGA, and does L-com sell cables for each?
Why Use Shielded Cat 6 Cable vs. Unshielded Cat 6 cable?
Wireless
How are bi-directional amplifiers used?
How do I choose the right WiFi amplifier?
How do I use a WiFi Antenna?
What Antennas are available?
What are common WiFi Antenna FAQs?
What are the key requirements of bi-directional amplifiers for use with the new high data rate 802.11a/g/n radios?
What are the uses of lightning protectors?
What is a Ceiling Mount WiFi Antenna?
What is a Distributed Antenna System (DAS)?
What is a High Gain WiFi Antenna?
What is a MIMO Antenna?
What is a Wireless Repeater?
What is a Yagi Antenna?
What is an Outdoor CPE?
What is Polarity?
What is the exact range of my wireless equipment? (Antennas, Access Points etc)
What is the main advantage of PoE (Power-over-Ethernet)?
What makes L-com's antennas unique among most Wi-Fi antennas vendors?
What types of bandpass filters does L-com offer?
What Wireless Products Does L-com Offer?
Why are antennas the most important element of a wireless link?
WLAN-LCCPE28-1 FAQs
Other Are L-com’s connectivity products UL Recognized?

Do you have a question that doesn't appear here?

If you have searched our Help/FAQ page and still cannot find the answer to your question--no problem. Please e-mail us at customerservice@L-com.com. We will be more than happy to assist you.
 
Free Newsletter



L-com Global Connectivity           50 High Street           North Andover, MA 01845
www.L-com.com E-mail: sales@L-com.com 1-800-341-5266 www.Facebook.com/LcomGlobal


© Infinite Electronics International, Inc.