L-com Global Connectivity
  
Cart is Empty
  
USA & Canada (800) 341-5266     International +1 (978) 682-6936
You Are Here:  Home  >  Fiber Optic

Fiber Optic cable, Optical cable, Fiber cable, Fiber Optic adapter and other Fiber Optic products

Cable Assemblies (2173)
Cable Assemblies (2173)
Adapters,Couplers,Splitters (79)
Adapters,Couplers,Splitters (79)
Attenuators (23)
Attenuators (23)
Connectors (74)
Connectors (74)
Bulk Cable (54)
Bulk Cable (54)
Tools (16)
Tools (16)
Loopbacks (13)
Loopbacks (13)
Kits (7)
Kits (7)
Fiber Termination Enclosures (52)
Fiber Termination Enclosures (52)

L-com's fiber optic offering includes popular fiber optic cable, fiber optic connector, fiber attenuators, splitters and fiber optic termination enclosure products.

Fiber optic cable assemblies are available including single mode fiber, multimode fiber, duplex fiber and simplex or duplex single mode fiber cables. These fiber optic cable assemblies utilize the most widely used connectors including: LC, SC, ST, FC, MTRJ, and more.

Informative video explaining fiber optic cable types

A Quick Lesson In Optical Transmission

Where copper cabling uses electricity to transmit signals from one end to another, fiber optics use light pulses to accomplish the same purpose. The fiber optic cable is made of a transparent glass core surrounded by a mirror like covering called cladding. Light passes through the fiber optic cable, bouncing off the cladding until it reaches the other end of the fiber channel - this is called total internal reflection. In today's high speed networks, Graded Index Multimode fiber or Step Index Single mode fiber cable is used to improve light transmission over long distances. Multimode fiber optic cable has a larger core and is typically used in short runs within buildings. Single mode fiber optic cable has a smaller core and is used in long distance runs typically outside between buildings.

Fiber Optic Cable Core Sizes

Fiber specifications list the core and cladding diameters as a ratio. The top example shows the ratio of core to cladding as 62.5/125 microns. Below, the ratio is 9/125 microns. Multimode fiber is commonly 62.5/125 or 50/125 micron, single mode fiber is commonly 9/125 micron.

Fiber Optic Cable Core Sizes

Fiber Connector Polish Types / Typical Back Reflection

In Single mode applications the amount of back reflection on assemblies can be critical. L-com offers both PC and APC Single mode assemblies off the shelf. UPC finishes are available by custom order.

Fiber Connector Polish Types

Fiber Optic Glass Types

Stepped Index Fiber relies on the reflection of light whereas in Graded Index Fiber, the properties of the glass are changed in layers to "bend" the light as it travels down the cable. This reduces modal dispersion within the cable allowing for higher transmission rates.

Fiber Optic Cable Types

 
Free Newsletter
L-com Global Connectivity           50 High Street           North Andover, MA 01845
www.L-com.com E-mail: sales@L-com.com 1-800-341-5266 www.Facebook.com/LcomGlobal


© L-com, Inc. All Rights Reserved. L-com, Inc., 50 High Street, West Mill, 3rd Floor, Suite #30, North Andover, MA 01845