Enlarge
|
|
AdderLink Infinity Network DVI Extender Description: The AdderLink INFINITY demonstrates Adder's leading IP capability by delivering fluid interaction with computers as far away as your network can extend.
AdderLink INFINITY allows you to build a flexible infrastructure, the likes of which have not been possible before. Locate computers anywhere you like, share connections to computers, watch the interactions others have with computers, share control, collaborate, switch computers and so on. The AdderLink INFINITY is also the first device of its kind to allow multicasting across your network.
Adder's expertise in IP based KVM solutions also means that you get the very best video quality and fluid USB based interactions with your computer. Adder's own USB True Emulation technology has also been built into the AdderLink INFINITY, allowing you to connect all HID (Human Interface Devices) as well as storage devices and many other USB device types too.
Optimized for both HID and Mass Storage devices, the AdderLink INFINITY uses USB 2.0 technology to deliver reliable and flexible device support.
|
|

Enlarge
|
|
Broadata Mini-DVI, DVI Fiber Extender Description: The Mini-DVI Series is a high performance, low cost, miniature, directly pluggable Fiber Optic DVI Transmission System. It carries one (1) unidirectional DVI video, together with DDC, through one (1) multimode fiber. This unique fiber optic transmission system lets your digital flat panel display extend up to 400m at WUXGA (1920x1200 @ 60Hz) resolution.
|
|

Enlarge
|
|
Broadata Mini-DVI-AD, DVI Fiber Extender Description: The Mini-DVI-AD Series is a high performance, low cost, miniature, Fiber Optic DVI
Transmission System. It carries one (1) unidirectional DVI video, one (1) bi-directional stereo audio and two (2) RS-232 through one multimode fiber. This unique fiber optic transmission system lets your digital flat panel display extend up to 600m at WUXGA (1920x1200 @ 60Hz) resolution.
|
|

Enlarge
|
|
Gefen Multi Port DVI splitters Description: Gefen's ex-tend-it DVI Splitters are stackable distribution hubs that send the same DVI graphics source to two or more DVI based digital screens up to 50 feet away! When multiple DVI Splitters are connected together, they can be used to create a 1x4 or a 1x6 distribution (one DVI input / multiple DVI display outputs). When multiple units are stacked you can switch between all the inputs into all the outputs with the RMT-16 remote control. These DVI Splitters use a unique DVI Bus technology to connect multiple splitters without sacrificing a DVI output connection. The DVI displays attached to the splitter must be able to run at the same native resolution. Order online today!
|
|

Enlarge
|
|
Gefen DVI to VGA Converter Description: The GFN-DVI-2-VGA is used to connect your analog monitor to a DVI video port on a PC. The HD15 female connector at the output side of the GFN-DVI-2-VGA converter connects to the analog monitor and the DVI connecter utilizes a DVI (M-M) cable between the GFN-DVI-2-VGA and the graphic card in the PC. This converter generates all the compatible digital to analog conversion signals to make the connection between the digital input and the analog output work. Ships with one DVI to VGA Converter, one 5V DC Power Supply, and one six foot M-M DVI Cable. Includes a 1-year manufacturers warranty. Order online today!
|
|

Enlarge
|
|
Gefen 1:4 DVI Distribution Amplifier Description: Gefen's 1:4 DVI distribution hub sends the same DVI graphics source to up to four DVI digital displays (flat panels or projectors). It is a reliable solution that accommodates four digital video displays at the same time, creating a multi-viewing environment that maintains the highest resolution video at all times. Order online today!
|
|

Enlarge
|
|
Gefen DVI Super Booster Description: Extending digital video via DVI beyond its specified 15-foot distance limitation using a DVI copper cable simply cannot replicate the highest resolutions perfectly. In fact, sparkles or other objectionable distractions of the video often appear that indicate the signal has been degraded. But add a Gefen DVI Super Booster to that same cable, and it can extend pristine HD resolutions up to 1080p or 1920x1200 up to 200-feet. It operates just like the DVI Booster, but comes with an optional power supply that guarantees performance up to 200-feet. So you can kick back and enjoy your video in the most precise, enthralling manner it was intended. Order online today!
|
|

Enlarge
|
|
Gefen Fiber DVI Extender (RX/TX Pair) Description: The Gefen DVI FMP Extender extends your DVI display up to 2,000 feet away from your source, with only a tiny transmitter and receiver required, using a 100% optical fiber solution. It's a great way to extend DVI video easily and unobtrusively. The DVI FMP sender unit plugs into your computer. The DVI FMP receiver unit plugs into your DVI display - up to 2,000 feet away. Multi mode LC fiber optic cable (4 strand) connects the DVI FMP sender and the DVI FMP receiver units to each other. Order online today!
|
|

Enlarge
|
|
DVI Extender/Equalizer Description: This DVI Extender/Equalizer expands DVI video signals up to 150 feet while maintaining a pristine image. This competitively priced DVI extender takes a signal from the source, sends it over a standard DVI cable and connects it to a display via a short (15 feet or less ) DVI cable. The unit features a Plug and Play design and includes a power adapter. Order online today!
|
|

Enlarge
|
|
UTP DVI Extender Description: This unique DVI extender extends digital video signals up to 100 feet @1024x768 XGA or 50 feet @ 1600x1200 UXGA! This product is ready to use right out of the box. No software is required and set up time is minimal. Simply connect a Category 5 or better UTP cable (sold separately) to each RJ45 jack and you are ready to extend DVI. Order online today!
|
|

Enlarge
|
|
Icron DVI Rover™ 800 Active DVI cables Description: The Icron DVI Rover 800 cables are active fiber and copper DVI&DDC extension cables that are available in various lengths These cables feature hotplug detect, DVI-D male connectors, and downward-compatible resolution support. The 800 series cables support PCs, Macs, and HDTV platforms. Available in SXGA and UXGA versions.
|
|

Enlarge
|
|
Gefen HDMI Super Booster Description: A great alternative to the traditional sender/receiver solutions for HD extension, the HDMI Super Booster enables your standard, "off the shelf" HDMI cable to transmit brilliant HDTV visuals plus multichannel digital audio in a single cable way beyond the limited HDMI specification of 15-feet! Up to 200-feet can be easily traversed using your HDMI cable plus a HDMI Super Booster, which corrects any digital degradation that occurs when HDMI is used to send AV signals beyond the specified distance. To go beyond the limited inherent HDMI distance or if you'd like to use two or more cables, these Boosters are a perfect option. They replicate digital video signals, enabling you to "daisy chain" cables and repeaters as far as you need to go. Order online today!
|
|

Enlarge
|
|
Inline HDMI Extender/Equalizer Description: This small form factor HDMI extender can be quickly installed and provides up to 150 feet of HDMI extension! The HDMI-EXT-150 requires no external power supply and supports popular HDTV (High Definition TV) resolutions including 1080p. Simply connect the Source port to a long HDMI cable (up to 150 feet) and then to an HDMI source such as a cable set-top box or satellite receiver. Next, connect a short HDMI cable (1 foot or 1 meter) to the Sync/Display port then to the display and set up is complete. NOTE: This product will not work with the PS3 Play Station (Version 3).
|
|

Enlarge
|
|
Gefen HDMI over Cat5 Extender Description: The GFN-HDMI-CAT5X extends your HDMI signal up to 200 feet (60 meters) away over two CAT-5 cables. This extender is equipped with HDMI™ (high definition multimedia interface) connectors and RJ45 jacks which support Cat5/e cabling. Order online today!
|
|

Enlarge
|
|
Gefen HDMI Fiber Extender- (100 Meters) Description: The GFN-HD-1000 allows an HDMI video signal to be extended up to 330 feet (1640 w/o HDCP) using multimode LC-LC fiber optic cable. Fiber Optic technology allows the GFN-HD-1000 to carry video signals over long distances that are not possible with other technologies. Fiber Optic cables are immune to video signal corruption from electromagnetic interference (EMI), ensuring a crystal clear picture.
|
|

Enlarge
|
|
Broadata Mini-HDMI, Fiber HDMI Extender Description: The Mini-HDMI Series is a high performance, low cost, miniature, directly pluggable Fiber Optic HDMI Transmission System. It carries one (1) unidirectional HDMI video, together with HDCP/DDC, through one (1) multimode fiber. This unique fiber optic transmission system lets your digital flat panel display extend up to 400m at WUXGA (1920x1200 @ 60Hz) resolution. Also supports 720p/1080i/1080p resolutions.
|
|

Enlarge
|
|
Broadata Mini-HDMI-AD, Fiber HDMI Extender Description: The Mini-HDMI-AD Series is a high performance, low cost, miniature, Fiber Optic HDMI Transmission System. It carries one (1) unidirectional HDMI video, one (1)
bi-directional stereo audio and two (2) RS-232 through one multimode fiber. This
unique fiber optic transmission system lets your digital flat panel display extend up to 600m at WUXGA (1920x1200 @ 60Hz) resolution. DVI video is also available through a DVI-to-HDMI adapter cable.
|
|

Enlarge
|
|
Broadata Mini-HDMI-WP, Fiber HDMI Extender Wall Plate Description: The Mini-HDMI-WP Series is a high performance, low cost, miniature, Fiber Optic HDMI extender system, designed specifically for wall plate installation. It carries one (1) unidirectional HDMI video, together with HDCP/DDC, through one (1) multimode fiber. This unique fiber optic transmission system lets your digital flat panel display extend up to 400m at WUXGA (1920x1200 @ 60Hz) resolution.
|
|

Enlarge
|
|
Aten 4 Port and 8 Port HDMI Switches Description: L-com offers a variety of HDMI switching solutions from Aten. The VS series of HDMI switches are perfect for home theater, Pro A/V and Digital Signage applications. Features include push button or remote control channel selection and signaling rates up to 2.25 Gbps. Additionally, these HDMI switches are plug and play making installation a snap. Order online today!
|
|

Enlarge
|
|
Gefen 1 X 2 HDMI Splitter Description: The Gefen 1x2 HDMI splitter allows set-top boxes, DVD players, D-VHS players and other HDTV devices with HDMI output to be connected to two HDTV displays. It is a flexible solution that accommodates multiple displays. The HDMI splitter is connected using a HDMI cable from the HDMI source to the HDMI splitter input. Order online today!
|
|

Enlarge
|
|
Gefen 1 X 4 HDMI Splitter Description: The 1x4 HDMI splitter allows set-top boxes, DVD players, D-VHS players and other HDTV devices with HDMI output to be connected to four or more HDTV displays.Gefen's 1x4 HDMI splitter is a distribution hub that sends the same video output to four or more HDTV digital displays. It is a flexible solution that accommodates multiple displays. When two or more HDMI splitters are connected together, they can be used to create a larger distribution. The HDMI splitter is connected using a HDMI cable from the HDMI source to the HDMI splitter input. There are four HDMI outputs. HDMI output 1 is the primary connection and is used for the main display. Outputs two, three and four follow the main display. Order today!
|
|

Enlarge
|
|
Gefen 2X1 HDMI Switcher Description: The Gefen 2x1 HDMI Switcher enables effortless HDMI source switching using a single high definition display. A simple and reliable solution, the 2x1 HDMI switcher links any two HDMI sources (DVD players and satellite set tops) to one HDMI display. It completely eliminates the need to disconnect then reconnect multiple HDMI sources, saving time by providing a fundamental tool that brings it all together behind the scenes. When all three devices (the display plus the two sources) are connected to the 2x1 HDMI Switcher and powered on, you simply select which source you want to view on the display using the Switcher, the IR remote that comes with it, or any universal remote you program to work with the Switcher. Order online today!
|
|