L-com Global Connectivity
  
Cart is Empty
  
USA & Canada (800) 341-5266     International +1 (978) 682-6936
You Are Here:  Home  >  D-Subminiature  >  Cable Assemblies  >  Premium D-Sub Cable Assemblies

Premium D-Sub Cable Assemblies

Our CS2N Series D-Sub cable assemblies are our top of the line D-Sub cable offering. The bulk cable utilizes 26 AWG stranded conductors with double shielding (copper braid plus aluminum mylar foil) and flexible PVC jacket. Fully molded backshells also have a unique stamped steel internal enclosure that provides the ultimate in shielding performance. Mounting is done via rugged 4-40 thumbscrews that are easy to grip without the need for a screwdriver. Hex nuts on female connectors are removable to expose 4-40 thumbscrews.

Show Descriptions     Show Matrix 
Premium D-sub 9 Position DB9 Male/Male Cables - Fully Populated, Double Shielded Premium D-sub 9 Position DB9 Male/Male Cables - Fully Populated, Double Shielded
Premium D-sub 9 Position DB9 Male/Female Cables - Fully Populated, Double Shielded Premium D-sub 9 Position DB9 Male/Female Cables - Fully Populated, Double Shielded
Premium Black D-sub 9 Position DB9 Male/Male Cables - Fully Populated, Double Shielded Premium Black D-sub 9 Position DB9 Male/Male Cables - Fully Populated, Double Shielded
Premium Black D-sub 9 Position DB9 Male/Female Cables - Fully Populated, Double Shielded Premium Black D-sub 9 Position DB9 Male/Female Cables - Fully Populated, Double Shielded
Premium D-sub 15 Position DB15 Cable Male/Male- Fully Populated, Double Shielded Premium D-sub 15 Position DB15 Cable Male/Male- Fully Populated, Double Shielded
Premium D-sub 15 Position DB15 Male/Female Cables - Fully Populated, Double Shielded Premium D-sub 15 Position DB15 Male/Female Cables - Fully Populated, Double Shielded
Premium Black D-sub 15 Position DB15 Male/Male Cables - Fully Populated, Double Shielded Premium Black D-sub 15 Position DB15 Male/Male Cables - Fully Populated, Double Shielded
Premium Black D-sub 15 Position DB15 Male/Female Cables - Fully Populated, Double Shielded Premium Black D-sub 15 Position DB15 Male/Female Cables - Fully Populated, Double Shielded
Premium Black D-sub 15 Position HD15 Male/Male Cables - Fully Populated, Double Shielded Premium Black D-sub 15 Position HD15 Male/Male Cables - Fully Populated, Double Shielded
Premium Black D-sub 15 Position HD15 Male/Female Cables - Fully Populated, Double Shielded Premium Black D-sub 15 Position HD15 Male/Female Cables - Fully Populated, Double Shielded
Premium High Density D-sub 15 Position HDB15 Male/Male Cables - Fully Populated, Double Shielded Premium High Density D-sub 15 Position HDB15 Male/Male Cables - Fully Populated, Double Shielded
Premium High Density D-sub 15 Position HDB15 Male/Female Cables - Fully Populated, Double Shielded Premium High Density D-sub 15 Position HDB15 Male/Female Cables - Fully Populated, Double Shielded
Premium D-sub 25 Position DB25 Male/Male Cables - Fully Populated, Double Shielded Premium D-sub 25 Position DB25 Male/Male Cables - Fully Populated, Double Shielded
Premium D-sub 25 Position DB25 Male/Female Cables - Fully Populated, Double Shielded Premium D-sub 25 Position DB25 Male/Female Cables - Fully Populated, Double Shielded
Premium Black D-sub 25 Position DB25 Male/Male Cables - Fully Populated, Double Shielded Premium Black D-sub 25 Position DB25 Male/Male Cables - Fully Populated, Double Shielded
Premium Black D-sub 25 Position DB25 Male/Female Cables - Fully Populated, Double Shielded Premium Black D-sub 25 Position DB25 Male/Female Cables - Fully Populated, Double Shielded
Premium D-sub 37 Position DB37 Male/Male Cables - Fully Populated, Double Shielded Premium D-sub 37 Position DB37 Male/Male Cables - Fully Populated, Double Shielded
Premium D-sub 37 Position DB37 Male/Female Cables - Fully Populated, Double Shielded Premium D-sub 37 Position DB37 Male/Female Cables - Fully Populated, Double Shielded
Show Descriptions     Show Matrix 
 
Free Newsletter
L-com Global Connectivity           50 High Street           North Andover, MA 01845
www.L-com.com E-mail: sales@L-com.com 1-800-341-5266 www.Facebook.com/LcomGlobal


© Infinite Electronics International, Inc.