The terms VGA, SVGA, XGA, SXGA, UXGA etc., all relate to the resolution a monitor supports.
The video format is the same despite the different designations and as an example a UXGA monitor can Display resolutions from VGA all the way up to UXGA. In all cases they use the same HD15 connector (below images) and VGA and SVGA cabling.
HD15 Male Interface image | HD15 Female Interface image |
Regardless of what resolution a Monitor or Video Card is able to support, they are commonly referred to as just being VGA, the naming conventions listed above never really caught on with the general public and thus even the most High End 3-D Graphics card from Companies like NVIDIA or ATI will have what they term a VGA port (in addition to a DVI port in many cases) even though the card may output resolutions greater than 1920 x 1440.
Some High End Monitors support resolutions up to 2048x1536 @ 79Hz, which is still part of the same Multisync format and is backwards compatible to lower resolutions. Most High End Monitor Manufacturers don't mention VGA, SVGA etc at all, they typically refer to Monitors as CRT's, LCD's or Plasma Displays and list the maximum resolution that they support and at what refresh rate.
The relationship is as follows:
| *Legacy Resolutions no longer supported (included only for reference) | | | | | Description | Code | Resolution | | *(Color Graphics Adapter) | CGA | 320 x 200 | | *(Enhanced Graphics Adapter) | EGA | 640 x 350 | | | | | | (Video Graphics Array) | VGA | 640 x 480 | | (Super Video Graphics Array) | SVGA | 800 x 600 | | (High Definition Television 720i/p) | HDTV | 1280 x 720 | | (Extended Graphics Array) | XGA | 1024 x 768 | | (Wide Extended Graphics Array) | WXGA | 1366 x 768 | | (Super Extended Graphics Array) | SXGA | 1280 x 1024 | | (Super Extended Graphics Array+) | SXGA+ | 1400 x 1050 | | (Wide Super Extended Graphics Array) | WSXGA | 1600 x 1024 | | (Wide Super Extended Graphics Array+) | WSXGA+ | 1680 x 1050 | | (High Definition Television 1080i/p) | HDTV | 1920 x 1080 | | (Ultra Extended Graphics Array) | UXGA | 1600 x 1200 | | (Wide Ultra Extended Graphics Array) | WUXGA | 1920 x 1200 | | (Quad Extended Graphics Array) | QXGA | 2048 x 1536 | | (Quad Super Extended Graphics Array) | QSXGA | 2560 x 2048 | | (Wide Quad Super Extended Graphics Array) | WQSXGA | 3200 x 2048 | | (Quad Ultra Extended Graphics Array) | QUXGA | 3200 x 2400 | | (Wide Quad Ultra Extended Graphics Array) | WQUXGA | 3840 x 2400 | | (Hex Super Extended Graphics Array) | HSXGA | 5120 x 4096 | | (Wide Hex Super Extended Graphics Array) | WHSXGA | 6400 x 4096 | | (Hex Ultra Extended Graphics Array) | HUXGA | 6400 x 4800 | | (Wide Hex Ultra Extended Graphics Array) | WHUXGA | 7680 x 4800 | |