Cart is Empty
Home   Request Catalog   Custom Cables   Product Wizards   Technical Resources   Contact Us

 

How To Setup A Laptop WiFi Booster Kit - Indoor Use Only (Video)

L-com video loading. . .

Email this video to a friend

How To Setup A Laptop WiFi Booster KitToday we are installing a laptop WiFi booster kit from L-com. This kit can be purchased by anyone in the United States and is FCC certified. No special FCC license is required to use or sell these WiFi Booster kits. This kit is intended for indoor use only.








Step 1
First, install the USB wireless adapter’s drivers from the supplied CD.

Step 2
Next, insert the USB wireless adapter into your laptops USB port.

Step 3
Then connect a reverse polarity SMA to reverse polarity TNC cable (can be purchased separately) for the USB wireless adapter to the WiFi booster port marked "Radio". For applications that require connections from the amplifier to the antenna, you can use these cables (can be purchased separately at http://www.l-com.com/productfamily.aspx?id=6467.)

Step 4
Next, connect a reverse polarity SMA to reverse polarity TNC coax adapter (can be purchased separately at http://www.l-com.com/item.aspx?id=22154) to the WiFi booster port marked "Antenna".

Step 5
Now connect the supplied rubber duck antenna to the coax adapter.

Step 6
Finally, plug the AC adapter into the WiFi booster's DC power jack and then into an AC wall outlet.

Setup is now complete. The LEDs will flash on the WiFi booster indicating transmitting and receiving activity.

L-com offers indoor, outdoor, PoE, economy WiFi booster kits and more!

View our complete line of WiFi signal boosters here.

View our WiFi booster kits which are available for anyone in the USA to purchase.