Home - L-com Connectivity Products
Login to My Account
Cart is Empty
Checkout
 
 
Home Quick Order Free Catalog Custom / OEM New Products Sale Items Government International Distributors About Us Contact Us
Request Your Free Catalog Sign Up For Our Newsletter

What is Power-over-Ethernet (PoE)?

View L-com's full line of Power over Ethernet (PoE) Product

Power-over-Ethernet (PoE) or "Active Ethernet" eliminates the need to run 110/220 VAC power to Wireless Access Points and other devices on a wired LAN. Using Power-over-Ethernet system installers need to run only a single CAT5 Ethernet cable that carries both power and data to each device. This allows greater flexibility in the locating of AP's and network devices and significantly decreasing installation costs in many cases.

Power-over-Ethernet begins with a CAT5 "Injector" that inserts a DC Voltage onto the CAT5 cable. The Injector is typically installed in the "wiring closet" near the Ethernet switch or hub.

Some Wireless Access Points and other network accept the injected DC power directly from the CAT5 cable through their RJ45 jack. These devices are considered to be "PoE-Compatible" or "Active Ethernet Compatible".

Devices that are not "PoE Compatible" can be converted to Power-over-Ethernet by way of a DC "Picker" or "Tap". These are sometimes called Active Ethernet "Splitters". This device picks-off the DC Voltage that has been injected into the CAT5 cable by the Injector and makes it available to the equipment through the regular DC power jack.

Therefore in order to use Power-over-Ethernet you need:

(Injector) + (PoE compatible device)
- or -
(Injector) + (non-PoE compatible device) + (Picker)

Types of Picker / Taps

Two basic types of Pickers and Taps are available: Passive and Regulated.

A Passive Tap simply takes the voltage from the CAT5 cable and directs it to the equipment for direct connection. Therefore if 48 VDC is injected by the Injector then 48 VDC will be produced at the output of the Passive Tap.

A Regulated Tap takes the voltage on the CAT5 cable and converts it to another voltage. Several standard regulated voltages are available: 12VDC, 6 VDC, 5 VDC. This allows a wide variety of non-PoE equipment to be powered through the CAT5 cable.

Voltage and Pinout Standards

Although the IEEE has a PoE standard called IEEE 802.3af, different equipment vendors use different PoE voltages and CAT5 pin configurations to provide the DC power. Therefore it is important to select the appropriate PoE devices for each piece of equipment you plan to power through the CAT5 cable.

The IEEE has standardized on the use of 48 VDC as the Injected PoE voltage. The use of this higher voltage reduces the current flowing through the CAT5 cable and therefore increases the load and increases the CAT5 cable length limitations. Where the maximum cable length has not been a major consideration some vendors have chosen 24 VDC and even 12 VDC as their "injected" voltage.

Multi-Port Injectors

Several manufacturers offer Multi-Port Injectors including 6 and 12-port models. These models are less versatile since they are only used where many devices are to be powered through the CAT5 cable originating in a single wiring closet or from a single switch. They typically operate in exactly the same manner as their more popular single-port counterparts.

PoE Applications

Power Over Ethernet Passive Injector Application image


Power Over Ethernet Single Regulated Tap Application image


Power Over Ethernet Dual Regulated Tap Application image

 View L-com's full line of Power over Ethernet (PoE) Products.

Product Note: The Power Over Ethernet products listed on this page may also be referred to as: passive ethernet injector, passive ethernet splitter, passive splitter, passive injector, active ethernet injector, active ethernet splitter, active injector, active splitter, data / power splitter, DC injector and power injector.



My Recent History . . .
Products that I have viewed
HD15 AB Switch Box, Female Connectors
RG223 Coaxial Cable, BNC Male/Male 10.0 ft
Coaxial Adapter, BNC Female / TNC Male
Media Converter, 10Base-T RJ45 to 10Base-5 DB15M AUI
Fibre Channel Cable, 1 Gb/s, HSSDCM/DB9M, 3.0 Meters
Search terms
korenix
Secure online ordering   L-com.com is a VeriSign Secure site.   L-com is a BBB accredited business.   L-com has been awarded the U.S. General Services Administration (GSA) contract.   L-com is UL Certified   ISO 9001:2008
Need Help or Want to Order By Phone? Call Toll Free at 1-800-341-5266
Home  | Privacy Policy  | Terms & Conditions  | Press Releases  | Customer Service  | Sitemap  | Links  | Contact Us
Connect with L-com Global Connectivity Follow L-com on Twitter Follow L-com on Facebook Follow L-com on YouTube
© L-com, Inc. All Rights Reserved. L-com Global Connectivity and the L-com logo are registered marks.
L-com, Inc., 45 Beechwood Drive, North Andover, MA 01845
  Shop by Category Antennas Audio/Video Coaxial D-Subminiature Ethernet Networking Fiber Optic Firewire/DIN/SCSI/SATA IEEE-488 GPIB Lightning Protectors Media Converters Patch Panels/Racks PoE Power Products RF Filters/Splitters Serial Converters Telecom/Modular Test Equipment USB Weatherproof Enclosures Wireless LAN Amplifiers Wireless Networking

Shop by Type Adapters Bulk Cable Cable Assemblies Connectors Ethernet & Serial Adapters Ethernet Switches KVM Switches Media Converters Switch Boxes Tools

Shop By Frequency

Product Configurator

Product Wizards

Product Comparisons

Technical Resources

Newsletter Archive