L-com Global Connectivity
  
Cart is Empty
  
USA & Canada (800) 341-5266     International +1 (978) 682-6936
 

Tech Tip- Installing IP Cameras with Access Points

When setting up IP cameras along with outdoor access points, be sure to use an access point that has a secondary LAN connection. This will enable you to plug the IP camera directly into the access point. When using more than one IP camera with your access point, you will need to add an Ethernet switch such as the Planet SWTC-PTG503. Remember to always check the camera specs so you don’t exceed the bandwidth capability of the access point.

The following access points feature a secondary LAN port:

L-com WLAN-LCCPE516-1                                                   Planet WNAP-7350

5GHz Access PointOutdoor Wireless Access Point

 

 

Engenius ENH500 and ENH210EXT

 

Long Range Access Point 2.4 GHz Outdoor Access Point

         
 
Free Newsletter
L-com Global Connectivity           50 High Street           North Andover, MA 01845
www.L-com.com E-mail: sales@L-com.com 1-800-341-5266 www.Facebook.com/LcomGlobal


© Infinite Electronics International, Inc.