Home - L-com Connectivity Products
Secure Online Ordering
Login to My Account
Cart is
Empty
L-com.com is a McAfee Secure Site Checkout

 
 
HomeQuick OrderRequest/Download a catalogCustom/OEM ProductsNew ProductsOverstock and Sale ItemsAbout UsContact Us
Print
What is L-com's Customer Service Pledge?

Our Pledge To You

RESPECT - We will treat all customers with respect, we will use proper etiquette with every communications medium that we use.

HONEST - We will be honest in all dealings with the customer.

HELPFUL - We will exhaust all options within our means when helping the customer. Then, if we can't solve their problem, we will help point them in the right direction.

RESPONSIVE - We will be diligent in responding to our customer's needs quickly:
    a. Every call is to be answered within 30 seconds.
    b. Every e-mail or fax is to be responded to the same day or sooner with an update on progress or the outcome of the request.

PROACTIVE - We will inform our customer of any issues prior to them becoming problems. We will anticipate our customer's needs and help them.

THANKFUL - We will end every conversation we have with the customer using "Thank You".

COMMITTED - We will be accurate with our commitments with the customer. Once a promise is made, it is every employee's responsibility to meet it.

ATTITUDE - We will keep a positive attitude about our company and ourselves. We will never say no to the customer; instead we will offer alternatives. We will give 110% and do everything we can to make each experience with us a satisfying one.


Other Frequently Asked Questions:
 
Account Management Can I change my billing address?
How can I apply for a credit account?
How can I view my account and payment types and pricing information?
How do I change my communication preferences?
How do I change my password or password hint information?
How do I change my product interests?
How do I change my product use?
How do I review my order history?
How do I track my order?
How do I view and manage my saved carts?
How do I view my item history?
What if I forgot my password?
Who is my L-com contact?
Enclosures What does NEMA mean?
How do I ... How can I assemble the 4 wires onto CNUSB-A or CNUSB-B USB sockets? Do I need to solder these 4 wires or use crimp tool?
How Can I transfer files between two(2) computers without networking them?
How do I find and download the free 2D Engineering Drawings on your products?
How do I split out two of the unused lines on my existing cat5 cable to add phone capability without pulling new lines in my building?
How do I use a flat panel monitor with a standard VGA connected computer?
L-com Policies Does L-com have a Code of Conduct Policy?
How do I return a purchase?
Is L-com ISO certified?
What are your shipping and processing fees?
What are your terms and conditions?
What is L-com's Cage Code?
What is L-com's Corporate Responsibility?
What is L-com's Customer Service Pledge?
What is L-com's Minimum Order Quantity (MOQ) or Minimum Dollar Amount?
What is your privacy policy?
Ordering How do I track my order?
Is your website secure?
What if I have a question about my order?
What payment methods do you offer?
Product Applications Does part # MWP4BNK work for light switches or is this just for some type of computer/video equipment?
I want to connect two computers to one printer without networking. Is there a connector or switch I can purchase to accomplish this task?
Is the SATA cable usable for a 2.5 inch standard Seagate Momentus 5400.2 hard drive ?
Will either cables TFC6101 or TFCLS6001, stranded, shielded, 26 AWG, work with TDS8PC6 plug?
Will the TDC053 series and ECF504-8SK coupler work in a 100-Base-T RJ45 product application?
Product Information How do I search for products or part numbers?
I am seeking 4x4 handset couplers, or extension cords. Are they even available anywhere?
I need the connector's measurements for cable model DK238MM series because I have to put it into a 1/2" hole.
I want cable assemblies at a special length. How do I request custom length cables?
I'm seeking something like the ZN-ZUC3100 but the female version. Do you carry it?
What are products that start with SP?
What are these Cable Tie Bars made of?
What is your part # for the RJ45 Keystone insert (used with MWP10 series)?
Coaxial Products Can you tell me the frequency range for the SMA/BNC (e.g. BA29, BA38) and SMA/SMA (e.g. BA23) adapters?
What does RG316/U mean?
What is an MCX Connector and what applications are MCX Connectors used in?
What is the difference between 75 Ohm and 50 Ohm coaxial cable and when should each one be used?
What is the difference between an SMB plug and SMB jack?
Why is proper termination of coaxial connectors imperative?
D-Sub Products Are the wire color codes available for the CHD high density cable assembly series?
Are your Economy 25 Pin D-Sub Molded Cables (CSM series) pass-through cables?
Is the material that the SD121 Plastic D-Sub Hoods are made of (PBT) Polybutylene Terephthalate Glass filled Thermoplastic?
What is a DB9 Connector?
What is cable dia of CSMN25MF D-sub cables?
What is the CS2N Series Operating Temperature Range?
What is the current carrying capacity of your CS2N37MM-10 and CS2N37MM-15 cables?
What is the minimum bend radius of your CAUZ900MM-3M cables?
What is the wire color code for L-com's D-Subminiature cables?
When the CSNULL9FF cables ship, do they come with dust caps on both ends?
Fiber Optic Products I downloaded your 3D model of your LC/LC Duplex Fiber Coupler. The A’s don’t line up with each other. The A on one end lines up with the B on the other end. Is this correct?
I have an existing copper infrastructure, what's the most cost-effective way to upgrade to fiber?
I'm trying to connect two male MTRJ connectors using the MTRJ fiber coupler part number FOA-600 and they won't work. What gender is the FOA-600 on each side?
Is fiber more difficult to install than copper?
Multimode, singlemode, laser optimized - What does it all mean?
What is the minimum bend radius for model SFOSC fiber patch cords?
Modular Products Can Cat 5E cabling be used in Gigabit Ethernet Applications?
How are your TRD855SIG-15 cables wired? Are they crossover?
I am trying to find something that looks like the TRD855SIG (double shield, zero halogen, CAT5e with RJ45 plugs) but with stranded conductors instead of solid (and preferably also AWG 26 if possible).
I need to know what the max material thickness your TDG1026KC6 couplers can fit in to.
I would like to know the crimp height and tolerance of a L-com Crimper P.N. HTS2500 using a TDS8PC5 Modular plug.
Regarding TDB4 bulk modular cable, what is the wire resistance per meter?
What is the conductor resistance per meter of TDB4 flat silver satin modular cable?
What is the difference between a shielded and unshielded modular coupler?
What is the minimum temperature rating for bulk cable TDB series?
What is the panel thickness of TDG1026KC5 modular couplers?
What type of keystone wall mounting styles are there?
Why is choosing the right type of cabling important for a network?
USB Products How can I find the USB cable for my camera on your website?
How do I connect a IEEE-1394 (Firewire) device to the USB port on my computer or laptop?
How do I download and install the driver for the ZN-ZUC3100?
How fast is USB?
Is there a difference for 1.0 or 2.0 on ECF504B-UAB?
What is a USB cable?
What kinds of USB peripherals can I connect to my PC?
Video Products Converting VGA to S-Video
I have 1 video card but I want to connect 2 monitors to it and have like an extended desktop. Do you have a splitter that can do what I need?
What is Digital Signage and where is it used?
What is HDMI?
What is the max length of DVI cable assemblies?
What is the max length of HDMI cable assemblies?
Technology and Terminology Are there any maximum manufacturer recommended lengths for CAT5/5E UTP, CAT5/5E STP, USB, 50 micron fiber or 62.5 micron fiber?
Can you please provide a table of minimum bend radius values that includes values for CAT5 UTP, CAT5E STP, USB, 50micron fiber optic and 62.5micron fiber optic cables?
Keystone connector dimensions
Minimum Lengths for Ethernet Cabling
Using PMOD4U-1 on a Cat5 Network?
We have a 100 megabit Ethernet network that is cabled with category-5 in our office...
What are the basic things a network consists of?
What cables connect a video card to a camcorder?
What is a PL-259 Plug and does L-Com carry any PL-259 products?
What is cat 5 plenum and PVC cable, and why is the plenum cable so much more expensive?
What is EIA232C?
What is the color code for SVGA Cable?
What is the difference between VGA, SVGA and UXGA, and does L-com sell cables for each?
Why Use Shielded Category 6 vs. Unshielded Category 6 cables?
Wireless
How are bi-directional amplifiers used?
How do I choose the right WiFi amplifier?
How do I use a HyperLink Brand WiFi Antenna?
What are the key requirements of bi-directional amplifiers for use with the new high data rate 802.11a/g/n radios?
What are the uses of lightning protectors?
What HyperLink Brand Antennas are Available?
What HyperLink Technologies Products Does L-com Offer?
What is a Ceiling Mount WiFi Antenna?
What is Polarity?
What is the exact range of my wireless equipment? (Antennas, Access Points etc)
What is the main advantage of PoE (Power-over-Ethernet)?
What makes L-com's HyperLink brand of antennas unique among most Wi-Fi antennas vendors?
What types of bandpass filters does L-com offer?
Why are antennas the most important element of a wireless link?
Other Are L-com’s connectivity products UL Approved?
Directions to L-com
Downloads and Plugins

Do you have a question that doesn't appear here?

If you have searched our Help/FAQ page and still cannot find the answer to your question--no problem. Please e-mail us at customerservice@L-com.com. We will be more than happy to assist you.


   L-com is a BBB accredited business    AlertSite is a leading provider of Web site monitoring and performance management solutions that help businesses ensure optimum Web experiences for their customers.   L-com has been awarded a U.S. General Services Administration (GSA) contract.  L-com is UL Certified  L-com is ISO 9001:2008 Registered
Need Help or Want to Order By Phone? Call Toll Free at 1-800-341-5266
Tell A Friend  |   Help/FAQ  |   Sitemap  |   Contact Us
Adjust Text Size Adjust text size to normal.  Adjust text size to large. 
Friendly and Knowledgeable Service
© L-com, Inc. All Rights Reserved. L-com Global Connectivity and the L-com logo are registered marks.
  Shop by Category Antennas Audio/Video Coaxial D-Subminiature Ethernet Networking Fiber Optic Firewire/DIN/SCSI/SATA IEEE-488 GPIB Lightning Protectors Media Converters Patch Panels/Racks PoE Power Products RF Filters/Splitters Serial Converters Telecom/Modular Test Equipment USB Weatherproof Enclosures Wireless LAN Amplifiers Wireless Networking

Shop by Type Adapters Bulk Cable Cable Assemblies Connectors Ethernet & Serial Adapters Ethernet Switches KVM Switches Media Converters Switch Boxes Tools

Shop By Frequency

Product Configurator

Product Wizards

Product Comparisons

Technical Resources