L-com Global Connectivity
  
Cart is Empty
  
USA & Canada (800) 341-5266     International +1 (978) 682-6936
Gigabit Ethernet Passive PoE Midspans Added to L-com Lineup
(Monday, March 26, 2012)
 

Gigabit Ethernet Passive PoE Midspans Added to L-com Lineup

Single-Port Cat6 PoE Injector/Midspan
Four-Port Cat6 PoE Injector/Midspan

NORTH ANDOVER, MA - 3/26/12 - L-com, Inc., a designer and manufacturer of wired and wireless connectivity products, has added two new PoE products for Category 6 gigabit Ethernet lines: a single-port and a four-port model. The new items are IEEE 802.3af compatible, and are available either individually or in kits with 48VDC power supplies at either 48W or 70W.

Power-over-Ethernet (PoE) is the technology that uses ordinary Ethernet cabling to carry power.  L-com's new BT-CAT6-P1 and BT-CAT6-P4 models use Gigabit transformers on all four data pairs in contrast to cheaper designs that only use transformers for two pairs. They feature die-cast aluminum housings with integral mounting feet for long-term installations. The metal housing helps reduce EMI interference on the Ethernet lines, while also providing superior grounding via a directly-attached ground lug and terminal.

"As the need for Ethernet connectivity grows, it becomes much more important to provide it for all corners of a building or campus, including places where there are no AC outlets nearby," said Patrick Pesa, Director of Product Management. "PoE is the best solution to this problem, and L-com provides options for Category 5, Category 5e, and now more options for Category 6 cabling."

Detailed datasheets for the single-port and four-port models are available for free download along with 2D engineering drawings on the L-com.com web site.  Both products are currently stocked in L-com's Florida distribution center for shipping on the same day as ordered.

Please click here to download a high-resolution version of the first image suitable for print publication.
Please click here to download a high-resolution version of the second image suitable for print publication.

For more information about this release, please contact:
Dave Fallon, Internet Marketing Strategist
978-682-6936 x1450, newsletters@L-com.com

L-com, a global designer and manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as the Hyperlink line of wireless products. Trusted for more than 25 years, L-com, Inc. is headquartered in North Andover, Mass., and is ISO 9001: 2008-certified. For more information, please visit: http://www.L-com.com/


Other press releases that may be of interest to you:
 
7/18/2019 L-com Introduces New Active Optical Cables for use in High-Speed Data Center Applications
7/17/2019 L-com Launches New 900 MHz Omni and Sector Antennas
7/16/2019 L-com Unveils Premium 8-Position, A-code, M12 Cable Assemblies for Sensor, Actuator and Fieldbus Applications
7/11/2019 L-com Releases New OM5 Fiber Cables for High-Speed Data Center Applications
6/27/2019 L-com Releases New Small Cell and Outdoor Power Protection Enclosures
6/26/2019 L-com Adds New Premium RJ45 to M12 Female Panel-Mount Cable Assemblies
6/13/2019 L-com Releases New Flat HDMI Cables with LSZH Jackets
5/23/2019 L-com Launches New Indoor and Outdoor-Rated Cat6a Lightning and Surge Protectors
5/14/2019 L-com Introduces New Cat7 LSZH Cable Assemblies for Shipboard, Aerospace and Defense Applications
5/9/2019 L-com Launches New M12 Field Termination Connectors and In-line Adapters to Address Industrial Networking Applications
5/7/2019 L-com Releases New Cat6a Outdoor-Rated, High-Flex Ethernet Cable Assemblies
4/25/2019 L-com Expands Outdoor Industrial Ethernet Cable Line with Additional Length Options Available with Same-Day Shipping
4/4/2019 L-com Releases New Patch Panels with N-Type Couplers and 0.630” D-Holes
4/2/2019 L-com Adds New Power Cords for Server, PC, Laptop, PDU Applications and More
3/21/2019 L-com now Stocks 12G-SDI, HD-BNC Connectors for use in Broadcast Video Applications
3/19/2019 L-com Launches New Line of Rugged Category 7 Cables with 10 Gig Rating for Outdoor and Industrial Applications
3/15/2019 L-com Launches Right-Angle USB 3.0 Cable Assemblies with Female Connectors
3/14/2019 L-com Introduces New Right-Angle Panel-Mount DisplayPort Cables
3/12/2019 L-com Unveils New DisplayPort to HDMI Cables with LSZH Jackets
3/5/2019 L-com Debuts New Line of Dual-Rated Slim-Line Ethernet Cables with Spline-Free Design and UL CM Burn Rating
  Page:  1 of 28
    
 
Free Newsletter
L-com Global Connectivity           50 High Street           North Andover, MA 01845
www.L-com.com E-mail: sales@L-com.com 1-800-341-5266 www.Facebook.com/LcomGlobal


© Infinite Electronics International, Inc.