L-com Global Connectivity
  
Cart is Empty
  
USA & Canada (800) 341-5266     International +1 (978) 682-6936

To our valued customers: Our offices will be closed Monday, May 27th, in observance of the Memorial Day Holiday.

Unshielded USB 2.0 Couplers Offer Secure Panel-Mounting to Any Thickness
(Monday, February 27, 2012)
 

Unshielded USB 2.0 Couplers Offer Secure Panel-Mounting to Any Thickness

Black Unshielded USB 2.0 A-A CouplerNORTH ANDOVER, MA - 02/27/12 - L-com, Inc., a designer and manufacturer of wired and wireless connectivity products, has added four new USB 2.0 couplers to its extensive USB component offering. The new couplers, which are unshielded and use the "ECF" style flange-mount design, offer beige and black colored shells with type A to A and type B to A styles.

L-com first announced the shielded type A to A adapters in 2004. These adapters have since become very popular because of their unique ECF design which allows them to be mounted on virtually any panel thickness. However, until now the A to A and B to A styles were only offered with the chrome-colored shielded shells. The new black and beige options expand the USB adapter offering.

"Until recently, the chrome-colored adapters served all applications," said Steve Smith, Product Manager. "Recent customer feedback made it clear that there is a demand for more black and beige unshielded versions."

The new adapters are offered on the L-com web site along with the existing couplers, and will include free 2D engineering drawings and 3D CAD model downloads. They will be stocked in the North Andover, MA fulfillment center for same-day shipment.

Please click here to download a high-resolution version of the image suitable for print publication.

For more information about this release, please contact:
Dave Fallon, Internet Marketing Strategist
978-682-6936 x1450, newsletters@L-com.com

L-com, a global designer and manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as the Hyperlink line of wireless products. Trusted for more than 25 years, L-com, Inc. is headquartered in North Andover, Mass., and is ISO 9001: 2008-certified. For more information, please visit: http://www.L-com.com/

 


Other press releases that may be of interest to you:
 
5/14/2019 L-com Introduces New Cat7 LSZH Cable Assemblies for Shipboard, Aerospace and Defense Applications
5/9/2019 L-com Launches New M12 Field Termination Connectors and In-line Adapters to Address Industrial Networking Applications
5/7/2019 L-com Releases New Cat6a Outdoor-Rated, High-Flex Ethernet Cable Assemblies
4/25/2019 L-com Expands Outdoor Industrial Ethernet Cable Line with Additional Length Options Available with Same-Day Shipping
4/4/2019 L-com Releases New Patch Panels with N-Type Couplers and 0.630” D-Holes
4/2/2019 L-com Adds New Power Cords for Server, PC, Laptop, PDU Applications and More
3/21/2019 L-com now Stocks 12G-SDI, HD-BNC Connectors for use in Broadcast Video Applications
3/19/2019 L-com Launches New Line of Rugged Category 7 Cables with 10 Gig Rating for Outdoor and Industrial Applications
3/15/2019 L-com Launches Right-Angle USB 3.0 Cable Assemblies with Female Connectors
3/14/2019 L-com Introduces New Right-Angle Panel-Mount DisplayPort Cables
3/12/2019 L-com Unveils New DisplayPort to HDMI Cables with LSZH Jackets
3/5/2019 L-com Debuts New Line of Dual-Rated Slim-Line Ethernet Cables with Spline-Free Design and UL CM Burn Rating
2/28/2019 L-com Releases New USB 3.1 Gen 2 Type-C Cables with Low-Smoke Zero-Halogen and PVC Jackets
2/21/2019 L-com Debuts New Cat5e, Cat6 and Cat6a Universal Sub-panels with PoE+ Compliant Jacks
2/14/2019 L-com Introduces New RJ45 Termination Block for Field Termination and Repair Applications
2/12/2019 L-com Debuts New Black and White Flat Cat5e and Cat6 Ethernet Cables
2/7/2019 L-com Releases New Cat5e Double-Shielded Outdoor High-Flex PoE Industrial Ethernet Cables
2/5/2019 L-com Debuts New Fiber LC Couplers with Internal Dustproof Shutters
1/31/2019 L-com Releases Aerial and Outdoor Bulk Cable for use in Demanding OSP Networks
1/29/2019 L-com Now Stocks Moldable M12 Connecters for Rugged Applications
  Page:  1 of 27
    
 
Free Newsletter
L-com Global Connectivity           50 High Street           North Andover, MA 01845
www.L-com.com E-mail: sales@L-com.com 1-800-341-5266 www.Facebook.com/LcomGlobal


© Infinite Electronics International, Inc.