L-com Global Connectivity
  
Cart is Empty
  
USA & Canada (800) 341-5266     International +1 (978) 682-6936
Flange-mount RJ45 Right-Angle Couplers Work on Thicker Panels to Prevent Cable Damage in Tight Spaces
(Thursday, December 15, 2011)
 

Flange-mount RJ45 Right-Angle Couplers Work on Thicker Panels to Prevent Cable Damage in Tight Spaces

RJ45 Flanged Feed-thru Right Angle Coupler KitNORTH ANDOVER, MA – 12/15/11 – L-com, Inc., a global leader in the manufacture of wired and wireless connectivity products, has released a flange-mount version of its popular right-angle RJ45 Cat 5e adapters. The flange-mount design allows secure mounting even on unusually thick panels, and the right-angle feature allows cables to connect through a panel or chassis while minimizing panel depth.

L-com originally released their keystone-mount right-angle RJ45 couplers over a year ago to meet the demand for a solution to Ethernet cables crimping in tight space applications. Keystone couplers fit in a recommended panel thickness of 0.040” to 0.062”. L-com’s ECF-style flanges, however, can be mounted in a panel up to 0.125” thick.

“The ECF-style flanges are popular because they allow design engineers to provide Ethernet jacks on thicker, sturdier surfaces,” said David Gallagher, Product Manager. “Providing an ECF-style version of our right-angle RJ45 couplers is the next step in supporting our customers’ needs.”

The new couplers come shielded or unshielded, offering options to suit different applications.  The mounting frame is solid die-cast metal and 4-40 machine screws are included in the kit for easy assembly. The product is to be stocked in the USA for same-day shipment and 2D engineering drawings are available for free on the L-com web site.

For more information about this release, please contact:
Dave Fallon, Internet Marketing Strategist
978-682-6936 x1450, newsletters@L-com.com

L-com, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as the Hyperlink line of wireless products. Trusted for more than 25 years, L-com, Inc. is headquartered in North Andover, Mass., and is ISO 9001: 2008-certified. For more information, please visit: http://www.L-com.com/

Other press releases that may be of interest to you:
 
5/14/2019 L-com Introduces New Cat7 LSZH Cable Assemblies for Shipboard, Aerospace and Defense Applications
5/9/2019 L-com Launches New M12 Field Termination Connectors and In-line Adapters to Address Industrial Networking Applications
5/7/2019 L-com Releases New Cat6a Outdoor-Rated, High-Flex Ethernet Cable Assemblies
4/25/2019 L-com Expands Outdoor Industrial Ethernet Cable Line with Additional Length Options Available with Same-Day Shipping
4/4/2019 L-com Releases New Patch Panels with N-Type Couplers and 0.630” D-Holes
4/2/2019 L-com Adds New Power Cords for Server, PC, Laptop, PDU Applications and More
3/21/2019 L-com now Stocks 12G-SDI, HD-BNC Connectors for use in Broadcast Video Applications
3/19/2019 L-com Launches New Line of Rugged Category 7 Cables with 10 Gig Rating for Outdoor and Industrial Applications
3/15/2019 L-com Launches Right-Angle USB 3.0 Cable Assemblies with Female Connectors
3/14/2019 L-com Introduces New Right-Angle Panel-Mount DisplayPort Cables
3/12/2019 L-com Unveils New DisplayPort to HDMI Cables with LSZH Jackets
3/5/2019 L-com Debuts New Line of Dual-Rated Slim-Line Ethernet Cables with Spline-Free Design and UL CM Burn Rating
2/28/2019 L-com Releases New USB 3.1 Gen 2 Type-C Cables with Low-Smoke Zero-Halogen and PVC Jackets
2/21/2019 L-com Debuts New Cat5e, Cat6 and Cat6a Universal Sub-panels with PoE+ Compliant Jacks
2/14/2019 L-com Introduces New RJ45 Termination Block for Field Termination and Repair Applications
2/12/2019 L-com Debuts New Black and White Flat Cat5e and Cat6 Ethernet Cables
2/7/2019 L-com Releases New Cat5e Double-Shielded Outdoor High-Flex PoE Industrial Ethernet Cables
2/5/2019 L-com Debuts New Fiber LC Couplers with Internal Dustproof Shutters
1/31/2019 L-com Releases Aerial and Outdoor Bulk Cable for use in Demanding OSP Networks
1/29/2019 L-com Now Stocks Moldable M12 Connecters for Rugged Applications
  Page:  1 of 27
    
 
Free Newsletter
L-com Global Connectivity           50 High Street           North Andover, MA 01845
www.L-com.com E-mail: sales@L-com.com 1-800-341-5266 www.Facebook.com/LcomGlobal


© Infinite Electronics International, Inc.