L-com Global Connectivity
  
Cart is Empty
  
USA & Canada (800) 341-5266     International +1 (978) 682-6936
USB Side-Flange Mount Jacks with 24" Wire Leads Provide Unique Mounting Options
(Friday, December 02, 2011)
 

USB Side-Flange Mount Jacks with 24" Wire Leads Provide Unique Mounting Options

USB 2.0 Side-Flange Mount Connector with 24 inch Wire LeadsNORTH ANDOVER, MA – December 2, 2011 – L-com, Inc., a global leader in the manufacture of wired and wireless connectivity products, has introduced a new USB mounting option with its new UPMA-LEADS and UPMB-LEADS part numbers.  These items use a side-flange to mount the USB jack, and provide 24” long wire leads for custom wiring through panels or enclosures.

L-com has long carried a popular line of “ECJ” style USB jacks for mounting with a flange that extends above and below the connector.  The new jacks provide mounting options for product designs where there is not enough room above or below the jack to mount the connector. They also come with longer leads than the previous styles, and mounting hardware is included.

“We created these new products in response to the increasing demand for designing in USB connectivity to OEM, military, and aerospace equipment,” said Steve Smith, Product Manager. “Our superior manufacturing capabilities allow us to offer our customers more off-the-shelf options for this demand.”

The new jacks will be stocked in North America so they can ship the same day as orders are placed. They will feature 30 microinch gold plating on contacts, 24 AWG UL1007 style tinned copper leads, with one lead connected to the jack shell for shield draining. Engineering drawings and 3D CAD models are available for free on the L-com web site.

For more information about this release, please contact:
Dave Fallon, Internet Marketing Strategist
978-682-6936 x1450, newsletters@L-com.com

L-com, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as the Hyperlink line of wireless products. Trusted for more than 25 years, L-com, Inc. is headquartered in North Andover, Mass., and is ISO 9001: 2008-certified. For more information, please visit: http://www.L-com.com/

Other press releases that may be of interest to you:
 
7/18/2019 L-com Introduces New Active Optical Cables for use in High-Speed Data Center Applications
7/17/2019 L-com Launches New 900 MHz Omni and Sector Antennas
7/16/2019 L-com Unveils Premium 8-Position, A-code, M12 Cable Assemblies for Sensor, Actuator and Fieldbus Applications
7/11/2019 L-com Releases New OM5 Fiber Cables for High-Speed Data Center Applications
6/27/2019 L-com Releases New Small Cell and Outdoor Power Protection Enclosures
6/26/2019 L-com Adds New Premium RJ45 to M12 Female Panel-Mount Cable Assemblies
6/13/2019 L-com Releases New Flat HDMI Cables with LSZH Jackets
5/23/2019 L-com Launches New Indoor and Outdoor-Rated Cat6a Lightning and Surge Protectors
5/14/2019 L-com Introduces New Cat7 LSZH Cable Assemblies for Shipboard, Aerospace and Defense Applications
5/9/2019 L-com Launches New M12 Field Termination Connectors and In-line Adapters to Address Industrial Networking Applications
5/7/2019 L-com Releases New Cat6a Outdoor-Rated, High-Flex Ethernet Cable Assemblies
4/25/2019 L-com Expands Outdoor Industrial Ethernet Cable Line with Additional Length Options Available with Same-Day Shipping
4/4/2019 L-com Releases New Patch Panels with N-Type Couplers and 0.630” D-Holes
4/2/2019 L-com Adds New Power Cords for Server, PC, Laptop, PDU Applications and More
3/21/2019 L-com now Stocks 12G-SDI, HD-BNC Connectors for use in Broadcast Video Applications
3/19/2019 L-com Launches New Line of Rugged Category 7 Cables with 10 Gig Rating for Outdoor and Industrial Applications
3/15/2019 L-com Launches Right-Angle USB 3.0 Cable Assemblies with Female Connectors
3/14/2019 L-com Introduces New Right-Angle Panel-Mount DisplayPort Cables
3/12/2019 L-com Unveils New DisplayPort to HDMI Cables with LSZH Jackets
3/5/2019 L-com Debuts New Line of Dual-Rated Slim-Line Ethernet Cables with Spline-Free Design and UL CM Burn Rating
  Page:  1 of 28
    
 
Free Newsletter
L-com Global Connectivity           50 High Street           North Andover, MA 01845
www.L-com.com E-mail: sales@L-com.com 1-800-341-5266 www.Facebook.com/LcomGlobal


© Infinite Electronics International, Inc.