L-com Global Connectivity
  
Cart is Empty
  
USA & Canada (800) 341-5266     International +1 (978) 682-6936
New USB 2.0 Right-Angle Type B and Mini-B5 Adapters Solve Tight Space Connection Problems
(Wednesday, November 30, 2011)
 

New USB 2.0 Right-Angle Type B and Mini-B5 Adapters Solve Tight Space Connection Problems

Right-Angle USB 2.0 Type B AdapterNORTH ANDOVER, MA – November 30, 2011 – L-com, Inc., a global leader in the manufacture of wired and wireless connectivity products, has introduced new right-angle USB adapters featuring USB type B male to female connectors and USB type mini-B5 male to female connectors.  The new adapters allow cables to plug into USB type B and mini-B5  jacks and cables at right angles without causing damaging bends in the cable.

These right angle adapters follow other recent angled USB products including right-angled USB 2.0 cables, right-angle USB type A adapters, and USB A flexible adapters. Like previous adapter types, the new adapters come in two “exit” styles, allowing the right angle to bend in either direction relative to the connector they are plugged into. The type B adapters use 20 AWG power leads providing maximum power transfer, and both styles use 30 microinch gold contact plating to endure repeated plugging and unplugging of the cable.

“We are finding that strain on cables from bending to fit in tight spaces is an increasing problem,” said Steve Smith, Product Manager. “These adapters are more and more in demand as customers combat this issue.”

These adapters will be stocked in North America for same-day shipment on orders.  They will come molded in PVC and will be 100% shielded to protect from EMI/RFI. Engineering drawings and 3D CAD models will be available for free on the L-com web site.

For more information about this release, please contact:
Dave Fallon, Internet Marketing Strategist
978-682-6936 x1450, newsletters@L-com.com

L-com, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as the Hyperlink line of wireless products. Trusted for more than 25 years, L-com, Inc. is headquartered in North Andover, Mass., and is ISO 9001: 2008-certified. For more information, please visit: http://www.L-com.com/

 


Other press releases that may be of interest to you:
 
8/13/2019 L-com Releases New Cat6 and Cat6a Plenum +105°C, 28AWG, Shielded, Slim Ethernet Patch Cords
8/8/2019 L-com Debuts New UL Listed NEMA-Rated Equipment Enclosures
8/6/2019 New Latching USB 3.0 Cable Assemblies Address Heavy Vibration Applications
8/1/2019 L-com Launches New Triple-Speed Ethernet Switches to Address Industrial Network Applications
7/30/2019 L-com Releases Cat6a Continuous Flex, ZHFR-PUR, Double Shielded Cable Assemblies
7/26/2019 L-com Debuts New Wall-Mount Cabinets and Racks to Address LAN Connectivity Applications
7/25/2019 L-com Introduces new Polycarbonate NEMA-Rated Equipment Enclosures for Wired and Wireless Applications
7/23/2019 L-com Releases New 1U and 2U Cat5e, Cat6 and Cat6a Patch Panels
7/18/2019 L-com Introduces New Active Optical Cables for use in High-Speed Data Center Applications
7/17/2019 L-com Launches New 900 MHz Omni and Sector Antennas
7/16/2019 L-com Unveils Premium 8-Position, A-code, M12 Cable Assemblies for Sensor, Actuator and Fieldbus Applications
7/11/2019 L-com Releases New OM5 Fiber Cables for High-Speed Data Center Applications
6/27/2019 L-com Releases New Small Cell and Outdoor Power Protection Enclosures
6/26/2019 L-com Adds New Premium RJ45 to M12 Female Panel-Mount Cable Assemblies
6/13/2019 L-com Releases New Flat HDMI Cables with LSZH Jackets
5/23/2019 L-com Launches New Indoor and Outdoor-Rated Cat6a Lightning and Surge Protectors
5/14/2019 L-com Introduces New Cat7 LSZH Cable Assemblies for Shipboard, Aerospace and Defense Applications
5/9/2019 L-com Launches New M12 Field Termination Connectors and In-line Adapters to Address Industrial Networking Applications
5/7/2019 L-com Releases New Cat6a Outdoor-Rated, High-Flex Ethernet Cable Assemblies
4/25/2019 L-com Expands Outdoor Industrial Ethernet Cable Line with Additional Length Options Available with Same-Day Shipping
  Page:  1 of 28
    
 
Free Newsletter
L-com Global Connectivity           50 High Street           North Andover, MA 01845
www.L-com.com E-mail: sales@L-com.com 1-800-341-5266 www.Facebook.com/LcomGlobal


© Infinite Electronics International, Inc.