L-com Global Connectivity
  
Cart is Empty
  
USA & Canada (800) 341-5266     International +1 (978) 682-6936
Indoor Lightning and Surge Protectors Mount On Standard In-Wall Electrical/Conduit Boxes
(Monday, November 14, 2011)
 

Indoor Lightning and Surge Protectors Mount On Standard In-Wall Electrical/Conduit Boxes

Wall Plate Lightning ProtectorNORTH ANDOVER, MA – November 14, 2011– L-com, Inc., a global leader in the manufacture of wired and wireless connectivity products, has developed lightning and surge protectors that are pre-mounted in stainless steel wall plates designed to mount to standard in-wall electrical/conduit boxes.  The new products offer an aesthetic solution to lightning and surge protection in homes and offices.

Previously, providing protection required mounting the protector on a wall or shelf and running extra cables to and from the protector. This new solution is perfect for new construction and buildings with existing in-wall Ethernet and telephone/DSL wiring. The four new items include protection for Cat5, Cat5e, and Cat6 lines, shielded or unshielded, as well as telephone, DSL, and T1 lines. 

“Providing protection from lightning and electrical surges is crucial to home and business owners,” said Patrick Pesa, Director of Product Management. “But running extra wires and mounting a large protector is not acceptable in many situations. The new WP series allows customers to safely and aesthetically protect their electronic equipment.”

The new Cat5, Cat5e, and Cat6 protectors are PoE compatible.  The telephone, DSL and T1 protectors feature superior three-stage protection using a Thyristor diode technology.

For more information about this release, please contact:
Dave Fallon, Internet Marketing Strategist
978-682-6936 x1450, newsletters@L-com.com

L-com, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as the Hyperlink line of wireless products. Trusted for more than 25 years, L-com, Inc. is headquartered in North Andover, Mass., and is ISO 9001: 2008-certified. For more information, please visit: http://www.L-com.com/.


Other press releases that may be of interest to you:
 
8/13/2019 L-com Releases New Cat6 and Cat6a Plenum +105°C, 28AWG, Shielded, Slim Ethernet Patch Cords
8/8/2019 L-com Debuts New UL Listed NEMA-Rated Equipment Enclosures
8/6/2019 New Latching USB 3.0 Cable Assemblies Address Heavy Vibration Applications
8/1/2019 L-com Launches New Triple-Speed Ethernet Switches to Address Industrial Network Applications
7/30/2019 L-com Releases Cat6a Continuous Flex, ZHFR-PUR, Double Shielded Cable Assemblies
7/26/2019 L-com Debuts New Wall-Mount Cabinets and Racks to Address LAN Connectivity Applications
7/25/2019 L-com Introduces new Polycarbonate NEMA-Rated Equipment Enclosures for Wired and Wireless Applications
7/23/2019 L-com Releases New 1U and 2U Cat5e, Cat6 and Cat6a Patch Panels
7/18/2019 L-com Introduces New Active Optical Cables for use in High-Speed Data Center Applications
7/17/2019 L-com Launches New 900 MHz Omni and Sector Antennas
7/16/2019 L-com Unveils Premium 8-Position, A-code, M12 Cable Assemblies for Sensor, Actuator and Fieldbus Applications
7/11/2019 L-com Releases New OM5 Fiber Cables for High-Speed Data Center Applications
6/27/2019 L-com Releases New Small Cell and Outdoor Power Protection Enclosures
6/26/2019 L-com Adds New Premium RJ45 to M12 Female Panel-Mount Cable Assemblies
6/13/2019 L-com Releases New Flat HDMI Cables with LSZH Jackets
5/23/2019 L-com Launches New Indoor and Outdoor-Rated Cat6a Lightning and Surge Protectors
5/14/2019 L-com Introduces New Cat7 LSZH Cable Assemblies for Shipboard, Aerospace and Defense Applications
5/9/2019 L-com Launches New M12 Field Termination Connectors and In-line Adapters to Address Industrial Networking Applications
5/7/2019 L-com Releases New Cat6a Outdoor-Rated, High-Flex Ethernet Cable Assemblies
4/25/2019 L-com Expands Outdoor Industrial Ethernet Cable Line with Additional Length Options Available with Same-Day Shipping
  Page:  1 of 28
    
 
Free Newsletter
L-com Global Connectivity           50 High Street           North Andover, MA 01845
www.L-com.com E-mail: sales@L-com.com 1-800-341-5266 www.Facebook.com/LcomGlobal


© Infinite Electronics International, Inc.