L-com Global Connectivity
  
Cart is Empty
  
USA & Canada (800) 341-5266     International +1 (978) 682-6936
 
4-20 mA Current Loop Lightning and Surge Protectors Prevent Costly Device Repairs
(Wednesday, May 04, 2011)
 

4-20 mA current loop protectorNORTH ANDOVER, MA – 05/04/2011 – L-com, Inc., a global leader in the manufacture of wired and wireless connectivity products, now carries a complete line of 4-20 mA current loop lightning and surge protectors.  The new protectors can minimize risks to expensive sensors and process controllers by lightning strikes or power surges.

“Current loops are ideal for analog and data transmission because of their inherent insensitivity to electrical noise,” said Patrick Pesa, product manager. “With the introduction of a complete family of 4-20 mA surge protectors at competitive prices, customers need not look further than L-com.”

All of the new models are available in 12V, 15V and 24V configurations, and in indoor, outdoor, and industrial grades. Most of them provide three-stage protection using screw terminals.

For more information about this release, please contact:
Dave Fallon, Internet Marketing Strategist
978-682-6936 x1450, newsletters@L-com.com

L-com, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their Hyperlink line of wireless products which include Antennas, RF Amplifiers, Coaxial lightning and surge protectors, and NEMA rated enclosures.  L-com’s HyperLink wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n, RFID and Bluetooth applications. Trusted for over 25 years, L-com, Inc, which is headquartered in North Andover, MA, is ISO 9001: 2008 certified and many of its products are UL® recognized. http://www.L-com.com/


Other press releases that may be of interest to you:
 
2/14/2019 L-com Introduces New RJ45 Termination Block for Field Termination and Repair Applications
2/12/2019 L-com Debuts New Black and White Flat Cat5e and Cat6 Ethernet Cables
2/7/2019 L-com Releases New Cat5e Double-Shielded Outdoor High-Flex PoE Industrial Ethernet Cables
2/5/2019 L-com Debuts New Fiber LC Couplers with Internal Dustproof Shutters
1/31/2019 L-com Releases Aerial and Outdoor Bulk Cable for use in Demanding OSP Networks
1/29/2019 L-com Now Stocks Moldable M12 Connecters for Rugged Applications
1/24/2019 L-com Debuts New Low-Smoke Zero-Halogen 3.5mm Audio Cables
1/22/2019 L-com Introduces New Time Saving Pull-Through RJ45 Plugs and Crimp Tool
1/17/2019 L-com Releases IP68-Rated USB 2.0 Cable Assemblies and Panel-Mount Coupler
1/15/2019 L-com Reveals New Premium Shielded Plenum Cat6a Cable Assemblies and Bulk Cable
1/10/2019 L-com Launches New Active Optical USB 3.0 Cables that Support 20 Meter Distances
10/16/2018 L-com Releases New Line of High-Temp, Aerospace-Rated Ethernet Cable Assemblies
9/27/2018 L-com Debuts Low-Smoke Zero-Halogen USB 2.0 Cables with Ferrites
9/25/2018 L-com Introduces new DVI to DisplayPort Cable Assemblies
8/14/2018 L-com Launches Cat5e Braid Shielded High-Flex Right Angle Ethernet Patch Cords
8/7/2018 L-com Releases USB 3.0 Cables with Ferrites and LSZH Cable Jackets
7/24/2018 L-com Launches High Speed HDMI Cable Assemblies with White Jackets and Connector Overmolds
7/19/2018 L-com Now Stocks Right Angle M12 Cable Assemblies for Confined Space Industrial Connectivity Applications
7/17/2018 L-com Introduces New Flat HDMI Cables for Tight Space A/V Applications
7/12/2018 L-com Introduces New IP67 Rated HDMI Cables and Coupler for Extreme Connectivity Applications
  Page:  1 of 26
    
 
Free Newsletter
L-com Global Connectivity           50 High Street           North Andover, MA 01845
www.L-com.com E-mail: sales@L-com.com 1-800-341-5266 www.Facebook.com/LcomGlobal


© Infinite Electronics International, Inc.