L-com Global Connectivity
  
Cart is Empty
  
USA & Canada (800) 341-5266     International +1 (978) 682-6936
L-com's New LSZH USB Bulk Cable Serves Military/Aerospace Applications
(Wednesday, February 16, 2011)
 

LSZH USB Bulk CableNORTH ANDOVER, MA – 02/16/2011 – L-com, Inc., a global leader in the manufacture of wired and wireless connectivity products, now sells bulk USB 2.0 cable with a Low Smoke Zero Halogen (LSZH) jacket. The new product is identical to L-com’s standard PVC USB Bulk Cable, except that the jacket is black and, when burned, the LSZH jacket will not produce toxic smoke.

The USB Bulk Cable can be used with L-com’s Type A and Type B USB connectors and hoods to manufacture custom USB cables if desired. L-com can also manufacture custom USB cables using this bulk cable with modest minimum order quantities.

“All LSZH products appeal to military customers and military subcontractors because they significantly reduce the amount of toxic gases emitted during combustion when compared to PVC,” said Steve Smith, Product Manager. “This is essential for confined areas like aircraft, submarines and shipboard. This is the same cable that is used in our popular CSUZAB and CSUZAA cable assemblies.”

LSZH hoods for the connectors will be available in about six weeks.

For more information about this release, please contact:
Dave Fallon, Internet Marketing Strategist
978-682-6936 x1450,
newsletters@L-com.com

L-com, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their Hyperlink line of wireless products which include Antennas, RF Amplifiers, Coaxial lightning and surge protectors, and NEMA rated enclosures. L-com’s HyperLink wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n, RFID and Bluetooth applications. Trusted for over 25 years, L-com, Inc, which is headquartered in North Andover, MA, is ISO 9001: 2008 certified and many of its products are UL® recognized. http://www.L-com.com/


Other press releases that may be of interest to you:
 
8/13/2019 L-com Releases New Cat6 and Cat6a Plenum +105°C, 28AWG, Shielded, Slim Ethernet Patch Cords
8/8/2019 L-com Debuts New UL Listed NEMA-Rated Equipment Enclosures
8/6/2019 New Latching USB 3.0 Cable Assemblies Address Heavy Vibration Applications
8/1/2019 L-com Launches New Triple-Speed Ethernet Switches to Address Industrial Network Applications
7/30/2019 L-com Releases Cat6a Continuous Flex, ZHFR-PUR, Double Shielded Cable Assemblies
7/26/2019 L-com Debuts New Wall-Mount Cabinets and Racks to Address LAN Connectivity Applications
7/25/2019 L-com Introduces new Polycarbonate NEMA-Rated Equipment Enclosures for Wired and Wireless Applications
7/23/2019 L-com Releases New 1U and 2U Cat5e, Cat6 and Cat6a Patch Panels
7/18/2019 L-com Introduces New Active Optical Cables for use in High-Speed Data Center Applications
7/17/2019 L-com Launches New 900 MHz Omni and Sector Antennas
7/16/2019 L-com Unveils Premium 8-Position, A-code, M12 Cable Assemblies for Sensor, Actuator and Fieldbus Applications
7/11/2019 L-com Releases New OM5 Fiber Cables for High-Speed Data Center Applications
6/27/2019 L-com Releases New Small Cell and Outdoor Power Protection Enclosures
6/26/2019 L-com Adds New Premium RJ45 to M12 Female Panel-Mount Cable Assemblies
6/13/2019 L-com Releases New Flat HDMI Cables with LSZH Jackets
5/23/2019 L-com Launches New Indoor and Outdoor-Rated Cat6a Lightning and Surge Protectors
5/14/2019 L-com Introduces New Cat7 LSZH Cable Assemblies for Shipboard, Aerospace and Defense Applications
5/9/2019 L-com Launches New M12 Field Termination Connectors and In-line Adapters to Address Industrial Networking Applications
5/7/2019 L-com Releases New Cat6a Outdoor-Rated, High-Flex Ethernet Cable Assemblies
4/25/2019 L-com Expands Outdoor Industrial Ethernet Cable Line with Additional Length Options Available with Same-Day Shipping
  Page:  1 of 28
    
 
Free Newsletter
L-com Global Connectivity           50 High Street           North Andover, MA 01845
www.L-com.com E-mail: sales@L-com.com 1-800-341-5266 www.Facebook.com/LcomGlobal


© Infinite Electronics International, Inc.