L-com Global Connectivity
  
Cart is Empty
  
USA & Canada (800) 341-5266     International +1 (978) 682-6936
Coax Cable Assemblies Featuring FME Connectors Now Available from L-com
(Wednesday, February 02, 2011)
 

Coax Cable Assemblies Featuring FME ConnectorsNORTH ANDOVER, MA – 2/2/2011 – L-com, Inc., a global leader in the manufacture of wired and wireless connectivity products is now offering low-loss coax cable assemblies featuring FME (For Mobile Equipment) connectors. These miniature 50Ω RF connectors allow cables to be snaked through tight access holes or spaces. FME connectors are commonly used in cellular communication devices as well as low frequency mobile antenna applications.

"FME connectors are the perfect complement to our already broad coax line," said Patrick Pesa, Product Manager. "They are popular because they have screw-down termination like the SMA connector, but are low-profile to fit through holes. I think our customers will be glad we added them."

These high-quality, fully-tested cable assemblies are built with L-com's CA-195 low-loss coax cable. Standard assemblies include FME to FME and FME to BNC. Along with standard cable assemblies, custom cable assemblies can be configured using the on-line Product Configurator.

For more information about this release, please contact:
Dave Fallon, Internet Marketing Strategist

978-682-6936 x1450, mailto:newsletters@L-com.com

To see all of our press releases, click here.

L-com, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their Hyperlink line of wireless products which include Antennas, RF Amplifiers, Coaxial lightning and surge protectors, and NEMA rated enclosures. L-com's HyperLink wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n, RFID and Bluetooth applications. Trusted for over 25 years, L-com, Inc, which is headquartered in North Andover, MA, is ISO 9001: 2008 certified and many of its products are UL® recognized. http://www.L-com.com/


Other press releases that may be of interest to you:
 
8/13/2019 L-com Releases New Cat6 and Cat6a Plenum +105°C, 28AWG, Shielded, Slim Ethernet Patch Cords
8/8/2019 L-com Debuts New UL Listed NEMA-Rated Equipment Enclosures
8/6/2019 New Latching USB 3.0 Cable Assemblies Address Heavy Vibration Applications
8/1/2019 L-com Launches New Triple-Speed Ethernet Switches to Address Industrial Network Applications
7/30/2019 L-com Releases Cat6a Continuous Flex, ZHFR-PUR, Double Shielded Cable Assemblies
7/26/2019 L-com Debuts New Wall-Mount Cabinets and Racks to Address LAN Connectivity Applications
7/25/2019 L-com Introduces new Polycarbonate NEMA-Rated Equipment Enclosures for Wired and Wireless Applications
7/23/2019 L-com Releases New 1U and 2U Cat5e, Cat6 and Cat6a Patch Panels
7/18/2019 L-com Introduces New Active Optical Cables for use in High-Speed Data Center Applications
7/17/2019 L-com Launches New 900 MHz Omni and Sector Antennas
7/16/2019 L-com Unveils Premium 8-Position, A-code, M12 Cable Assemblies for Sensor, Actuator and Fieldbus Applications
7/11/2019 L-com Releases New OM5 Fiber Cables for High-Speed Data Center Applications
6/27/2019 L-com Releases New Small Cell and Outdoor Power Protection Enclosures
6/26/2019 L-com Adds New Premium RJ45 to M12 Female Panel-Mount Cable Assemblies
6/13/2019 L-com Releases New Flat HDMI Cables with LSZH Jackets
5/23/2019 L-com Launches New Indoor and Outdoor-Rated Cat6a Lightning and Surge Protectors
5/14/2019 L-com Introduces New Cat7 LSZH Cable Assemblies for Shipboard, Aerospace and Defense Applications
5/9/2019 L-com Launches New M12 Field Termination Connectors and In-line Adapters to Address Industrial Networking Applications
5/7/2019 L-com Releases New Cat6a Outdoor-Rated, High-Flex Ethernet Cable Assemblies
4/25/2019 L-com Expands Outdoor Industrial Ethernet Cable Line with Additional Length Options Available with Same-Day Shipping
  Page:  1 of 28
    
 
Free Newsletter
L-com Global Connectivity           50 High Street           North Andover, MA 01845
www.L-com.com E-mail: sales@L-com.com 1-800-341-5266 www.Facebook.com/LcomGlobal


© Infinite Electronics International, Inc.