L-com Global Connectivity
  
Cart is Empty
  
USA & Canada (800) 341-5266     International +1 (978) 682-6936
L-com Expands LSZH D-subminiature Cable Line with LSZH DB15 Cable Assemblies
(Thursday, September 23, 2010)
 
Low Smoke Zero Halogen (LSZH) 15 Pin D-Sub Cables - Male to Male, Fully Populated, Double Shielded

NORTH ANDOVER, MA – 9/22/2010 – L-com, Inc, a global leader in the manufacture of wired and wireless connectivity products, has developed new DB15 male to male and male to female cable assemblies with black low-smoke zero-halogen (LSZH) jackets. The new cables join L-com’s existing DB25 and DB9 cables with LSZH jackets.

All LSZH jacketed cables are ideal for military and military-subcontracting customers because they significantly reduce the amount of toxic gases emitted during combustion when compared with standard PVC jackets. This is essential for confined areas like aircraft, submarines and shipboard.

“The men and women of our military absolutely require—and benefit from--LSZH jacketed cables,” said Steve Smith, L-com’s product manager in charge of D-sub products. “To use PVC in an enclosed space is unthinkable. I’m glad L-com is able to support our military’s efforts with quality-built LSZH D-subminiature products.”

All of L-com’s LSZH D-sub cables have 24AWG conductors, allowing users to send more current down the cables, as opposed to their standard D-sub cables (CSM, CSMN, and CS2N), which have 26AWG conductors.

For more information about this release, please contact:
Dave Fallon, Internet Marketing Strategist
978-682-6936 x1450, newsletters@L-com.com

L-com, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their Hyperlink line of wireless products which include Antennas, RF Amplifiers, Coaxial lightning and surge protectors, and NEMA rated enclosures. L-com’s HyperLink wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n, RFID and Bluetooth applications. Trusted for over 25 years, L-com, which is headquartered in North Andover, MA, is ISO 9001: 2008 certified and many of its products are UL® recognized.

 


Other press releases that may be of interest to you:
 
7/18/2019 L-com Introduces New Active Optical Cables for use in High-Speed Data Center Applications
7/17/2019 L-com Launches New 900 MHz Omni and Sector Antennas
7/16/2019 L-com Unveils Premium 8-Position, A-code, M12 Cable Assemblies for Sensor, Actuator and Fieldbus Applications
7/11/2019 L-com Releases New OM5 Fiber Cables for High-Speed Data Center Applications
6/27/2019 L-com Releases New Small Cell and Outdoor Power Protection Enclosures
6/26/2019 L-com Adds New Premium RJ45 to M12 Female Panel-Mount Cable Assemblies
6/13/2019 L-com Releases New Flat HDMI Cables with LSZH Jackets
5/23/2019 L-com Launches New Indoor and Outdoor-Rated Cat6a Lightning and Surge Protectors
5/14/2019 L-com Introduces New Cat7 LSZH Cable Assemblies for Shipboard, Aerospace and Defense Applications
5/9/2019 L-com Launches New M12 Field Termination Connectors and In-line Adapters to Address Industrial Networking Applications
5/7/2019 L-com Releases New Cat6a Outdoor-Rated, High-Flex Ethernet Cable Assemblies
4/25/2019 L-com Expands Outdoor Industrial Ethernet Cable Line with Additional Length Options Available with Same-Day Shipping
4/4/2019 L-com Releases New Patch Panels with N-Type Couplers and 0.630” D-Holes
4/2/2019 L-com Adds New Power Cords for Server, PC, Laptop, PDU Applications and More
3/21/2019 L-com now Stocks 12G-SDI, HD-BNC Connectors for use in Broadcast Video Applications
3/19/2019 L-com Launches New Line of Rugged Category 7 Cables with 10 Gig Rating for Outdoor and Industrial Applications
3/15/2019 L-com Launches Right-Angle USB 3.0 Cable Assemblies with Female Connectors
3/14/2019 L-com Introduces New Right-Angle Panel-Mount DisplayPort Cables
3/12/2019 L-com Unveils New DisplayPort to HDMI Cables with LSZH Jackets
3/5/2019 L-com Debuts New Line of Dual-Rated Slim-Line Ethernet Cables with Spline-Free Design and UL CM Burn Rating
  Page:  1 of 28
    
 
Free Newsletter
L-com Global Connectivity           50 High Street           North Andover, MA 01845
www.L-com.com E-mail: sales@L-com.com 1-800-341-5266 www.Facebook.com/LcomGlobal


© Infinite Electronics International, Inc.