L-com Global Connectivity
  
Cart is Empty
  
USA & Canada (800) 341-5266     International +1 (978) 682-6936
L-com Releases IP67 RJ45 Cables, Feed-Thru Adapters, and Strain Reliefs
(Thursday, May 06, 2010)
 

IP67 rated RJ45 Industrial Ethernet cablesNORTH ANDOVER, MA – 5/6/2010 – L-com, Inc., a global leader in the manufacture of wired and wireless connectivity products, announced today the release of a new series of IP67 rated RJ45 Industrial Ethernet cables, panel mount IP67 RJ45 jacks (feed-thru and 110 styles), and IP67 long and short body RJ45 strain reliefs. These IP67 rated products are designed for use in harsh environments where dust and moisture are present.

  • The TRD5WP cable series features UV and chemical resistant PUR jackets as well as shielding to protect against EMI/RFI.
  • The WPRJ series panel mount jacks feature straight and 90 degree shielded feed-thru options as well as a 110 style punch down version.
  • The WPRJ-XSR series features long and short body IP67 rated strain reliefs which can be used to build your own IP67 rated Industrial Ethernet cable assemblies.

“Our new IP67 series of cable assemblies and panel mount jacks were created to address the ever growing Industrial Ethernet market. By offering these high quality, competitively priced IP67 products, we have further enhanced our already extensive line of IP rated Ethernet products. By giving our customers more choices we are able to address new application requirements.” said Peter McNeil, L-com’s Telecom Product Manager.

For more information about this release, please contact:
Dave Fallon, Internet Marketing Strategist
978-682-6936 x1450,
newsletters@L-com.com

L-com, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their Hyperlink line of wireless products which include Antennas, RF Amplifiers, Coaxial lightning and surge protectors, and NEMA rated enclosures. L-com’s HyperLink wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n, RFID and Bluetooth applications. Trusted for over 25 years, L-com, which is headquartered in North Andover, MA, is ISO 9001: 2008 certified and many of its products are UL® recognized.

http://www.L-com.com/

 


Other press releases that may be of interest to you:
 
1/18/2018 L-com Introduces New Cat6a Low-Smoke Zero-Halogen Cable Assemblies and Bulk Cable
11/28/2017 L-com Releases a New Line of Versatile HDMI Adapters
11/14/2017 L-com Launches New USB 2.0 ECF-Style Panel Mount USB Adapter Cables
10/26/2017 L-com Introduces New Line of Universal Sub-Panels with USB, DisplayPort and Cat6a RJ45 Couplers
10/25/2017 L-com Releases New M12 Connectors, Coupler and Receptacles
10/24/2017 L-com Debuts New Windowed NEMA Enclosures
10/5/2017 L-com Launches New USB 3.0 High-Flex Cable Assemblies
10/3/2017 L-com Introduces Ruggedized IP68-Rated Cat6 Receptacles, Plugs and Jam Nuts
9/28/2017 L-com Debuts New USB 3.0 ECF-Style Panel Mount USB Adapter Cables
9/19/2017 L-com Introduces New USB 3.0 Armored Cables for Extreme Environments
9/14/2017 L-com Releases New USB 3.0 Bulk Cable
8/29/2017 L-com Debuts New High Flex HDMI Cable Assemblies
8/24/2017 L-com Launches new USB 2.0 and 3.0 Cables with Ferrite Beads
8/22/2017 L-com Introduces New Mini-HDMI to Mini-HDMI Cables
7/25/2017 L-com Releases IP68 Fiber Plugs, Receptacles and Jam Nuts
7/18/2017 L-com Debuts New Line of Space Saving Mini-Coupler Patch Panels
7/11/2017 L-com Launches New Line of IP68-Rated Cable Glands and Couplers
6/29/2017 L-com Introduces Cat6 Low-Smoke Zero-Halogen Cable Assemblies
6/22/2017 L-com Expands Portfolio of Outdoor Cables for Industrial Ethernet Applications
6/20/2017 L-com Releases Cat5e TPE and PUR High Flex Outdoor Industrial Ethernet Cables
  Page:  1 of 25
    
 
Free Newsletter
L-com Global Connectivity           50 High Street           North Andover, MA 01845
www.L-com.com E-mail: sales@L-com.com 1-800-341-5266 www.Facebook.com/LcomGlobal


© L-com, Inc. All Rights Reserved. L-com, Inc., 50 High Street, West Mill, 3rd Floor, Suite #30, North Andover, MA 01845
an Infinite company