NORTH ANDOVER, MA – 3/8/2010 – L-com, Inc., a leading manufacturer of both wired and wireless connectivity products, announced today the availability of a new line of actively cooled and ventilated NEMA enclosures based on the company's extremely popular NBP141004-100 model.
In this new line of NEMA enclosures, L-com has modified its base model to include a number of heat-dissipating features, including multiple rain shielded vents and active cooling fans controlled by thermostats. These enclosures assure cooling in outdoor applications, protecting equipment from the elements and heat buildup. The new enclosures come in 120VAC, 240VAC Universal Plug EURO, and Power over Ethernet (PoE) versions.
L-com, Inc., a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their Hyperlink line of wireless products which include Antennas, RF Amplifiers, Coaxial lightning and surge protectors, and NEMA rated enclosures. L-com’s HyperLink wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n, RFID and Bluetooth applications. Trusted for over 25 years, L-com, which is headquartered in North Andover, MA, is ISO 9001: 2008 certified and many of its products are UL® recognized.
http://www.L-com.com/
L-com Global Connectivity 45 Beechwood Drive North Andover, MA 01845www.L-com.com E-mail: sales@L-com.com Phone: 1-800-341-5266 Fax: 1-978-689-9484