L-com Global Connectivity
  
Cart is Empty
  
USA & Canada (800) 341-5266     International +1 (978) 682-6936
New Field Termination USB Connector and Shielded USB Coupler from L-com
(Thursday, July 23, 2009)
 

North Andover, MA – July 23, 2009 –  L-com, a global leader in the manufacture of wired and wireless connectivity products today announced the release of two new USB products. 

The USBAFT is a unique field terminate USB Type A connector that is designed to be used in the field for quick and easy terminations. Separate connection points are provided for all four positions of the connector plus the ground. Terminal block design with set screws provides reliable electrical connections utilizing no special tools. The terminal block area is clearly marked making proper termination virtually foolproof. The USBAFT is panel mountable using 4-40 screws provided

  L-com USB Field Termination Connector

L-com's UADKEY-AB shielded USB keystone coupler can be easily installed into panels, wall plate openings and enclosures. The UADKEY-AB features a USB A female connector on the front and USB B female connector on the back of the coupler housing. The stamped metal shell and one piece design provides maximum protection from data corrupting EMI/RFI.

 L-com Sheilded USB Keystone Coupler

For more information about this release, please contact:
Steve Smith, Product Manager
978-682-6936 x1156, ssmith@L-com.com

About L-com

L-com, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their Hyperlink line of wireless products which include Antennas, RF Amplifiers, Coaxial lightning and surge protectors, and NEMA rated enclosures.  L-com’s HyperLink wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n, RFID and Bluetooth applications. Trusted for over 25 years, L-com, which is headquartered in North Andover, MA, is ISO 9001: 2000 certified and many of its products are UL® recognized. www.l-com.com

Other press releases that may be of interest to you:
 
7/18/2019 L-com Introduces New Active Optical Cables for use in High-Speed Data Center Applications
7/17/2019 L-com Launches New 900 MHz Omni and Sector Antennas
7/16/2019 L-com Unveils Premium 8-Position, A-code, M12 Cable Assemblies for Sensor, Actuator and Fieldbus Applications
7/11/2019 L-com Releases New OM5 Fiber Cables for High-Speed Data Center Applications
6/27/2019 L-com Releases New Small Cell and Outdoor Power Protection Enclosures
6/26/2019 L-com Adds New Premium RJ45 to M12 Female Panel-Mount Cable Assemblies
6/13/2019 L-com Releases New Flat HDMI Cables with LSZH Jackets
5/23/2019 L-com Launches New Indoor and Outdoor-Rated Cat6a Lightning and Surge Protectors
5/14/2019 L-com Introduces New Cat7 LSZH Cable Assemblies for Shipboard, Aerospace and Defense Applications
5/9/2019 L-com Launches New M12 Field Termination Connectors and In-line Adapters to Address Industrial Networking Applications
5/7/2019 L-com Releases New Cat6a Outdoor-Rated, High-Flex Ethernet Cable Assemblies
4/25/2019 L-com Expands Outdoor Industrial Ethernet Cable Line with Additional Length Options Available with Same-Day Shipping
4/4/2019 L-com Releases New Patch Panels with N-Type Couplers and 0.630” D-Holes
4/2/2019 L-com Adds New Power Cords for Server, PC, Laptop, PDU Applications and More
3/21/2019 L-com now Stocks 12G-SDI, HD-BNC Connectors for use in Broadcast Video Applications
3/19/2019 L-com Launches New Line of Rugged Category 7 Cables with 10 Gig Rating for Outdoor and Industrial Applications
3/15/2019 L-com Launches Right-Angle USB 3.0 Cable Assemblies with Female Connectors
3/14/2019 L-com Introduces New Right-Angle Panel-Mount DisplayPort Cables
3/12/2019 L-com Unveils New DisplayPort to HDMI Cables with LSZH Jackets
3/5/2019 L-com Debuts New Line of Dual-Rated Slim-Line Ethernet Cables with Spline-Free Design and UL CM Burn Rating
  Page:  1 of 28
    
 
Free Newsletter
L-com Global Connectivity           50 High Street           North Andover, MA 01845
www.L-com.com E-mail: sales@L-com.com 1-800-341-5266 www.Facebook.com/LcomGlobal


© Infinite Electronics International, Inc.