L-com Global Connectivity
  
Cart is Empty
  
USA & Canada (800) 341-5266     International +1 (978) 682-6936

To our valued customers: Our offices will be closed Monday, May 28th, in observance of the Memorial Day holiday.

L-com Announces HyperLink Brand 2.4 GHz 9 dBi Omni-Directional Antenna with 7 Degree Down-Tilt
(Monday, February 23, 2009)
 

North Andover, MA – February 23, 2009 – L-com Global Connectivity, a leading manufactureHyperLink Brand 2.4 GHz 9 dBi Omni-Directional Antennar and distributor of HyperLink brand antennas, amplifiers, waterproof enclosures, and other wireless connection equipment, announced their new 2.4 GHz 9 dBi Omni-Directional Antenna with 7° Down-Tilt.

The HyperGain HG2409UDT-PRO high-performance down-tilt Omni-directional antenna provides 9.0 dBi gain and a down-tilt of 7° for long-range, downward biased pattern to aid in Omni coverage in the close-in areas of applications. This includes point to multi-point systems, and wireless bridges in the 2.4 GHz ISM band as well as IEEE 802.11b and 802.11g. It can be installed for coverage over a wider low angle range than a conventional Omni-directional antenna.

This 9dBi Omni-directional antenna's construction features a stainless steel base, fiberglass radome and rugged mounting hardware for superior strength and light weight installation. The antenna's integrated connector permits simple installation and ease of hookup with the systems radio.

The HG2409UDT-PRO compliments the successful family of broad coverage antennas that include the popular Sectorial Omni-Directional Array and panel antennas, such as HK2414-090 and HK215-180 models, offering customers the option to select the antenna that best fits their network and communication requirements.

Orders for the HG2409UDT-PRO can be taken now, with expected delivery from stock.

For more information about this release, please contact:
Karl Blomgren, Product Manager
561.995.2256 x7183, mailto:kblomgren@hyperlinktech.com

L-com, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their Hyperlink line of wireless products which include Antennas, RF Amplifiers, Coaxial lightning and surge protectors, and NEMA rated enclosures.  L-com’s HyperLink wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n, RFID and Bluetooth applications. Trusted for over 25 years, L-com, which is headquartered in North Andover, MA, is ISO 9001: 2000 certified and many of its products are UL® recognized. www.l-com.com


Other press releases that may be of interest to you:
 
5/25/2018 L-com Releases New High-Flex, Continuous Motion, Braided Shield Ethernet Cable Assemblies
5/23/2018 L-com Debuts New Tool-less RJ45 Jacks with PoE+ Compliance
5/3/2018 L-com Introduces a New Series of Data-line Lightning and Surge Protectors for Ethernet and Serial Data Applications
4/26/2018 L-com Now Stocks Icron Technologies’ New Raven USB 3-2-1 Extenders
4/25/2018 L-com Launches New Line of Coaxial RF Lightning and Surge Protectors
4/9/2018 L-com Introduces New IP67 Category5e/6 Dual Use Waterproof Ethernet Cables
3/8/2018 L-com Releases USB 2.0 Type-C Cables with Panel-Mount Connectors
3/6/2018 L-com Launches New 20-Pin DisplayPort Cables with Power Support
3/5/2018 L-com Appoints M-RF Co., Ltd. as Authorized Distributor in Japan
2/27/2018 L-com Now Stocking High-Flex USB 3.0 Cable Assemblies with Type-A to Type-C Connectors
2/22/2018 L-com Introduces New Low-Smoke Zero-Halogen USB 2.0 Bulk Cable with 28/28 AWG Conductors
2/20/2018 L-com Releases Cat5e/6 Patch Panels with PoE + Interfaces
2/15/2018 L-com Launches New IP67-Rated Industrial USB 3.0 Cable Assemblies and Coupler
1/31/2018 L-com Now Offers Waterproof IP67-Rated USB Type-A/A Cable Assemblies
1/30/2018 L-com Unveils New Extended-Length Active HDMI Cables
1/26/2018 L-com Releases M12 and M8 Field Term Connectors, Couplers, Adapters and Receptacles
1/25/2018 L-com Launches New Plenum Rated, Shielded Cat6 Cable Assemblies with 23 AWG Solid Conductors
1/18/2018 L-com Introduces New Cat6a Low-Smoke Zero-Halogen Cable Assemblies and Bulk Cable
11/28/2017 L-com Releases a New Line of Versatile HDMI Adapters
11/14/2017 L-com Launches New USB 2.0 ECF-Style Panel Mount USB Adapter Cables
  Page:  1 of 25
    
 
Free Newsletter
L-com Global Connectivity           50 High Street           North Andover, MA 01845
www.L-com.com E-mail: sales@L-com.com 1-800-341-5266 www.Facebook.com/LcomGlobal


© Infinite Electronics International, Inc.
an Infinite company