L-com Global Connectivity
  
Cart is Empty
  
USA & Canada (800) 341-5266     International +1 (978) 682-6936
L-com Adds Two New Cable Assemblies to Their USB Line
(Monday, July 14, 2008)
 

USB type A female horizontal mount to USB type A maleNorth Andover, MA · July 14, 2008 -- L-com Connectivity Products announced today that it has added two new USB cable assemblies to their already broad USB line. Both of the new additions use a molded "horizontal panel mount" USB type A female connector on one side. On the other side of the cable is either a USB type A male connector or a 5 pin female header connector.

L-com already carries panel mount USB connectors which includes their widely popular ECF504 series of USB adapters. These new additions mark the first time that L-com has carried a "horizontal panel mount" style where the mounting flanges are on either side of the USB jack, rather than above and below it.

USB type A female horizontal mount to 5 pin header connector"Supporting USB applications is a priority at L-com," said Steve Smith, Product Manager for the USB line. "We already offer many options of USB cables including different jacket materials, different wire AWG sizes and different connector combinations. Now we are pleased to offer different panel mount styles."

Though new to the lineup, L-com expects these cable assemblies to be stocked in the next few weeks and available for same day shipping.

For more information about this release, please contact:
Steve Smith, Product Manager
978-682-6936 x156, ssmith@L-com.com

About L-com

Founded in 1982, L-com (www.L-com.com) is a privately held Massachusetts Corporation dedicated to the design and production of a wide range of interconnect products for the electronics and data communications industries. Primary product emphasis is placed on copper and fiber cable assemblies and accessories for modular and coaxial applications as well as computer networking. The company endeavors to serve the industry by offering solutions to interconnect problems. This effort has led to the development of many new products, some of which are proprietary. L-com has also introduced switching and testing devices in each of their basic product areas. Products are marketed domestically and internationally.


Other press releases that may be of interest to you:
 
8/13/2019 L-com Releases New Cat6 and Cat6a Plenum +105°C, 28AWG, Shielded, Slim Ethernet Patch Cords
8/8/2019 L-com Debuts New UL Listed NEMA-Rated Equipment Enclosures
8/6/2019 New Latching USB 3.0 Cable Assemblies Address Heavy Vibration Applications
8/1/2019 L-com Launches New Triple-Speed Ethernet Switches to Address Industrial Network Applications
7/30/2019 L-com Releases Cat6a Continuous Flex, ZHFR-PUR, Double Shielded Cable Assemblies
7/26/2019 L-com Debuts New Wall-Mount Cabinets and Racks to Address LAN Connectivity Applications
7/25/2019 L-com Introduces new Polycarbonate NEMA-Rated Equipment Enclosures for Wired and Wireless Applications
7/23/2019 L-com Releases New 1U and 2U Cat5e, Cat6 and Cat6a Patch Panels
7/18/2019 L-com Introduces New Active Optical Cables for use in High-Speed Data Center Applications
7/17/2019 L-com Launches New 900 MHz Omni and Sector Antennas
7/16/2019 L-com Unveils Premium 8-Position, A-code, M12 Cable Assemblies for Sensor, Actuator and Fieldbus Applications
7/11/2019 L-com Releases New OM5 Fiber Cables for High-Speed Data Center Applications
6/27/2019 L-com Releases New Small Cell and Outdoor Power Protection Enclosures
6/26/2019 L-com Adds New Premium RJ45 to M12 Female Panel-Mount Cable Assemblies
6/13/2019 L-com Releases New Flat HDMI Cables with LSZH Jackets
5/23/2019 L-com Launches New Indoor and Outdoor-Rated Cat6a Lightning and Surge Protectors
5/14/2019 L-com Introduces New Cat7 LSZH Cable Assemblies for Shipboard, Aerospace and Defense Applications
5/9/2019 L-com Launches New M12 Field Termination Connectors and In-line Adapters to Address Industrial Networking Applications
5/7/2019 L-com Releases New Cat6a Outdoor-Rated, High-Flex Ethernet Cable Assemblies
4/25/2019 L-com Expands Outdoor Industrial Ethernet Cable Line with Additional Length Options Available with Same-Day Shipping
  Page:  1 of 28
    
 
Free Newsletter
L-com Global Connectivity           50 High Street           North Andover, MA 01845
www.L-com.com E-mail: sales@L-com.com 1-800-341-5266 www.Facebook.com/LcomGlobal


© Infinite Electronics International, Inc.