L-com Global Connectivity
  
Cart is Empty
  
USA & Canada (800) 341-5266     International +1 (978) 682-6936
New “Shark Fin” Style Snagless Boots Make High-Density Patching Easy
(Thursday, July 12, 2007)
 

Premium Category 5e Patch Cord GrayNorth Andover, MA – July 11, 2007 – L-com Connectivity Products today unveiled its latest patch cord innovation: snagless boots specially designed to be easily depressed. These new “shark fin” style cables are expected to be the new preferred style of patch cables especially for today’s high-density patch panels.

Snagless boots are used on RJ45 modular connectors to ensure the connector latch does not snag when the patch cable is being pulled through conduit, behind walls, or on cable ladders. Unfortunately, many typical snagless boots are difficult to depress due to a combination of design and material selection. L-com’s new shark fin boots are made of much more flexible material and are designed for easy latch depression. The low profile boot also allows for easy patch cable connection in high-density patch panels since the boot is the same width as the plug. The new series is fully compliant with Category 5E specifications for performance

The new cables come in nine standard colors and lengths from 3 feet all the way up to 100 feet. Custom length cables are also available on request and with modest minimum order quantities. Additionally, crossover versions will be available as well for direct connecting computers.

For more information about this release, please contact:

David Gallagher, Product Marketing Manager
978-682-6936 x127, dgallagher@L-com.com

For over 25 years, L-com Connectivity Products has designed, manufactured, and distributed an extensive offering of copper and fiber telecom and datacom interconnect components such as cable assemblies, adapters, couplers, and connectors, in addition to custom product design and manufacturing capabilities. L-com is headquartered in North Andover, Massachusetts. For more information please visit www.L-com.com.


Other press releases that may be of interest to you:
 
7/18/2019 L-com Introduces New Active Optical Cables for use in High-Speed Data Center Applications
7/17/2019 L-com Launches New 900 MHz Omni and Sector Antennas
7/16/2019 L-com Unveils Premium 8-Position, A-code, M12 Cable Assemblies for Sensor, Actuator and Fieldbus Applications
7/11/2019 L-com Releases New OM5 Fiber Cables for High-Speed Data Center Applications
6/27/2019 L-com Releases New Small Cell and Outdoor Power Protection Enclosures
6/26/2019 L-com Adds New Premium RJ45 to M12 Female Panel-Mount Cable Assemblies
6/13/2019 L-com Releases New Flat HDMI Cables with LSZH Jackets
5/23/2019 L-com Launches New Indoor and Outdoor-Rated Cat6a Lightning and Surge Protectors
5/14/2019 L-com Introduces New Cat7 LSZH Cable Assemblies for Shipboard, Aerospace and Defense Applications
5/9/2019 L-com Launches New M12 Field Termination Connectors and In-line Adapters to Address Industrial Networking Applications
5/7/2019 L-com Releases New Cat6a Outdoor-Rated, High-Flex Ethernet Cable Assemblies
4/25/2019 L-com Expands Outdoor Industrial Ethernet Cable Line with Additional Length Options Available with Same-Day Shipping
4/4/2019 L-com Releases New Patch Panels with N-Type Couplers and 0.630” D-Holes
4/2/2019 L-com Adds New Power Cords for Server, PC, Laptop, PDU Applications and More
3/21/2019 L-com now Stocks 12G-SDI, HD-BNC Connectors for use in Broadcast Video Applications
3/19/2019 L-com Launches New Line of Rugged Category 7 Cables with 10 Gig Rating for Outdoor and Industrial Applications
3/15/2019 L-com Launches Right-Angle USB 3.0 Cable Assemblies with Female Connectors
3/14/2019 L-com Introduces New Right-Angle Panel-Mount DisplayPort Cables
3/12/2019 L-com Unveils New DisplayPort to HDMI Cables with LSZH Jackets
3/5/2019 L-com Debuts New Line of Dual-Rated Slim-Line Ethernet Cables with Spline-Free Design and UL CM Burn Rating
  Page:  1 of 28
    
 
Free Newsletter
L-com Global Connectivity           50 High Street           North Andover, MA 01845
www.L-com.com E-mail: sales@L-com.com 1-800-341-5266 www.Facebook.com/LcomGlobal


© Infinite Electronics International, Inc.