N. ANDOVER, MA -- December 16, 2008 -- L-com (www.l-com.com), a global leader in the manufacture of wired and wireless connectivity products, will feature its DisplayPort (www.l-com.com/DisplayPort) products at CES 2009 in the DisplayPort Tech Zone, Booth #73611, on January 8 – 11, 2009 in Las Vegas.
L-com’s DisplayPort cable assemblies and adapters support the latest computer monitor and home theatre system offerings of OEMs, in order to bring viewers a true digital experience through more efficient use of available bandwidth and the delivery of a robust signal. As the new standard in digital interface technology, DisplayPort-ready devices are able to accommodate the latest graphics and LCD technologies to vastly improve picture brightness and make device-to-device connections easier than ever before.
“As a member of the Video Electronics Standards Association (VESA), L-com is proud to help define new standards and interfaces as well as being engaged in the latest new technologies such as the DisplayPort initiative,” said Zig Woronko, COO of L-com.
L-com offers DisplayPort Cables in two configurations: standard male-to-male and an LSZH version designed for specialty applications. Both are available in two meter and three meter length. Please join us at CES 2009 to see L-com’s portfolio of DisplayPort products.
For more information about L-com products call 1-866-439-2722 x 1450 or 1-978-682-6936 x 1450 or e-mail MediaRelations@L-com.com.
Media Contact:
Kammie Lombardi
Topaz Partners
781-404-2413
klombardi@topazpartners.com
About L-com
L-com, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their Hyperlink line of wireless products which include Antennas, RF Amplifiers, Coaxial lightning and surge protectors, and NEMA rated enclosures. L-com’s HyperLink wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n, RFID and Bluetooth applications. Trusted for over 25 years, L-com, which is headquartered in North Andover, MA, is ISO 9001: 2000 certified and many of its products are UL® recognized. www.l-com.com
# # #