L-com Global Connectivity
  
Cart is Empty
  
USA & Canada (800) 341-5266     International +1 (978) 682-6936
L-com Releases IP68-Rated USB 2.0 Cable Assemblies and Panel-Mount Coupler
(Thursday, January 17, 2019)
 

NORTH ANDOVER, Mass. (Jan. 17, 2019) - L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, announced today that it has released a new line of IP68-rated, USB 2.0 cable assemblies designed for use in harsh environment connectivity applications.

The new U3A00064-series cables feature a USB 2.0, Type-C, waterproof, IP68-rated connector on one end of the assembly and a standard USB 2.0 Type-A connector on the other end. Additional features include gold-plated contacts that stand up to repeated mating cycles, 32/24/28 AWG cable and double shielding to reduce the effects of EMI/RFI.

In addition to the new U3A00064 cable assemblies, L-com has also introduced a new waterproof, panel-mount, Type-C connector with PC tails that is also IP68-rated. The U3B00001 features threaded couplings and an O-ring seal ensuring protection against water and dust. 

“The addition of these new IP68-rated USB connectivity products complements our extensive line of waterproof USB interconnects designed for use in harsh, demanding environments. These new products address the growing need for USB Type-C applications that are now being implemented in harsh, industrial applications, “said Brian Gates, Product Manager.

L-com’s IP68-rated USB 2.0 cable assemblies and IP68-rated Type-C panel mount couplers are in stock and available for immediate shipment.

For more information about this release, please contact:

Peter McNeil
L-com Global Connectivity
17792 Fitch
Irvine, CA
978-682-6936 

About L-com Global Connectivity:

L-com Global Connectivity, a leading manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, antennas, enclosures, surge protectors and more. L-com is headquartered in North Andover, Mass., is ISO 9001: 2008 certified and many of its products are UL® recognized. L-com is an Infinite Electronics brand.

About Infinite Electronics:

Infinite Electronics is a leading global supplier of electronic components serving the urgent needs of engineers through a family of highly recognized and trusted brands.  Our portfolio brands are specialists within their respective product set, offering broad inventories of engineering-grade product, paired with expert technical support and same day shipping. Over 100,000 customers across a diverse set of markets rely upon Infinite Electronics to stock and reliably ship urgently needed products every day.


Other press releases that may be of interest to you:
 
4/4/2019 L-com Releases New Patch Panels with N-Type Couplers and 0.630” D-Holes
4/2/2019 L-com Adds New Power Cords for Server, PC, Laptop, PDU Applications and More
3/21/2019 L-com now Stocks 12G-SDI, HD-BNC Connectors for use in Broadcast Video Applications
3/19/2019 L-com Launches New Line of Rugged Category 7 Cables with 10 Gig Rating for Outdoor and Industrial Applications
3/15/2019 L-com Launches Right-Angle USB 3.0 Cable Assemblies with Female Connectors
3/14/2019 L-com Introduces New Right-Angle Panel-Mount DisplayPort Cables
3/12/2019 L-com Unveils New DisplayPort to HDMI Cables with LSZH Jackets
3/5/2019 L-com Debuts New Line of Dual-Rated Slim-Line Ethernet Cables with Spline-Free Design and UL CM Burn Rating
2/28/2019 L-com Releases New USB 3.1 Gen 2 Type-C Cables with Low-Smoke Zero-Halogen and PVC Jackets
2/21/2019 L-com Debuts New Cat5e, Cat6 and Cat6a Universal Sub-panels with PoE+ Compliant Jacks
2/14/2019 L-com Introduces New RJ45 Termination Block for Field Termination and Repair Applications
2/12/2019 L-com Debuts New Black and White Flat Cat5e and Cat6 Ethernet Cables
2/7/2019 L-com Releases New Cat5e Double-Shielded Outdoor High-Flex PoE Industrial Ethernet Cables
2/5/2019 L-com Debuts New Fiber LC Couplers with Internal Dustproof Shutters
1/31/2019 L-com Releases Aerial and Outdoor Bulk Cable for use in Demanding OSP Networks
1/29/2019 L-com Now Stocks Moldable M12 Connecters for Rugged Applications
1/24/2019 L-com Debuts New Low-Smoke Zero-Halogen 3.5mm Audio Cables
1/22/2019 L-com Introduces New Time Saving Pull-Through RJ45 Plugs and Crimp Tool
1/17/2019 L-com Releases IP68-Rated USB 2.0 Cable Assemblies and Panel-Mount Coupler
1/15/2019 L-com Reveals New Premium Shielded Plenum Cat6a Cable Assemblies and Bulk Cable
  Page:  1 of 27
    
 
Free Newsletter
L-com Global Connectivity           50 High Street           North Andover, MA 01845
www.L-com.com E-mail: sales@L-com.com 1-800-341-5266 www.Facebook.com/LcomGlobal


© Infinite Electronics International, Inc.