L-com Global Connectivity
  
Cart is Empty
  
USA & Canada (800) 341-5266     International +1 (978) 682-6936
L-com Introduces New IP67 Rated HDMI Cables and Coupler for Extreme Connectivity Applications
(Thursday, July 12, 2018)
 

NORTH ANDOVER, Mass. (July 12, 2018) - L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, announced today that it has introduced a new line of waterproof HDMI cable assemblies for use in industrial computing, digital signage, factory automation, medical and harsh environment A/V applications.

These unique IP67 rated HDMI cables feature a waterproof coupling that allows the HDMI connectors to survive harsh environments by preventing the ingress of water and fine particulates such as dust that would typically debilitate standard HDMI connectors.

These unique cables feature support for 4K and 1080p resolutions, rugged molded backshells and gold plated contacts that stand up to repeated mating cycles.

In addition to the new waterproof HDMI cables, L-com has also released a new IP67-rated HDMI panel-mount coupler that can be used with the cable assemblies. The VHC00023 features a standard female HDMI Type-A connector on one side and PC tails on other side for termination to wire or a PC board.

“Our waterproof HDMI cables and coupler offer a perfect solution for our customers who require HDMI connectivity in harsh environments often found in industrial computing and display applications. These unique IP67 rated interconnects are available off-the-shelf with no minimum order quantities,” said Brian Gates, Product Manager.

L-com’s waterproof HDMI cables and panel-mount coupler are in stock and available for immediate shipment.

For more information about this release, please contact:

Peter McNeil
L-com Global Connectivity
17792 Fitch
Irvine, CA
978-682-6936 x1174

About L-com Global Connectivity:

L-com Global Connectivity, a leading manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, antennas, enclosures, surge protectors and more. L-com is headquartered in North Andover, Mass., is ISO 9001: 2008 certified and many of its products are UL® recognized. L-com is an Infinite Electronics company.


Other press releases that may be of interest to you:
 
4/4/2019 L-com Releases New Patch Panels with N-Type Couplers and 0.630” D-Holes
4/2/2019 L-com Adds New Power Cords for Server, PC, Laptop, PDU Applications and More
3/21/2019 L-com now Stocks 12G-SDI, HD-BNC Connectors for use in Broadcast Video Applications
3/19/2019 L-com Launches New Line of Rugged Category 7 Cables with 10 Gig Rating for Outdoor and Industrial Applications
3/15/2019 L-com Launches Right-Angle USB 3.0 Cable Assemblies with Female Connectors
3/14/2019 L-com Introduces New Right-Angle Panel-Mount DisplayPort Cables
3/12/2019 L-com Unveils New DisplayPort to HDMI Cables with LSZH Jackets
3/5/2019 L-com Debuts New Line of Dual-Rated Slim-Line Ethernet Cables with Spline-Free Design and UL CM Burn Rating
2/28/2019 L-com Releases New USB 3.1 Gen 2 Type-C Cables with Low-Smoke Zero-Halogen and PVC Jackets
2/21/2019 L-com Debuts New Cat5e, Cat6 and Cat6a Universal Sub-panels with PoE+ Compliant Jacks
2/14/2019 L-com Introduces New RJ45 Termination Block for Field Termination and Repair Applications
2/12/2019 L-com Debuts New Black and White Flat Cat5e and Cat6 Ethernet Cables
2/7/2019 L-com Releases New Cat5e Double-Shielded Outdoor High-Flex PoE Industrial Ethernet Cables
2/5/2019 L-com Debuts New Fiber LC Couplers with Internal Dustproof Shutters
1/31/2019 L-com Releases Aerial and Outdoor Bulk Cable for use in Demanding OSP Networks
1/29/2019 L-com Now Stocks Moldable M12 Connecters for Rugged Applications
1/24/2019 L-com Debuts New Low-Smoke Zero-Halogen 3.5mm Audio Cables
1/22/2019 L-com Introduces New Time Saving Pull-Through RJ45 Plugs and Crimp Tool
1/17/2019 L-com Releases IP68-Rated USB 2.0 Cable Assemblies and Panel-Mount Coupler
1/15/2019 L-com Reveals New Premium Shielded Plenum Cat6a Cable Assemblies and Bulk Cable
  Page:  1 of 27
    
 
Free Newsletter
L-com Global Connectivity           50 High Street           North Andover, MA 01845
www.L-com.com E-mail: sales@L-com.com 1-800-341-5266 www.Facebook.com/LcomGlobal


© Infinite Electronics International, Inc.