L-com Global Connectivity
  
Cart is Empty
  
USA & Canada (800) 341-5266     International +1 (978) 682-6936
L-com Now Stocks Icron Technologies’ New Raven USB 3-2-1 Extenders
(Thursday, April 26, 2018)
 

NORTH ANDOVER, Mass. (April 26, 2018) - L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, announced today that it is now stocking the new Raven series USB extenders by Icron Technologies Corporation.

The USB 3-2-1 Raven 3104 is the world’s first and only backward compatible USB 3.1 Gen 1 (5 Gbps) extender system for up to 100m distance over a single CAT 6a/7 cable, making it ideal for USB 3.1 web conference cameras as well as any other USB 3.1, 2.0 or 1.1 application. The USB 3-2-1 Raven 3124, suitable for medical and secure environments, provides up to 200m extension over OM3 fiber with additional isolation.

Both FCC/CE Class B certified Raven four-port extender models include an Ethernet side channel for LAN pass-through. They incorporate the ExtremeUSB-C™ suite of features such as transparent USB extension, true plug and play operation (no software drivers required) and are compatible with all major operating systems including Windows®, macOS™, Linux® and Chrome OS™.

“Corporate meeting spaces, large and small, are being equipped with high bandwidth USB 3.1 web conferencing cameras to improve communication and collaboration,” said Glenn Antonelli, Director of Business Management at Icron Technologies. “As a leading connectivity solutions distributor, L-com has been providing Icron extenders to their customers for years. By adding the USB 3-2-1 Raven series to their portfolio, they will be able to better serve the growing market of huddle and conference room installations.”

“Our customers have come to rely on Icron for best-in-class USB extension solutions to address a wide variety of applications. The new Raven USB extenders provide the features, performance and interoperability that other suppliers of USB extension products don’t offer,” said Manuel Martinez, L-com Product Manager.

The new Icron Raven USB extenders are in stock and available for immediate shipment.

For more information about this release, please contact:

Peter McNeil
L-com Global Connectivity
17792 Fitch
Irvine, CA
978-682-6936 x1174

About L-com Global Connectivity

L-com Global Connectivity, a leading manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, antennas, enclosures, surge protectors and more. L-com is headquartered in North Andover, Mass., is ISO 9001: 2008 certified and many of its products are UL® recognized. L-com is an Infinite Electronics company.


Other press releases that may be of interest to you:
 
3/21/2019 L-com now Stocks 12G-SDI, HD-BNC Connectors for use in Broadcast Video Applications
3/19/2019 L-com Launches New Line of Rugged Category 7 Cables with 10 Gig Rating for Outdoor and Industrial Applications
3/15/2019 L-com Launches Right-Angle USB 3.0 Cable Assemblies with Female Connectors
3/14/2019 L-com Introduces New Right-Angle Panel-Mount DisplayPort Cables
3/12/2019 L-com Unveils New DisplayPort to HDMI Cables with LSZH Jackets
3/5/2019 L-com Debuts New Line of Dual-Rated Slim-Line Ethernet Cables with Spline-Free Design and UL CM Burn Rating
2/28/2019 L-com Releases New USB 3.1 Gen 2 Type-C Cables with Low-Smoke Zero-Halogen and PVC Jackets
2/21/2019 L-com Debuts New Cat5e, Cat6 and Cat6a Universal Sub-panels with PoE+ Compliant Jacks
2/14/2019 L-com Introduces New RJ45 Termination Block for Field Termination and Repair Applications
2/12/2019 L-com Debuts New Black and White Flat Cat5e and Cat6 Ethernet Cables
2/7/2019 L-com Releases New Cat5e Double-Shielded Outdoor High-Flex PoE Industrial Ethernet Cables
2/5/2019 L-com Debuts New Fiber LC Couplers with Internal Dustproof Shutters
1/31/2019 L-com Releases Aerial and Outdoor Bulk Cable for use in Demanding OSP Networks
1/29/2019 L-com Now Stocks Moldable M12 Connecters for Rugged Applications
1/24/2019 L-com Debuts New Low-Smoke Zero-Halogen 3.5mm Audio Cables
1/22/2019 L-com Introduces New Time Saving Pull-Through RJ45 Plugs and Crimp Tool
1/17/2019 L-com Releases IP68-Rated USB 2.0 Cable Assemblies and Panel-Mount Coupler
1/15/2019 L-com Reveals New Premium Shielded Plenum Cat6a Cable Assemblies and Bulk Cable
1/10/2019 L-com Launches New Active Optical USB 3.0 Cables that Support 20 Meter Distances
10/16/2018 L-com Releases New Line of High-Temp, Aerospace-Rated Ethernet Cable Assemblies
  Page:  1 of 27
    
 
Free Newsletter
L-com Global Connectivity           50 High Street           North Andover, MA 01845
www.L-com.com E-mail: sales@L-com.com 1-800-341-5266 www.Facebook.com/LcomGlobal


© Infinite Electronics International, Inc.