L-com Global Connectivity
  
Cart is Empty
  
USA & Canada (800) 341-5266     International +1 (978) 682-6936
L-com Debuts New High Flex HDMI Cable Assemblies
(Tuesday, August 29, 2017)
 

NORTH ANDOVER, Mass. (August, 29 2017) - L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, announced today that it has released a new series of high-flex HDMI cables to address confined space A/V applications.

L-com’s high flex HDMI cables were designed to address applications where routing an HDMI cable through tight spaces and around tight corners is required. Additionally, these new high flex HDMI cables can be used in applications where the cable is frequently moved or flexed.

The new VHA00001 series cables feature a fully molded back shell construction providing excellent strain relief and 30 micro-inch gold plated contacts which minimize signal loss even after repeated mating cycles. Additionally, these cables support 4K and 1080p resolutions.

 “We are excited to offer these new high flex HDMI cables to help our customers with tricky installations where standard cables won’t cut it. In addition to their high flex capabilities, these cables also offer all of the same features found in standard high speed HDMI cables,” said Brian Gates, Product Manager.

L-com’s new high flex HDMI cables are in stock and available for immediate shipment.

For more information about this release, please contact:

Peter McNeil
L-com Global Connectivity
17792 Fitch
Irvine, CA
978-682-6936 x1174

About L-com Global Connectivity:

L-com Global Connectivity, a leading manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, antennas, enclosures, surge protectors and more. L-com is headquartered in North Andover, Mass., is ISO 9001: 2008 certified and many of its products are UL® recognized. L-com is an Infinite Electronics company.


Other press releases that may be of interest to you:
 
3/19/2019 L-com Launches New Line of Rugged Category 7 Cables with 10 Gig Rating for Outdoor and Industrial Applications
3/15/2019 L-com Launches Right-Angle USB 3.0 Cable Assemblies with Female Connectors
3/14/2019 L-com Introduces New Right-Angle Panel-Mount DisplayPort Cables
3/12/2019 L-com Unveils New DisplayPort to HDMI Cables with LSZH Jackets
3/5/2019 L-com Debuts New Line of Dual-Rated Slim-Line Ethernet Cables with Spline-Free Design and UL CM Burn Rating
2/28/2019 L-com Releases New USB 3.1 Gen 2 Type-C Cables with Low-Smoke Zero-Halogen and PVC Jackets
2/21/2019 L-com Debuts New Cat5e, Cat6 and Cat6a Universal Sub-panels with PoE+ Compliant Jacks
2/14/2019 L-com Introduces New RJ45 Termination Block for Field Termination and Repair Applications
2/12/2019 L-com Debuts New Black and White Flat Cat5e and Cat6 Ethernet Cables
2/7/2019 L-com Releases New Cat5e Double-Shielded Outdoor High-Flex PoE Industrial Ethernet Cables
2/5/2019 L-com Debuts New Fiber LC Couplers with Internal Dustproof Shutters
1/31/2019 L-com Releases Aerial and Outdoor Bulk Cable for use in Demanding OSP Networks
1/29/2019 L-com Now Stocks Moldable M12 Connecters for Rugged Applications
1/24/2019 L-com Debuts New Low-Smoke Zero-Halogen 3.5mm Audio Cables
1/22/2019 L-com Introduces New Time Saving Pull-Through RJ45 Plugs and Crimp Tool
1/17/2019 L-com Releases IP68-Rated USB 2.0 Cable Assemblies and Panel-Mount Coupler
1/15/2019 L-com Reveals New Premium Shielded Plenum Cat6a Cable Assemblies and Bulk Cable
1/10/2019 L-com Launches New Active Optical USB 3.0 Cables that Support 20 Meter Distances
10/16/2018 L-com Releases New Line of High-Temp, Aerospace-Rated Ethernet Cable Assemblies
9/27/2018 L-com Debuts Low-Smoke Zero-Halogen USB 2.0 Cables with Ferrites
  Page:  1 of 27
    
 
Free Newsletter
L-com Global Connectivity           50 High Street           North Andover, MA 01845
www.L-com.com E-mail: sales@L-com.com 1-800-341-5266 www.Facebook.com/LcomGlobal


© Infinite Electronics International, Inc.