L-com Global Connectivity
  
Cart is Empty
  
USA & Canada (800) 341-5266     International +1 (978) 682-6936

L-com Launches New Screw-Down Lid Weatherproof NEMA Enclosures
(Tuesday, May 02, 2017)
 

NORTH ANDOVER, Mass. (May 2, 2017) - L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, announced today that it has released a series of new screw-down lid, weatherproof NEMA enclosures that are ideal for both indoor and outdoor applications.

L-com’s NBC-series NEMA enclosures are rugged, weatherproof enclosures constructed from hot compression molded, halogen-free, self-extinguishing, fiberglass-reinforced polyester (FRP). The durable exterior makes them well suited for both indoor and outdoor applications in high-temperature and corrosive environments. The new models, that measure 14x12x6 inches, are now available with modified bases which include a non-power mounting plate, as well as vented options and 120 VAC power plate versions that also include venting or heating options.

The NBC-series enclosures are UL/CSA® listed and feature a fully gasketed lid secured by four stainless steel captive screws to ensure optimal integrity. The cover is secured to the base by four threaded brass inserts within the base that create a weatherproof seal to protect the contents inside. An integral mounting flange allows the enclosure to be mounted to a wall or a flat surface without extra mounting hardware. Integral mounting stand-offs inside the enclosure can be used for mounting plates. Blank and custom mounting plates are also available.

“These new NEMA enclosures are a perfect fit for both indoor and outdoor applications; they can withstand the most grueling conditions while boasting a sleek design and attractive appearance. In addition to the six new off-the-shelf models, we offer there enclosures with custom modifications to suit unique application requirements,” said Manuel Martinez, Product Manager.

All models are light gray in color with a contoured body for a clean, cool, contemporary aesthetic. The lighter color also provides better heat reflection and UV resistance. They are ideal for many installations including WLAN equipment, industrial control equipment and hydraulic or pneumatic controls.

For more information about this release, please contact:

Peter McNeil
L-com Global Connectivity
17792 Fitch
Irvine, CA
978-682-6936 x1174 

About L-com Global Connectivity:

L-com Global Connectivity, a leading manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, antennas, enclosures, surge protectors and more. L-com is headquartered in North Andover, Mass., is ISO 9001: 2008 certified and many of its products are UL® recognized. L-com is an Infinite Electronics company.


Other press releases that may be of interest to you:
 
2/15/2018 L-com Launches New IP67-Rated Industrial USB 3.0 Cable Assemblies and Coupler
1/31/2018 L-com Now Offers Waterproof IP67-Rated USB Type-A/A Cable Assemblies
1/30/2018 L-com Unveils New Extended-Length Active HDMI Cables
1/26/2018 L-com Releases M12 and M8 Field Term Connectors, Couplers, Adapters and Receptacles
1/25/2018 L-com Launches New Plenum Rated, Shielded Cat6 Cable Assemblies with 23 AWG Solid Conductors
1/18/2018 L-com Introduces New Cat6a Low-Smoke Zero-Halogen Cable Assemblies and Bulk Cable
11/28/2017 L-com Releases a New Line of Versatile HDMI Adapters
11/14/2017 L-com Launches New USB 2.0 ECF-Style Panel Mount USB Adapter Cables
10/26/2017 L-com Introduces New Line of Universal Sub-Panels with USB, DisplayPort and Cat6a RJ45 Couplers
10/25/2017 L-com Releases New M12 Connectors, Coupler and Receptacles
10/24/2017 L-com Debuts New Windowed NEMA Enclosures
10/5/2017 L-com Launches New USB 3.0 High-Flex Cable Assemblies
10/3/2017 L-com Introduces Ruggedized IP68-Rated Cat6 Receptacles, Plugs and Jam Nuts
9/28/2017 L-com Debuts New USB 3.0 ECF-Style Panel Mount USB Adapter Cables
9/19/2017 L-com Introduces New USB 3.0 Armored Cables for Extreme Environments
9/14/2017 L-com Releases New USB 3.0 Bulk Cable
8/29/2017 L-com Debuts New High Flex HDMI Cable Assemblies
8/24/2017 L-com Launches new USB 2.0 and 3.0 Cables with Ferrite Beads
8/22/2017 L-com Introduces New Mini-HDMI to Mini-HDMI Cables
7/25/2017 L-com Releases IP68 Fiber Plugs, Receptacles and Jam Nuts
  Page:  1 of 25
    
 
Free Newsletter
L-com Global Connectivity           50 High Street           North Andover, MA 01845
www.L-com.com E-mail: sales@L-com.com 1-800-341-5266 www.Facebook.com/LcomGlobal


© L-com, Inc. All Rights Reserved. L-com, Inc., 50 High Street, West Mill, 3rd Floor, Suite #30, North Andover, MA 01845
an Infinite company