L-com Global Connectivity
  
Cart is Empty
  
USA & Canada (800) 341-5266     International +1 (978) 682-6936


L-com Releases New USB 3.0 Type-C Cable Assemblies
(Tuesday, April 18, 2017)
 

NORTH ANDOVER, Mass. (April 18, 2017) - L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, announced today that it has launched two new series of USB 3.0 Type-C to Type-A cable assemblies that are ideal for data storage, video transfer and data acquisition applications.

L-com’s new USB 3.0 Type-C to Type-A cable assemblies are available in two configurations: Type-C female to Type-A male and Type-C male to Type-A female. With data transfer rates of 4.8 Gbps, these cable assemblies meet USB 3.0 standards. They feature 360-degrees of shielding with an overall aluminum/polyester shield and a tinned copper braid shield.

These cable assemblies have fully shielded, twisted pair data lines that provide protection against EMI/RFI, reduce crosstalk and allow for maximum cable flexibility. Type-C connectors allow for simple plug-and-play connections with hand held devices and other USB 3.0 Type-C devices. Both cable series are available in .3, .5, 1, 2 and 3 meter, and 3 foot lengths.

“L-com’s USB 3.0 Type-C to Type-A cable assemblies feature double-shielding and robust cable jacketing to meet the highest manufacturing standards and exceed customer expectations of quality, durability and performance,” said Brian Gates, Product Manager.

L-com's USB 3.0 Type-C cable assemblies include 30u gold-plated connectors for repeated mating cycles, and fully molded connectors for excellent strain relief. They are ideal for mobile devices, computer peripheral devices, gaming, diagnostic tools and medical, military and aerospace applications. 

For more information about this release, please contact:

Peter McNeil
L-com Global Connectivity
17792 Fitch
Irvine, CA
978-682-6936 x1174

About L-com Global Connectivity:

L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking equipment, and custom products, as well as wireless connectivity products which include antennas, RF amplifiers, coaxial lightning and surge protectors, and NEMA rated enclosures. Trusted for more than 30 years, L-com, which is headquartered in North Andover, Mass., is ISO 9001: 2008 certified and many of its products are UL® recognized. For more information, please visit:  http://www.L-com.com/

Other press releases that may be of interest to you:
 
4/26/2018 L-com Now Stocks Icron Technologies’ New Raven USB 3-2-1 Extenders
4/25/2018 L-com Launches New Line of Coaxial RF Lightning and Surge Protectors
4/9/2018 L-com Introduces New IP67 Category5e/6 Dual Use Waterproof Ethernet Cables
3/8/2018 L-com Releases USB 2.0 Type-C Cables with Panel-Mount Connectors
3/6/2018 L-com Launches New 20-Pin DisplayPort Cables with Power Support
3/5/2018 L-com Appoints M-RF Co., Ltd. as Authorized Distributor in Japan
2/27/2018 L-com Now Stocking High-Flex USB 3.0 Cable Assemblies with Type-A to Type-C Connectors
2/22/2018 L-com Introduces New Low-Smoke Zero-Halogen USB 2.0 Bulk Cable with 28/28 AWG Conductors
2/20/2018 L-com Releases Cat5e/6 Patch Panels with PoE + Interfaces
2/15/2018 L-com Launches New IP67-Rated Industrial USB 3.0 Cable Assemblies and Coupler
1/31/2018 L-com Now Offers Waterproof IP67-Rated USB Type-A/A Cable Assemblies
1/30/2018 L-com Unveils New Extended-Length Active HDMI Cables
1/26/2018 L-com Releases M12 and M8 Field Term Connectors, Couplers, Adapters and Receptacles
1/25/2018 L-com Launches New Plenum Rated, Shielded Cat6 Cable Assemblies with 23 AWG Solid Conductors
1/18/2018 L-com Introduces New Cat6a Low-Smoke Zero-Halogen Cable Assemblies and Bulk Cable
11/28/2017 L-com Releases a New Line of Versatile HDMI Adapters
11/14/2017 L-com Launches New USB 2.0 ECF-Style Panel Mount USB Adapter Cables
10/26/2017 L-com Introduces New Line of Universal Sub-Panels with USB, DisplayPort and Cat6a RJ45 Couplers
10/25/2017 L-com Releases New M12 Connectors, Coupler and Receptacles
10/24/2017 L-com Debuts New Windowed NEMA Enclosures
  Page:  1 of 25
    
 
Free Newsletter
L-com Global Connectivity           50 High Street           North Andover, MA 01845
www.L-com.com E-mail: sales@L-com.com 1-800-341-5266 www.Facebook.com/LcomGlobal


© Infinite Electronics International, Inc.
an Infinite company