L-com Global Connectivity
  
Cart is Empty
  
USA & Canada (800) 341-5266     International +1 (978) 682-6936

L-com Introduces New Angled USB 3.0 Type-A Cable Assemblies
(Thursday, April 06, 2017)
 

Angled USB 3.0 CableNORTH ANDOVER, Mass. (April 6, 2017) - L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, announced today that it has released a new line of angled USB 3.0 Type-A cable assemblies for applications that include data storage, video transfer and data acquisition.

L-com’s new USB 3.0 Type-A cable assemblies are available in four connector configurations: Type-A to left-angle Type-A, Type-A to right-angle Type-A, Type-A to left-angle Micro-B and Type-A to right-angle Micro-B.  These cables feature 360-degree shield termination and deliver data transfer speeds of 4.8 Gbps to meet USB 3.0 requirements. They are fully shielded for optimal protection from EMI/RFI, and feature two twisted pair 30 AWG cables with an aluminum/poly foil shield and drain wire.

L-com's USB 3.0 Type-A right angle cable assemblies feature double shielding and robust cable jacketing to ensure reliable performance. These cables are ideal for high speed data transfer in tight spaces, for use with mobile devices, computer peripheral devices, gaming, diagnostic tooling, and medical and military aerospace applications. 

“Our new right angle USB 3.0 Type-A cables are designed to meet USB 3.0 standards, withstand rigorous use and fulfill our customers’ expectations of quality products available when they need them,” said Brian Gates, Product Manager.

All of these new cable assemblies are available off-the-shelf in .3, .5, 1, 2, 3 and 5 meter lengths, with custom lengths available upon request.

For more information about this release, please contact:

Peter McNeil
L-com Global Connectivity
17792 Fitch
Irvine, CA
978-682-6936 x1174

About L-com Global Connectivity:

L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adaptors, computer networking equipment, and custom products, as well as wireless connectivity products which include antennas, RF amplifiers, coaxial lightning and surge protectors, and NEMA rated enclosures. Trusted for more than 30 years, L-com, which is headquartered in North Andover, Mass., is ISO 9001: 2008 certified and many of its products are UL® recognized. For more information, please visit:  http://www.L-com.com/


Other press releases that may be of interest to you:
 
5/30/2018 L-com Launches New Ruggedized, IP68-Rated, Electroless Nickel Finish, Cat6 Receptacles, Plugs and Jam Nuts
5/25/2018 L-com Releases New High-Flex, Continuous Motion, Braided Shield Ethernet Cable Assemblies
5/23/2018 L-com Debuts New Tool-less RJ45 Jacks with PoE+ Compliance
5/3/2018 L-com Introduces a New Series of Data-line Lightning and Surge Protectors for Ethernet and Serial Data Applications
4/26/2018 L-com Now Stocks Icron Technologies’ New Raven USB 3-2-1 Extenders
4/25/2018 L-com Launches New Line of Coaxial RF Lightning and Surge Protectors
4/9/2018 L-com Introduces New IP67 Category5e/6 Dual Use Waterproof Ethernet Cables
3/8/2018 L-com Releases USB 2.0 Type-C Cables with Panel-Mount Connectors
3/6/2018 L-com Launches New 20-Pin DisplayPort Cables with Power Support
3/5/2018 L-com Appoints M-RF Co., Ltd. as Authorized Distributor in Japan
2/27/2018 L-com Now Stocking High-Flex USB 3.0 Cable Assemblies with Type-A to Type-C Connectors
2/22/2018 L-com Introduces New Low-Smoke Zero-Halogen USB 2.0 Bulk Cable with 28/28 AWG Conductors
2/20/2018 L-com Releases Cat5e/6 Patch Panels with PoE + Interfaces
2/15/2018 L-com Launches New IP67-Rated Industrial USB 3.0 Cable Assemblies and Coupler
1/31/2018 L-com Now Offers Waterproof IP67-Rated USB Type-A/A Cable Assemblies
1/30/2018 L-com Unveils New Extended-Length Active HDMI Cables
1/26/2018 L-com Releases M12 and M8 Field Term Connectors, Couplers, Adapters and Receptacles
1/25/2018 L-com Launches New Plenum Rated, Shielded Cat6 Cable Assemblies with 23 AWG Solid Conductors
1/18/2018 L-com Introduces New Cat6a Low-Smoke Zero-Halogen Cable Assemblies and Bulk Cable
11/28/2017 L-com Releases a New Line of Versatile HDMI Adapters
  Page:  1 of 25
    
 
Free Newsletter
L-com Global Connectivity           50 High Street           North Andover, MA 01845
www.L-com.com E-mail: sales@L-com.com 1-800-341-5266 www.Facebook.com/LcomGlobal


© Infinite Electronics International, Inc.
an Infinite company