L-com Global Connectivity
  
Cart is Empty
  
USA & Canada (800) 341-5266     International +1 (978) 682-6936

L-com Launches New Line of High-Performance Ethernet Mini-Couplers
(Wednesday, March 15, 2017)
 

NORTH ANDOVER, Mass. (March 15,2017) - L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, announced today that it has released a new line of Ethernet mini-couplers that are engineered to deliver exceptional performance in a very compact design.

L-com’s eight new mini-couplers provide the same performance and quality as full-size Ethernet couplers, but measure less than one inch in length. They are shorter and lighter than standard couplers which maximizes usable space behind the panel. This design provides more room for installers to work with behind racks, panels or enclosures, improves air flow and reduces stress on cable exits, ensuring that the mating assembly’s bend radius is not exceeded.

These mini-couplers are available with three options: Cat5e or Cat6 rating, shielded or unshielded and either in-line or keystone-style. The keystone-style, snap-in couplers are easy to use and are ideal for patch panel and enclosure applications. The in-line couplers offer a versatile and economical way to couple two Ethernet cables, and their compact design allows them to be stacked vertically or horizontally with no space between couplers.

 “Our new mini-couplers offer the same superior performance and quality as our best-selling full-size models, but in a super-compact, versatile package that is a perfect fit for almost any application,” said Dustin Guttadauro, Product Manager.

L-com's high performance mini-couplers are ideal for premise applications such as wiring, telecommunications, LAN; 10BASE-T, 100BASE-TX or 1000BASE-T Ethernet; voice, data and video networking. They are RJ45 (8x8) female to RJ45 (8x8) female which allows for easy coupling of cables without requiring tools or punch-downs. These couplers exceed category standards and EIA568A/B dual wiring provides compatibility for every installation.

For more information about this release, please contact:

Peter McNeil
L-com Global Connectivity
17792 Fitch
Irvine, CA
978-682-6936 x1174

About L-com Global Connectivity:

L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking equipment, and custom products, as well as their HyperLink® brand of wireless products which include antennas, RF amplifiers, coaxial lightning and surge protectors, and NEMA rated enclosures. L-com's HyperLink® wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n/ac, RFID and Bluetooth applications. In addition to HyperLink® , L-com’s other brands include MilesTek®, specialists in Military/Aeronautics connectivity solutions, Aiconics®, a leading manufacturer of electrical connector products and Point Six™ Wireless, pioneers in the design and manufacture of wireless sensors used in IoT applications. Trusted for more than 30 years, L-com, which is headquartered in North Andover, Mass., is ISO 9001: 2008 certified and many of its products are UL® recognized. For more information, please visit:  http://www.L-com.com/


Other press releases that may be of interest to you:
 
2/15/2018 L-com Launches New IP67-Rated Industrial USB 3.0 Cable Assemblies and Coupler
1/31/2018 L-com Now Offers Waterproof IP67-Rated USB Type-A/A Cable Assemblies
1/30/2018 L-com Unveils New Extended-Length Active HDMI Cables
1/26/2018 L-com Releases M12 and M8 Field Term Connectors, Couplers, Adapters and Receptacles
1/25/2018 L-com Launches New Plenum Rated, Shielded Cat6 Cable Assemblies with 23 AWG Solid Conductors
1/18/2018 L-com Introduces New Cat6a Low-Smoke Zero-Halogen Cable Assemblies and Bulk Cable
11/28/2017 L-com Releases a New Line of Versatile HDMI Adapters
11/14/2017 L-com Launches New USB 2.0 ECF-Style Panel Mount USB Adapter Cables
10/26/2017 L-com Introduces New Line of Universal Sub-Panels with USB, DisplayPort and Cat6a RJ45 Couplers
10/25/2017 L-com Releases New M12 Connectors, Coupler and Receptacles
10/24/2017 L-com Debuts New Windowed NEMA Enclosures
10/5/2017 L-com Launches New USB 3.0 High-Flex Cable Assemblies
10/3/2017 L-com Introduces Ruggedized IP68-Rated Cat6 Receptacles, Plugs and Jam Nuts
9/28/2017 L-com Debuts New USB 3.0 ECF-Style Panel Mount USB Adapter Cables
9/19/2017 L-com Introduces New USB 3.0 Armored Cables for Extreme Environments
9/14/2017 L-com Releases New USB 3.0 Bulk Cable
8/29/2017 L-com Debuts New High Flex HDMI Cable Assemblies
8/24/2017 L-com Launches new USB 2.0 and 3.0 Cables with Ferrite Beads
8/22/2017 L-com Introduces New Mini-HDMI to Mini-HDMI Cables
7/25/2017 L-com Releases IP68 Fiber Plugs, Receptacles and Jam Nuts
  Page:  1 of 25
    
 
Free Newsletter
L-com Global Connectivity           50 High Street           North Andover, MA 01845
www.L-com.com E-mail: sales@L-com.com 1-800-341-5266 www.Facebook.com/LcomGlobal


© L-com, Inc. All Rights Reserved. L-com, Inc., 50 High Street, West Mill, 3rd Floor, Suite #30, North Andover, MA 01845
an Infinite company