L-com Global Connectivity
  
Cart is Empty
  
USA & Canada (800) 341-5266     International +1 (978) 682-6936


L-com Debuts 802.11ac Dual-Band, Dual- Polarized 2x2 MIMO Outdoor Omni-Directional Antennas
(Wednesday, March 08, 2017)
 

NORTH ANDOVER, Mass. (March 8,2017) - L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, announced today that it has released a new series of dual-band, dual-polarized 2x2 MIMO antennas for use in MIMO/802.11ac devices.

L-com’s DPU2-series antennas are dual-band, outdoor, Omni-directional  antennas with dual-polarization that permits them to operate in both vertical and horizontal polarizations. One of these antennas can do the same work as two antennas by simultaneously transmitting data on one polarization while receiving data on the other polarization. These antennas also increase Wi-Fi data speed by allowing the attenuation of unwanted signals from adjacent channels and/or co-located equipment, which improves RF performance and increases data speed.

DPU2-series antennas feature both 2.4/5 GHz horizontally and vertically polarized antennas in one radome. They deliver 360-degree 302.11ac coverage while decreasing performance issues from RF interference. These antennas are ideal for enabling multi-stream communications on IEEE 802.11n/ac networks. Supported MIMO types include 1x2 systems for 802.11a/g/n protocols and 2x2 systems for 802.11ac protocols.

“Our DPU2-series antennas are essentially two antennas in one package, able to provide multi-stream communication from a single antenna instead of requiring two opposite-polarized antennas to do the same task,” said Patrick Pesa, Director of Wireless Product Management.

L-com's DPU2-series antennas boast industrial-grade construction and are available in 6 dBi, 9 dBi and 11 dBi versions. A UV-resistant, PVC radome helps ensure long-term, reliable operation in all weather conditions. A heavy duty extruded aluminum base/mount allows the antenna to be mounted to masts up to 3.7 inches in diameter.

For more information about this release, please contact:

Peter McNeil
L-com Global Connectivity
17792 Fitch
Irvine, CA
978-682-6936 x1174

About L-com Global Connectivity:

L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking equipment, and custom products, as well as their HyperLink® brand of wireless products which include antennas, RF amplifiers, coaxial lightning and surge protectors, and NEMA rated enclosures. L-com's HyperLink® wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n/ac, RFID and Bluetooth applications. In addition to HyperLink® , L-com’s other brands include MilesTek®, specialists in Military/Aeronautics connectivity solutions, Aiconics®, a leading manufacturer of electrical connector products and Point Six™ Wireless, pioneers in the design and manufacture of wireless sensors used in IoT applications. Trusted for more than 30 years, L-com, which is headquartered in North Andover, Mass., is ISO 9001: 2008 certified and many of its products are UL® recognized. For more information, please visit:  http://www.L-com.com/


Other press releases that may be of interest to you:
 
4/26/2018 L-com Now Stocks Icron Technologies’ New Raven USB 3-2-1 Extenders
4/25/2018 L-com Launches New Line of Coaxial RF Lightning and Surge Protectors
4/9/2018 L-com Introduces New IP67 Category5e/6 Dual Use Waterproof Ethernet Cables
3/8/2018 L-com Releases USB 2.0 Type-C Cables with Panel-Mount Connectors
3/6/2018 L-com Launches New 20-Pin DisplayPort Cables with Power Support
3/5/2018 L-com Appoints M-RF Co., Ltd. as Authorized Distributor in Japan
2/27/2018 L-com Now Stocking High-Flex USB 3.0 Cable Assemblies with Type-A to Type-C Connectors
2/22/2018 L-com Introduces New Low-Smoke Zero-Halogen USB 2.0 Bulk Cable with 28/28 AWG Conductors
2/20/2018 L-com Releases Cat5e/6 Patch Panels with PoE + Interfaces
2/15/2018 L-com Launches New IP67-Rated Industrial USB 3.0 Cable Assemblies and Coupler
1/31/2018 L-com Now Offers Waterproof IP67-Rated USB Type-A/A Cable Assemblies
1/30/2018 L-com Unveils New Extended-Length Active HDMI Cables
1/26/2018 L-com Releases M12 and M8 Field Term Connectors, Couplers, Adapters and Receptacles
1/25/2018 L-com Launches New Plenum Rated, Shielded Cat6 Cable Assemblies with 23 AWG Solid Conductors
1/18/2018 L-com Introduces New Cat6a Low-Smoke Zero-Halogen Cable Assemblies and Bulk Cable
11/28/2017 L-com Releases a New Line of Versatile HDMI Adapters
11/14/2017 L-com Launches New USB 2.0 ECF-Style Panel Mount USB Adapter Cables
10/26/2017 L-com Introduces New Line of Universal Sub-Panels with USB, DisplayPort and Cat6a RJ45 Couplers
10/25/2017 L-com Releases New M12 Connectors, Coupler and Receptacles
10/24/2017 L-com Debuts New Windowed NEMA Enclosures
  Page:  1 of 25
    
 
Free Newsletter
L-com Global Connectivity           50 High Street           North Andover, MA 01845
www.L-com.com E-mail: sales@L-com.com 1-800-341-5266 www.Facebook.com/LcomGlobal


© Infinite Electronics International, Inc.
an Infinite company