L-com Global Connectivity
Cart is Empty
USA & Canada (800) 341-5266     International +1 (978) 682-6936

L-com Debuts Premium M12 Cable Assemblies for Harsh Environments
(Tuesday, November 22, 2016)

NORTH ANDOVER, Mass. (November 22, 2016) -L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, announced today that it has released a new series of premium M12 cable assemblies.

L-com’s new line of premium M12 cable assemblies are made for the toughest, most demanding applications. For extra strength, these cables are built with high-flex, outdoor CMX-rated, double-shielded, FR-TPE cable and IP68 rated M12 connectors. They are designed to exceed category standards and ensure optimal network throughput even in harsh industrial or extreme weather conditions. These cable assemblies are available off-the-shelf with connector options that include D-coded, 4-position male M12, 4-position female M12 and standard RJ45 combinations.

The Flame-Retardant Thermoplastic Elastomer (FR-TPE) cable jackets are resistant to oil, sunlight (UV) and weld spatter. Additionally, these cables are rated for 600V and are flex-tested to 1 million cycles at 10x cable OD and 10 million cycles at 20x cable OD. A double-shielded braid and foil design provides maximum protection from EMI/RFI. These cables are ideal for various applications such as industrial Ethernet, test equipment, industrial controls, factory automation, I/O connectivity and sensor and actuator connectivity.

“Our premium M12 cable assemblies are as robust as they come. They are specifically designed to withstand the harshest conditions and ensure that your network will run smoothly in any harsh environment,” said Dustin Guttadauro, Product Manager.

L-com's premium M12 cables are available in 0.5, 1, 2, 3, 5 and 10 meter lengths. Custom lengths and labeling are also available by contacting L-com or using L-com’s Custom Cable Configurator.

For more information about this release, please contact:

Peter McNeil
L-com Global Connectivity
17792 Fitch
Irvine, CA
978-682-6936 x1174

About L-com Global Connectivity:

L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking equipment, and custom products, as well as their HyperLink® brand of wireless products which include antennas, RF amplifiers, coaxial lightning and surge protectors, and NEMA rated enclosures. L-com's HyperLink® wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n/ac, RFID and Bluetooth applications. In addition to HyperLink® , L-com’s other brands include MilesTek®, specialists in Military/Aeronautics connectivity solutions, Aiconics®, a leading manufacturer of electrical connector products and Point Six™ Wireless, pioneers in the design and manufacture of wireless sensors used in IoT applications. Trusted for more than 30 years, L-com, which is headquartered in North Andover, Mass., is ISO 9001: 2008 certified and many of its products are UL® recognized. For more information, please visit: http://www.L-com.com/

Other press releases that may be of interest to you:
3/8/2018 L-com Releases USB 2.0 Type-C Cables with Panel-Mount Connectors
3/6/2018 L-com Launches New 20-Pin DisplayPort Cables with Power Support
3/5/2018 L-com Appoints M-RF Co., Ltd. as Authorized Distributor in Japan
2/27/2018 L-com Now Stocking High-Flex USB 3.0 Cable Assemblies with Type-A to Type-C Connectors
2/22/2018 L-com Introduces New Low-Smoke Zero-Halogen USB 2.0 Bulk Cable with 28/28 AWG Conductors
2/20/2018 L-com Releases Cat5e/6 Patch Panels with PoE + Interfaces
2/15/2018 L-com Launches New IP67-Rated Industrial USB 3.0 Cable Assemblies and Coupler
1/31/2018 L-com Now Offers Waterproof IP67-Rated USB Type-A/A Cable Assemblies
1/30/2018 L-com Unveils New Extended-Length Active HDMI Cables
1/26/2018 L-com Releases M12 and M8 Field Term Connectors, Couplers, Adapters and Receptacles
1/25/2018 L-com Launches New Plenum Rated, Shielded Cat6 Cable Assemblies with 23 AWG Solid Conductors
1/18/2018 L-com Introduces New Cat6a Low-Smoke Zero-Halogen Cable Assemblies and Bulk Cable
11/28/2017 L-com Releases a New Line of Versatile HDMI Adapters
11/14/2017 L-com Launches New USB 2.0 ECF-Style Panel Mount USB Adapter Cables
10/26/2017 L-com Introduces New Line of Universal Sub-Panels with USB, DisplayPort and Cat6a RJ45 Couplers
10/25/2017 L-com Releases New M12 Connectors, Coupler and Receptacles
10/24/2017 L-com Debuts New Windowed NEMA Enclosures
10/5/2017 L-com Launches New USB 3.0 High-Flex Cable Assemblies
10/3/2017 L-com Introduces Ruggedized IP68-Rated Cat6 Receptacles, Plugs and Jam Nuts
9/28/2017 L-com Debuts New USB 3.0 ECF-Style Panel Mount USB Adapter Cables
  Page:  1 of 25
Free Newsletter
L-com Global Connectivity           50 High Street           North Andover, MA 01845
www.L-com.com E-mail: sales@L-com.com 1-800-341-5266 www.Facebook.com/LcomGlobal

© L-com, Inc. All Rights Reserved. L-com, Inc., 50 High Street, West Mill, 3rd Floor, Suite #30, North Andover, MA 01845
an Infinite company