L-com Global Connectivity
  
Cart is Empty
  
USA & Canada (800) 341-5266     International +1 (978) 682-6936

L-com Debuts Dual-Polarized, High-Density MIMO Antenna
(Thursday, September 01, 2016)
 

NORTH ANDOVER, Mass. (September 1, 2016) - L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, announced today that it has released a dual-polarized, high-density antenna.

L-com’s HyperLink brand HG2458-13HDP-4NF is a dual-polarized, high-density antenna that features a narrow beamwidth in both vertical and horizontal polarization. This allows the antenna to be positioned exactly where needed to reduce channel-to-channel interference and increase capacity. The high-gain of the HG2458-13HDP-4NF allows for greater distance between the antenna and the user(s), which is ideal in large venues such as stadiums and arenas.

In addition to supporting high-density applications, the HG2458-13HDP-4NF is also dual-band and dual-polarized. This versatile MIMO antenna combines four dual-band antennas in a single housing. The unit consists of two vertical and two horizontal polarized, multi-patch antennas. These are accessed via four separate N-female connectors on the rear of the antenna. Each port on the HG2458-13HDP-4NF can support 2.4 GHz and 4.9-5.8 GHz frequencies. By providing coverage for the full Wi-Fi band, this antenna is compatible with many of the new generation IEEE 802.11ac MIMO radios.

”Large venues with high-concentrations of wireless users, such as stadiums and convention centers, often have performance and capacity issues that cause difficulties with wireless coverage. Our high-density antenna solves these problems with a focused beamwidth that minimizes interference, improves coverage and provides greater capacity,” said Ken Burgner, Product Manager.

Designed for both indoor and outdoor operation, the HG2458-13HDP-4NF features a heavy duty UV-resistant radome and ships with a tilt and swivel mast mount kit that provides quick installation at various degrees of up/down tilt.   

For more information about this release, please contact:
Peter McNeil, Marketing Manager
978-682-6936 x1174, pmcneil@l-com.com

About L-com Global Connectivity:

L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking equipment, and custom products, as well as their HyperLink® brand of wireless products which include antennas, RF amplifiers, coaxial lightning and surge protectors, and NEMA rated enclosures. L-com's HyperLink® wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n/ac, RFID and Bluetooth applications. In addition to HyperLink® , L-com’s other brands include MilesTek®, specialists in Military/Aeronautics connectivity solutions, Aiconics®, a leading manufacturer of electrical connector products and Point Six™ Wireless, pioneers in the design and manufacture of wireless sensors used in IoT applications. Trusted for more than 30 years, L-com, which is headquartered in North Andover, Mass., is ISO 9001: 2008 certified and many of its products are UL® recognized. For more information, please visit:  http://www.L-com.com/

Other press releases that may be of interest to you:
 
2/15/2018 L-com Launches New IP67-Rated Industrial USB 3.0 Cable Assemblies and Coupler
1/31/2018 L-com Now Offers Waterproof IP67-Rated USB Type-A/A Cable Assemblies
1/30/2018 L-com Unveils New Extended-Length Active HDMI Cables
1/26/2018 L-com Releases M12 and M8 Field Term Connectors, Couplers, Adapters and Receptacles
1/25/2018 L-com Launches New Plenum Rated, Shielded Cat6 Cable Assemblies with 23 AWG Solid Conductors
1/18/2018 L-com Introduces New Cat6a Low-Smoke Zero-Halogen Cable Assemblies and Bulk Cable
11/28/2017 L-com Releases a New Line of Versatile HDMI Adapters
11/14/2017 L-com Launches New USB 2.0 ECF-Style Panel Mount USB Adapter Cables
10/26/2017 L-com Introduces New Line of Universal Sub-Panels with USB, DisplayPort and Cat6a RJ45 Couplers
10/25/2017 L-com Releases New M12 Connectors, Coupler and Receptacles
10/24/2017 L-com Debuts New Windowed NEMA Enclosures
10/5/2017 L-com Launches New USB 3.0 High-Flex Cable Assemblies
10/3/2017 L-com Introduces Ruggedized IP68-Rated Cat6 Receptacles, Plugs and Jam Nuts
9/28/2017 L-com Debuts New USB 3.0 ECF-Style Panel Mount USB Adapter Cables
9/19/2017 L-com Introduces New USB 3.0 Armored Cables for Extreme Environments
9/14/2017 L-com Releases New USB 3.0 Bulk Cable
8/29/2017 L-com Debuts New High Flex HDMI Cable Assemblies
8/24/2017 L-com Launches new USB 2.0 and 3.0 Cables with Ferrite Beads
8/22/2017 L-com Introduces New Mini-HDMI to Mini-HDMI Cables
7/25/2017 L-com Releases IP68 Fiber Plugs, Receptacles and Jam Nuts
  Page:  1 of 25
    
 
Free Newsletter
L-com Global Connectivity           50 High Street           North Andover, MA 01845
www.L-com.com E-mail: sales@L-com.com 1-800-341-5266 www.Facebook.com/LcomGlobal


© L-com, Inc. All Rights Reserved. L-com, Inc., 50 High Street, West Mill, 3rd Floor, Suite #30, North Andover, MA 01845
an Infinite company