L-com Global Connectivity
  
Cart is Empty
  
USA & Canada (800) 341-5266     International +1 (978) 682-6936


L-com Releases Embedded Flexible DAS Antenna
(Thursday, August 25, 2016)
 

NORTH ANDOVER, Mass. (August 25, 2016) - L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, announced today that it has launched a flexible embedded antenna.

L-com’s HyperLink brand HG72705FPU-UFL is a flexible, Omni-directional embedded antenna designed to be directly integrated into devices that require wireless capability. By embedding this antenna into a device, the need for external antennas is eliminated. The Omni-directional design of the HG72705FPU-UFL provides complete 360° coverage, making it ideal for multipoint and mobile wireless systems.

The HG72705FPU-UFL is specifically designed for Distributed Antenna Systems (DAS) used to distribute cellular and Wi-Fi signals throughout a building or area. With an operating range of 698-960 MHz to 1710-2700 MHz, it is ideal for cellular LTE and Wi-Fi applications. The multi-band capability of this antenna eliminates the need to use different antennas for each frequency.

”Today’s antennas need to be small enough to embed into smaller devices yet powerful enough to operate on a wide range of frequencies that include cellular, Wi-Fi and even DAS networks. The HG72705FPU-UFL was designed as a quick off-the-shelf solution and is ideal for engineers developing prototype equipment that requires an antenna for devices with tight space constraints,” said Ken Burgner, Product Manager.

Constructed from a flexible polymer, the HG72705FPU-UFL can be attached to flat or curved surfaces by its adhesive backing. This unique design provides engineers with greater flexibility when designing wireless communications equipment.

For more information about this release, please contact:
Peter McNeil, Marketing Manager
978-682-6936 x1174, pmcneil@l-com.com

About L-com Global Connectivity:

L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking equipment, and custom products, as well as their HyperLink® brand of wireless products which include antennas, RF amplifiers, coaxial lightning and surge protectors, and NEMA rated enclosures. L-com's HyperLink® wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n/ac, RFID and Bluetooth applications. In addition to HyperLink® , L-com’s other brands include MilesTek®, specialists in Military/Aeronautics connectivity solutions, Aiconics®, a leading manufacturer of electrical connector products and Point Six™ Wireless, pioneers in the design and manufacture of wireless sensors used in IoT applications. Trusted for more than 30 years, L-com, which is headquartered in North Andover, Mass., is ISO 9001: 2008 certified and many of its products are UL® recognized. For more information, please visit:  http://www.L-com.com/

Other press releases that may be of interest to you:
 
4/26/2018 L-com Now Stocks Icron Technologies’ New Raven USB 3-2-1 Extenders
4/25/2018 L-com Launches New Line of Coaxial RF Lightning and Surge Protectors
4/9/2018 L-com Introduces New IP67 Category5e/6 Dual Use Waterproof Ethernet Cables
3/8/2018 L-com Releases USB 2.0 Type-C Cables with Panel-Mount Connectors
3/6/2018 L-com Launches New 20-Pin DisplayPort Cables with Power Support
3/5/2018 L-com Appoints M-RF Co., Ltd. as Authorized Distributor in Japan
2/27/2018 L-com Now Stocking High-Flex USB 3.0 Cable Assemblies with Type-A to Type-C Connectors
2/22/2018 L-com Introduces New Low-Smoke Zero-Halogen USB 2.0 Bulk Cable with 28/28 AWG Conductors
2/20/2018 L-com Releases Cat5e/6 Patch Panels with PoE + Interfaces
2/15/2018 L-com Launches New IP67-Rated Industrial USB 3.0 Cable Assemblies and Coupler
1/31/2018 L-com Now Offers Waterproof IP67-Rated USB Type-A/A Cable Assemblies
1/30/2018 L-com Unveils New Extended-Length Active HDMI Cables
1/26/2018 L-com Releases M12 and M8 Field Term Connectors, Couplers, Adapters and Receptacles
1/25/2018 L-com Launches New Plenum Rated, Shielded Cat6 Cable Assemblies with 23 AWG Solid Conductors
1/18/2018 L-com Introduces New Cat6a Low-Smoke Zero-Halogen Cable Assemblies and Bulk Cable
11/28/2017 L-com Releases a New Line of Versatile HDMI Adapters
11/14/2017 L-com Launches New USB 2.0 ECF-Style Panel Mount USB Adapter Cables
10/26/2017 L-com Introduces New Line of Universal Sub-Panels with USB, DisplayPort and Cat6a RJ45 Couplers
10/25/2017 L-com Releases New M12 Connectors, Coupler and Receptacles
10/24/2017 L-com Debuts New Windowed NEMA Enclosures
  Page:  1 of 25
    
 
Free Newsletter
L-com Global Connectivity           50 High Street           North Andover, MA 01845
www.L-com.com E-mail: sales@L-com.com 1-800-341-5266 www.Facebook.com/LcomGlobal


© Infinite Electronics International, Inc.
an Infinite company